RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Seeking Your Interest in RoadTesting an IR light angle sensor board
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 14 replies
  • Subscribers 2747 subscribers
  • Views 2948 views
  • Users 0 members are here
  • roadtester poll
Related

Seeking Your Interest in RoadTesting an IR light angle sensor board

rscasny
rscasny over 1 year ago

imageI have had a conversation with a supplier interesting in having the element14 community roadtest its IR light angle sensor board. I don't recall us previously roadtesting this type of sensor (or at least recently within the past year), so let me give you a few facts about it.

If you have the time to explore the device, I'd appreciate you voting in my poll below. Of course, you are free to leave a comment. Many thinks.

Randall
element14 Community Team

Here's a few facts about the board:

EVAL-ADPD2140Z is an evaluation kit to evaluate the ADPD2140 IR light angle sensor, collect data from the ADPD2140, and evaluate gesture recognition and triangulation capabilities. The evaluation kit requires the EVAL-ADPDM3Z evaluation board and the Applications Wavetool, a graphical user interface (GUI) that provides users with low level and high level configurability, real-time data analysis, and user datagram protocol (UDP) transfer capability, which allows the EVAL-ADPDM3Z evaluation board to interface to a PC. The USB port of the PC powers the EVAL-ADPDM3Z evaluation board and provides power to the EVAL-ADPD2140Z evaluation board. On-board voltage regulators provide voltage supplies for the ADPD2140.

Here's some documentation

  • UG-1358: ADPD2140 Evaluation Board User Guide
  • UG-1282: EVAL-ADPDM3Z Evaluation Board User Guide
  • Reference Design CN0569 Infrared Gesture Recognition Module

Here's the poll:

  • Sign in to reply
  • Cancel
  • beacon_dave
    beacon_dave over 1 year ago in reply to obones
    obones said:
    That's not going to be really easy to move an human hand in such a small volume

    I seem to manage ok when using a computer mouse / 3D mouse.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • kmikemoo
    kmikemoo over 1 year ago in reply to obones

    obones I agree that the range drives the application.  It makes me think of those "foot operated" sensors that are supposed to open passenger vehicle liftgates simply by waving your foot beneath the vehicle.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • DAB
    DAB over 1 year ago in reply to obones

    True, but you could use a reflective ball on the end of a rod to see just how accurately you could make the position locations respond to a series of preset activities.

    That and you could use it to test sobriety based upon how steady you could hold your position.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • obones
    obones over 1 year ago in reply to DAB

    Albeit in a very small cube of 20cm wall size, as stated in the EVAL-ADPD2140Z User Guide:

    > Move a hand or other reflective object within 20 cm directly above the device.

    That's not going to be really easy to move an human hand in such a small volume, but I'm very interested in seeing if it can see anything more than just "the hand went from left to right"

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • DAB
    DAB over 1 year ago

    I just realized that you could set up two of these boards and do 3D mapping of gestures, that would be a very interesting capability to explore.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • rsjawale24
    rsjawale24 over 1 year ago

    Seems interesting. Apart from gesture recognition, I wonder if it can also be used for applications like shaft alignment, counting rotations or other IR applications.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur over 1 year ago

    image

    I'm thinking I got the setup correct in order to Roadtest.

    The hardware descriptive name both being "Evaluation boards" at first glance confused me. I had to a deeper dive to understand.

    I rather enjoy dabbling with IR stuff. Might me interesting. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • embeddedguy
    embeddedguy over 1 year ago in reply to shabaz

    Oh, Now I see, there is SCL visible on the board in the image above. Thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 1 year ago in reply to embeddedguy

    The sensor board has I2C and supply connections, to allow it to be connected to other hardware instead of the supplied microcontroller board, to allow users to develop their own code.

    But, it may require a level converter (I believe the voltages levels are 1.8V).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dwinhold
    dwinhold over 1 year ago

    Very interesting hardware, it looks to be limited, since the program is "Evaluation only".  It would be interesting to see what can be done once we have it in hand.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
>