RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Difficulty getting good ripple / noise measurements
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 21 replies
  • Subscribers 2752 subscribers
  • Views 4251 views
  • Users 0 members are here
Related

Difficulty getting good ripple / noise measurements

Fred27
Fred27 over 1 year ago

Im currently roadtesting the Rohde & Schwarz NGC103 and as part of my investigation I'm trying to measure the ripple / noise and compare it to other supplies. The problem I'm having is that I don't seem to be able to get a reasonable measurement. I get the feeling that isn't swamped by external interference.

I watched a helpful EEVBlog video and tried to optimise my setup but I don't seem to be able to get close to any meaningful measurement. In fact, there's not much different if I just connect the two banana plugs together and measure the noise on my 0V there!

Here's a photo of the best setup I've managed so far. I tried differential measurement with one probe on + and one on - and measuring the difference. Whilst I could see the common mode noise on both channes that were being cancelled out, the result was still noisier than this. I have AC coupling, a 20Mhz bandwidth limit and have tried via a 10:1 probe, a 1:1 probe, and probeless direct via banana to BNC as pictured.

Noise measurement setup

Noise measurement screenshot

Any suggestions? In fact, is measuring noise in a setup like this even useful? Would you just trust the datasheet on this? For reference, the datasheet says < 6mV peak-to-peak and < 1mV RMS. I'm getting over an order of magniture more.

  • Sign in to reply
  • Cancel
Parents
  • battlecoder
    0 battlecoder over 1 year ago

    I would definitely recommend using a resistor as a load instead of an electronic load (they do introduce some amount of noise and ripple). From the EEVblog videos I've watched, if you are going to use what's essentially a direct BNC connection you need to terminate the connection with a 50 ohm resistor. There's this video, where he discusses a mistake he made previously measuring the noise in a switching supply, and goes through the 50 ohm resistor method for straight BNC connections.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • battlecoder
    0 battlecoder over 1 year ago

    I would definitely recommend using a resistor as a load instead of an electronic load (they do introduce some amount of noise and ripple). From the EEVblog videos I've watched, if you are going to use what's essentially a direct BNC connection you need to terminate the connection with a 50 ohm resistor. There's this video, where he discusses a mistake he made previously measuring the noise in a switching supply, and goes through the 50 ohm resistor method for straight BNC connections.