RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Seeking 2 People to RoadTest an FPGA Board
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 20 replies
  • Subscribers 2749 subscribers
  • Views 3474 views
  • Users 0 members are here
  • roadtester survey
  • auboard
  • AES-AUB-15P-DK-G
Related

Seeking 2 People to RoadTest an FPGA Board

rscasny
rscasny over 1 year ago

Hi All. I have been talking to a sponsor who's interested in having element14 roadtest one of its FPGA boards. We are looking for someone who is familiar with AMD products and design tools. It's about a $700 board and have significant capabilities. Let me describe the high points below. If you are interested, please vote in the poll.

imageHere's some basic information on the AUBoard 15P FPGA Development Kit:

The board is based on the AMD AMD Artix UltraScale+ 15P FPGA, featuring 170K logic cells, 12 GTH transceivers, 7.6 Mb on-chip memory, and 576 DSP slices. It's a great board to experiment with and learn the AMD Artix UltraScale+ Tm architecture. Whether you want to explore bare metal, RTOS, or Linux software, the AUBoard 15P will give you a solid base foundation to experiment.

The board also features 2GB of ISSI DDR4 and non-volatile configuration and boot from the 512Mb of ISSI QSPI Flash. A Microchip PHY enables the 10/100 Ethernet interface. A microUSB port provides on-board JTAG/UART access. A Renesas clock generator and ECS crystal oscillators provide clocking to the AU15P device, GTH transceivers, JTAG, and communication interfaces. All 12 GTH transceivers are brought out to SFP+ 10 GbE Ethernet (1), HDMI 2.0 Rx & Tx (3), and PCIe end point (4) interfaces and FMC (4) I/O expansion.

A temperature sensor from STMicroelectronics adds environmental data to the system. Additionally, 80 FPGA I/Os are exposed through the Samtec connectors for FMC LPC high-speed expansion and one Click BoardTm site.

Target applications include: Embedded vision, Embedded processing, Wired communications, Prototyping & experimentation, and Industrial networking

Are are some of the features:

  • AMD Xilinx Artix UltraScale+ 15P FPGA
    170K logic cells
    12 GTH transceivers
    7.6 Mb on-chip memory
    576 DSP slices
    ISSI 2GB DDR4 memory
  • ISSI 512Mb QSPI Flash memory (configuration and boot)
  • PetaLinux BSP available for download
  • Microchip 10/100 MII wired Ethernet PHY and MAC ID EEPROM
  • Renesas and TDK power devices
  • On-board JTAG and UART debug interface
  • STMicroelectronics temperature sensor
  • Expansion with 1 Click site and FMC LPC enabled by Samtec connectors
  • 4x GTH transceivers on the FMC
  • User RGB and monochrome LEDs
  • User slide and push button switches
  • HDMI 2.0 Rx & Tx
  • SFP+ 10Gb Ethernet
  • PCIe Gen. 4 x4 end point interface

Here are some links to documentation:

  • Product Brief 
  • Getting Started Guide
  • Manufacturer's Page 

RoadTester Poll

  • Sign in to reply
  • Cancel
Parents
  • manihatn
    manihatn over 1 year ago

    Thanks for sharing the opportunity rscasny .  I would definitely be interested to road test the AUBoard 15P FPGA Development Kit as I have the time and skill to do a thorough review. As a FPGA design engineer, I have a lot of experience working with FPGA's across devices from Spartan to modern SoC (Zynq, Zynq MPSoC, K26). I have also experience working with PCIe based high speed networking cards (designing and benchmarking), video and image processing. I am confident I can put the SFP+ to good use in terms of building a 10G ethernet subsystem and extending it to be used as a switch or a network interface card that can modify the header or payload information. I can also test the video subsystem part of the design by write some IP to display some custom patterns on the HDMI or take in a USB camera feed, do some image processing and display it on to HDMI. Based on the time provided for the road test I am happy to go into greater depth. 

    Being an active member of the element14 FPGA community, I have participated across multiple FPGA design challenges and road tests. This will be a great opportunity to explore a PCIe based FPGA, share the knowledge with the community and feedback to Tria. I very much look forward to being a road tester if given the opportunity.       

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • manihatn
    manihatn over 1 year ago

    Thanks for sharing the opportunity rscasny .  I would definitely be interested to road test the AUBoard 15P FPGA Development Kit as I have the time and skill to do a thorough review. As a FPGA design engineer, I have a lot of experience working with FPGA's across devices from Spartan to modern SoC (Zynq, Zynq MPSoC, K26). I have also experience working with PCIe based high speed networking cards (designing and benchmarking), video and image processing. I am confident I can put the SFP+ to good use in terms of building a 10G ethernet subsystem and extending it to be used as a switch or a network interface card that can modify the header or payload information. I can also test the video subsystem part of the design by write some IP to display some custom patterns on the HDMI or take in a USB camera feed, do some image processing and display it on to HDMI. Based on the time provided for the road test I am happy to go into greater depth. 

    Being an active member of the element14 FPGA community, I have participated across multiple FPGA design challenges and road tests. This will be a great opportunity to explore a PCIe based FPGA, share the knowledge with the community and feedback to Tria. I very much look forward to being a road tester if given the opportunity.