RoadTests & Reviews
  • Products & Partners
  • More
RoadTests & Reviews
RoadTest Forum Weller Micro Soldering Kit and Filtration Unit - first test with the nano solder kit
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 20 replies
  • Subscribers 2742 subscribers
  • Views 2082 views
  • Users 0 members are here
  • weller
Related

Weller Micro Soldering Kit and Filtration Unit - first test with the nano solder kit

Jan Cumps
Jan Cumps 9 months ago

The kits for the Weller Micro Soldering Kit and Filtration Unit arrived. I used the pico/nano solder iron to replace an tiny resistor on a multilayer board.

The pico/nano iron is 40 W, and I used a 1.3 x 0.4 mm chisel tip. Lead free solder and the iron at 350° C

image

I need magnification to do this kind of work. When soldering, I used the magnifying glasses. The pcb photo was taken with a phone through the loupe:

image

  • Sign in to reply
  • Cancel
Parents
  • Jan Cumps
    Jan Cumps 8 months ago

    The difference in size of the two irons and their tips:

    image

    With the nano iron, your hand is way closer to the solder point..

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur 8 months ago in reply to Jan Cumps

    Are both attachments provided in the kit? Mine is fairly simple to change, I would assume the same on the new model?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps 8 months ago in reply to colporteur

    there are 3 irons in the kit:

    micro: WTMP handle, 3 different tips

    nano: WTPP handle, 4 different tips

    rework tweezers: WTMT handle, 2 different tweezers

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps 8 months ago in reply to OwainM

    The part with the tweezers plugs in / out. It's a click system - no screws or clamps.

    image

    Once plugged in, the tweezer part fits firm into the handle.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Jan Cumps
    Jan Cumps 8 months ago in reply to OwainM

    The part with the tweezers plugs in / out. It's a click system - no screws or clamps.

    image

    Once plugged in, the tweezer part fits firm into the handle.