RoadTests & Reviews
  • Products & Partners
  • More
RoadTests & Reviews
RoadTest Forum What data would you acquire with this?
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 11 replies
  • Subscribers 2747 subscribers
  • Views 737 views
  • Users 0 members are here
  • Digital I/O
  • USB-6421
  • ni
  • mioDAQ
  • data acquisition
  • Analogue I/O
Related

What data would you acquire with this?

OwainM
OwainM 2 months ago

We're appraising the USB-6421 for a RoadTest and would appreciate some member input.
image

It's USB Type-C powered and has analogue and digital IO and 4 counters, analogue input channels with four input range settings between ± 200 mV to ± 10 V. The analogue output channels have an update rate of 250 kS/s/ch at up to ± 10 V.

It's compatible with some free data acquisition software from NI, but also has some professional software to use with it that's also available.

The full product specifications are available below:



Thanks for reading and commenting below

  • Sign in to reply
  • Cancel
Parents
  • meera_hussien
    meera_hussien 2 months ago

    I would like to use this in a project that i am currently working on to study the power and the performance of the motor and also the current consumption as well. This would be a handy tool to capture all the data that would be necessary for the studies. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • meera_hussien
    meera_hussien 2 months ago

    I would like to use this in a project that i am currently working on to study the power and the performance of the motor and also the current consumption as well. This would be a handy tool to capture all the data that would be necessary for the studies.