RoadTests & Reviews
  • Products & Partners
  • More
RoadTests & Reviews
RoadTest Forum Can you test this cellular, cell-less and GNSS Development Kit?
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 2745 subscribers
  • Views 66 views
  • Users 0 members are here
  • 5g
  • lte-m
  • Non-Cellular 5G
  • Pre-certified
  • development kit
  • DECT NR+
  • nordic semiconductor
  • Cell-less 5G
  • gnss
  • nb-iot
Related

Can you test this cellular, cell-less and GNSS Development Kit?

OwainM
OwainM 7 hours ago

We're thinking of offering the Nordic nRF9151-DK up for review.

It's a pre-certified development kit with an on-board LTE-M, NB-IoT and DECT NR+ antenna based around the nRF9191 System-in-Package.

image

It supports an array of LTE Bands, and also includes user programmable LEDs, push buttons and is Arduino Uno Shield Compatible.

There's on-board sim slots for nano/4FF SIM cards, MFF2 SIM footprint to support plug-in and soldered (e)SIMs and the kit includes a SIM card that is pre-loaded free data.

I've dropped the product brief in below:


The DECT NR+ cell-less 5G is interesting to me, but it looks like more than one of these kits might be required to review that capability, or the testing hardware may be quite specialised and isn't something a lot of members have access to.


  • Sign in to reply
  • Cancel
Parents
  • shabaz
    shabaz 5 hours ago

    Interesting device! And nice to see the trend of interesting microcontrollers/SoCs in recent RoadTests.

    I too am curious to hear about DECT NR+, but as you suggest, it would need more hardware (i.e. at least one more of these dev-boards), plus probably there is a learning curve.

    However, some of these wireless modules are good to even just get the main microcontroller up-and-running, even if the wireless is not exercised much initially. Part of the battle is just getting the development environment and SDK in place, so even that is good to see, because some manufacturers make it easier than others.

    The GNSS would be another low-hanging fruit, fairly easy to get going with that normally. Then LTE-M would require a small purchase to test for real (some firms sell a SIM for not a lot of £/$). The DECT NR+ may well be the hardest bit to get going with initially.

    I'd love to try it out but am backlogged, and I still have a small review to write which I promised e14 ages ago : ( plus I'm very unfamiliar with Nordic Semi devices. I think there are element14 users familiar with Nordic Semi development tools.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz 5 hours ago

    Interesting device! And nice to see the trend of interesting microcontrollers/SoCs in recent RoadTests.

    I too am curious to hear about DECT NR+, but as you suggest, it would need more hardware (i.e. at least one more of these dev-boards), plus probably there is a learning curve.

    However, some of these wireless modules are good to even just get the main microcontroller up-and-running, even if the wireless is not exercised much initially. Part of the battle is just getting the development environment and SDK in place, so even that is good to see, because some manufacturers make it easier than others.

    The GNSS would be another low-hanging fruit, fairly easy to get going with that normally. Then LTE-M would require a small purchase to test for real (some firms sell a SIM for not a lot of £/$). The DECT NR+ may well be the hardest bit to get going with initially.

    I'd love to try it out but am backlogged, and I still have a small review to write which I promised e14 ages ago : ( plus I'm very unfamiliar with Nordic Semi devices. I think there are element14 users familiar with Nordic Semi development tools.