RoadTests & Reviews
  • Products & Partners
  • More
RoadTests & Reviews
RoadTest Forum Can you test this cellular, cell-less and GNSS Development Kit?
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 2745 subscribers
  • Views 66 views
  • Users 0 members are here
  • 5g
  • lte-m
  • Non-Cellular 5G
  • Pre-certified
  • development kit
  • DECT NR+
  • nordic semiconductor
  • Cell-less 5G
  • gnss
  • nb-iot
Related

Can you test this cellular, cell-less and GNSS Development Kit?

OwainM
OwainM 7 hours ago

We're thinking of offering the Nordic nRF9151-DK up for review.

It's a pre-certified development kit with an on-board LTE-M, NB-IoT and DECT NR+ antenna based around the nRF9191 System-in-Package.

image

It supports an array of LTE Bands, and also includes user programmable LEDs, push buttons and is Arduino Uno Shield Compatible.

There's on-board sim slots for nano/4FF SIM cards, MFF2 SIM footprint to support plug-in and soldered (e)SIMs and the kit includes a SIM card that is pre-loaded free data.

I've dropped the product brief in below:


The DECT NR+ cell-less 5G is interesting to me, but it looks like more than one of these kits might be required to review that capability, or the testing hardware may be quite specialised and isn't something a lot of members have access to.


  • Sign in to reply
  • Cancel
Parents
  • MATRIX7878
    MATRIX7878 5 hours ago

    I actually created a board with this chip.  I used it to create a 5G tablet.  Just for fun, I'll post the link here for people to see (I even made a datasheet for it): The Engineering Tablet - Share Project - PCBWay.  I would definitely see if I could use AT commands with it to make calls and stuff like that.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • MATRIX7878
    MATRIX7878 5 hours ago

    I actually created a board with this chip.  I used it to create a 5G tablet.  Just for fun, I'll post the link here for people to see (I even made a datasheet for it): The Engineering Tablet - Share Project - PCBWay.  I would definitely see if I could use AT commands with it to make calls and stuff like that.