Hello Ventuno_Q road testers, Hi cstanton , Hi OwainM , Hi ralphjy ,
The three MIPI-CSI ports on the Ventuno_Q board are now functional.

The RPI IMX219 V2 NoIR cameras are compatible. Qualcomm and Arduino have updated the firmware and drivers.
As a preliminary note: I flashed the Ubuntu OS onto the board with the latest operating system over the weekend.
This proved to be helpful.
https://docs.arduino.cc/tutorials/ventuno-q/flash-image/
Flashing the Ventuno_Q (not on UNO_Q) wipes ALL installed files and settings, as it resets everything to factory defaults. Afterward, you have an up-to-date Ubuntu OS and AppLab version 0.9.0.
The system then automatically checks online for updates (for both AppLab and the OS) and prompts you to install them.
In the interest of a controlled test, I chose to update only AppLab first—this allowed for better oversight, as an OS update would have required downloading approximately 1 GB of data.
My goal was to quickly verify that the ports were working.
Testing the MIPI/CSI ports:
The process was remarkably straightforward.
Connect the cameras while the board is powered off, then plug in the power and boot up the system.
Next, install the streamer by following the instructions provided on the Arduino documentation page for MIPI/CSI cameras.
https://docs.arduino.cc/tutorials/ventuno-q/mipi-csi-camera/
2 sudo apt upgrade -y
3 sudo apt install gstreamer1.0-plugins-qcom -y // (here is the version 1.0 of the gstreamer; actual is version 1.24.2
Probe success line.This means the camera is identified and is working.


Gerald
---