RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Please Read: An Important RoadTest Program Change
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 91 replies
  • Subscribers 2754 subscribers
  • Views 9702 views
  • Users 0 members are here
Related

Please Read: An Important RoadTest Program Change

rscasny
rscasny over 9 years ago

This is the third virtual "fireside chat" that I'm writing regarding the RoadTest Program. For this one, I'd like to roll out a RoadTest Program change and explain why the change is occurring.

 

To start, I'd like to share a snippet of an email I received yesterday from a vendor who participates in the RoadTest Program:

 

"We received only 13% reviews back from the RoadTests we sponsored in 2016. I would like to know the status of each of these roadtests. Are the missing reviews still being pursued? I would also like to know if the members that failed to post a review are now being flagged so we do not chose them again."

 

It was not pleasant to respond to. I had to eat "humble pie," as we say in the US, when I responded to this vendor.

 

To solve the problem, I decided I don't want to go down the road of suspending members from the RoadTest program. Suspensions sound too much like the hard rules of the military. I was in the Navy for 10 years and I didn't like tough rules back then, but I knew they were necessary given the reality of uncomfortable shipboard conditions and potentially dangerous operations we were participating in.

 

But this is a community. It should be a place to have some fun, meet new people, network professionally, be a mentor, or get mentored. Suspending people just is the wrong road to follow.

 

The way I've chosen to resolve the problem is the program change.

 

RoadTest application reports will soon include whether a specific applicant has completed all of his/her previous RoadTest reviews. I'm told by our developers this is very easy to do. We will provide this information to the vendor with a RoadTester's application. The supplier will make the decision where to select the RoadTester or not. Given the above comment by the supplier, I think the answer is self-evident.

 

Now, this change will probably cause me more work. If someone were flagged, I will have to check to see if that person is on a current RoadTest and it's before the due date of the official review. I surely don't want to penalize a conscientious RoadTester. I will also have to ensure there are not any extenuating circumstances that have caused the person not to write the review, i.e., sickness, family issues.

 

I am ambivalent about this whole thing. There are many RoadTesters who are doing a fantastic job. But a 13% success rate is not successful. I really have no choice but to implement this change.

 

Sincerely,

 

Randall Scasny

RoadTest Program Manager

  • Sign in to reply
  • Cancel
Parents
  • Fred27
    Fred27 over 9 years ago

    Wouldn't a tiered system of promotion rather than punishment be easier to manage and more difficult to game with multiple accounts, etc.? By which I mean that if you complete a good review on a less popular piece of equipment you then become eligible for the more popular items. This should increase both the quality and return rate of reviews. It's frustrating for community members to miss out on a road test you think you could do a good job on and see either no reviews appear or pointless ones. When someone is supposed to review an oscilloscope and decides pictures of their dog are relevant, you know it's just typing for the sake of typing.

     

    Personally, I only apply for testing something that I believe I can review well and that I have a particular interest in. I imagine most people are the same, but I'm sure there are people who just think "ooh. free stuff."

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Fred27
    Fred27 over 9 years ago

    Wouldn't a tiered system of promotion rather than punishment be easier to manage and more difficult to game with multiple accounts, etc.? By which I mean that if you complete a good review on a less popular piece of equipment you then become eligible for the more popular items. This should increase both the quality and return rate of reviews. It's frustrating for community members to miss out on a road test you think you could do a good job on and see either no reviews appear or pointless ones. When someone is supposed to review an oscilloscope and decides pictures of their dog are relevant, you know it's just typing for the sake of typing.

     

    Personally, I only apply for testing something that I believe I can review well and that I have a particular interest in. I imagine most people are the same, but I'm sure there are people who just think "ooh. free stuff."

    • Cancel
    • Vote Up +4 Vote Down