RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Please Read: An Important RoadTest Program Change
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 91 replies
  • Subscribers 2754 subscribers
  • Views 9669 views
  • Users 0 members are here
Related

Please Read: An Important RoadTest Program Change

rscasny
rscasny over 9 years ago

This is the third virtual "fireside chat" that I'm writing regarding the RoadTest Program. For this one, I'd like to roll out a RoadTest Program change and explain why the change is occurring.

 

To start, I'd like to share a snippet of an email I received yesterday from a vendor who participates in the RoadTest Program:

 

"We received only 13% reviews back from the RoadTests we sponsored in 2016. I would like to know the status of each of these roadtests. Are the missing reviews still being pursued? I would also like to know if the members that failed to post a review are now being flagged so we do not chose them again."

 

It was not pleasant to respond to. I had to eat "humble pie," as we say in the US, when I responded to this vendor.

 

To solve the problem, I decided I don't want to go down the road of suspending members from the RoadTest program. Suspensions sound too much like the hard rules of the military. I was in the Navy for 10 years and I didn't like tough rules back then, but I knew they were necessary given the reality of uncomfortable shipboard conditions and potentially dangerous operations we were participating in.

 

But this is a community. It should be a place to have some fun, meet new people, network professionally, be a mentor, or get mentored. Suspending people just is the wrong road to follow.

 

The way I've chosen to resolve the problem is the program change.

 

RoadTest application reports will soon include whether a specific applicant has completed all of his/her previous RoadTest reviews. I'm told by our developers this is very easy to do. We will provide this information to the vendor with a RoadTester's application. The supplier will make the decision where to select the RoadTester or not. Given the above comment by the supplier, I think the answer is self-evident.

 

Now, this change will probably cause me more work. If someone were flagged, I will have to check to see if that person is on a current RoadTest and it's before the due date of the official review. I surely don't want to penalize a conscientious RoadTester. I will also have to ensure there are not any extenuating circumstances that have caused the person not to write the review, i.e., sickness, family issues.

 

I am ambivalent about this whole thing. There are many RoadTesters who are doing a fantastic job. But a 13% success rate is not successful. I really have no choice but to implement this change.

 

Sincerely,

 

Randall Scasny

RoadTest Program Manager

  • Sign in to reply
  • Cancel
Parents
  • geralds
    geralds over 9 years ago

    Hi Randall,

     

    for me, I'm absolut agree with you.

    I think that many can be misunderstood  because many of Road Testers are not so fit with the English language.

    Me too a bit, because my language is German, so i translate difficult sentences every time with the (e.g. google) translator.

    I hope so much all of you can understand me with my jargon mishmash "Kauderwelsch".

     

    If i write here the review is this enough or have i write also via email to an email address?

    Because i never have seen some email address what you meant above -  "reviews back to the sponsors."

    How goes the review back to the sponsors? - with our review here written in element14 road test, or with an email from you?

    Are the sponsors reading here the reviews?

     

    Best Regards

    Gerald

    ---

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • rscasny
    rscasny over 9 years ago in reply to geralds

    Gerald,

     

    Thanks for asking the question because the answer has to do with an understanding of our internal processes.

     

    So, you go online and complete a RoadTest application.

     

    After the enrollment period of the RoadTest, all the applications are aggregated or put together in a spreadsheet. This spreadsheet has additional fields. Such as how many points have you earned as a community member or whether you have submitted all your RoadTest reviews. It is this spreadhseet that will get forwarded to the supplier.

     

    Randall

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • Cancel
  • awneil
    awneil over 9 years ago in reply to rscasny

    Randall Scasny wrote:

     

    This spreadsheet has additional fields. Such as how many points have you earned as a community member...

     

    Isn't there a chicken-and-egg problem there: if you don't have enough points, you don't get picked - so you can't gain the points to get picked ... ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • hlipka
    hlipka over 9 years ago in reply to awneil

    In the questionnaire for the finalist its stated as "Have you completed all of your previous RoadTests Reviews for which you  were selected as an official RoadTester? (Yes, No, In progress, First  Time Applicant)".

    Maybe the number of completed road tests would be interesting, but probably Randall can find that out more easily than I can do image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • awneil
    awneil over 9 years ago in reply to hlipka

    Hendrik Lipka wrote:

     

    Some people have a good chance of always have an open review when applying

    Having an open review should not be an issue - it's having an overdue review (or reviews) that's the problem.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • hlipka
    hlipka over 9 years ago in reply to rscasny

    The number of completed reviews is also interesting. Some people have a good chance of always have an open review when applying, just because they participate in so many road tests. (Happens also to me - I still have an open review for the Raspberry DIN rail enclosure, while applying for BBBW road test). But I guess this is where Randall does the manual corrections to the spreadsheet.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • hlipka
    hlipka over 9 years ago in reply to rscasny

    The number of completed reviews is also interesting. Some people have a good chance of always have an open review when applying, just because they participate in so many road tests. (Happens also to me - I still have an open review for the Raspberry DIN rail enclosure, while applying for BBBW road test). But I guess this is where Randall does the manual corrections to the spreadsheet.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • hlipka
    hlipka over 9 years ago in reply to awneil

    In the questionnaire for the finalist its stated as "Have you completed all of your previous RoadTests Reviews for which you  were selected as an official RoadTester? (Yes, No, In progress, First  Time Applicant)".

    Maybe the number of completed road tests would be interesting, but probably Randall can find that out more easily than I can do image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • awneil
    awneil over 9 years ago in reply to hlipka

    Hendrik Lipka wrote:

     

    Some people have a good chance of always have an open review when applying

    Having an open review should not be an issue - it's having an overdue review (or reviews) that's the problem.

    • Cancel
    • Vote Up +5 Vote Down