Products
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
RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Please Read: An Important RoadTest Program Change
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 91 replies
  • Subscribers 2754 subscribers
  • Views 9750 views
  • Users 0 members are here
Related

Please Read: An Important RoadTest Program Change

rscasny
rscasny over 9 years ago

This is the third virtual "fireside chat" that I'm writing regarding the RoadTest Program. For this one, I'd like to roll out a RoadTest Program change and explain why the change is occurring.

 

To start, I'd like to share a snippet of an email I received yesterday from a vendor who participates in the RoadTest Program:

 

"We received only 13% reviews back from the RoadTests we sponsored in 2016. I would like to know the status of each of these roadtests. Are the missing reviews still being pursued? I would also like to know if the members that failed to post a review are now being flagged so we do not chose them again."

 

It was not pleasant to respond to. I had to eat "humble pie," as we say in the US, when I responded to this vendor.

 

To solve the problem, I decided I don't want to go down the road of suspending members from the RoadTest program. Suspensions sound too much like the hard rules of the military. I was in the Navy for 10 years and I didn't like tough rules back then, but I knew they were necessary given the reality of uncomfortable shipboard conditions and potentially dangerous operations we were participating in.

 

But this is a community. It should be a place to have some fun, meet new people, network professionally, be a mentor, or get mentored. Suspending people just is the wrong road to follow.

 

The way I've chosen to resolve the problem is the program change.

 

RoadTest application reports will soon include whether a specific applicant has completed all of his/her previous RoadTest reviews. I'm told by our developers this is very easy to do. We will provide this information to the vendor with a RoadTester's application. The supplier will make the decision where to select the RoadTester or not. Given the above comment by the supplier, I think the answer is self-evident.

 

Now, this change will probably cause me more work. If someone were flagged, I will have to check to see if that person is on a current RoadTest and it's before the due date of the official review. I surely don't want to penalize a conscientious RoadTester. I will also have to ensure there are not any extenuating circumstances that have caused the person not to write the review, i.e., sickness, family issues.

 

I am ambivalent about this whole thing. There are many RoadTesters who are doing a fantastic job. But a 13% success rate is not successful. I really have no choice but to implement this change.

 

Sincerely,

 

Randall Scasny

RoadTest Program Manager

  • Sign in to reply
  • Cancel
  • rachaelp
    rachaelp over 9 years ago in reply to rscasny

    Hi Randall,

     

    Randall Scasny wrote:

     

    Rachael,

     

    You have a sound argument. Clearly, it appears some folks consider RoadTests a giveaway program, which it is not. We really need your professional opinions. My concern is perhaps if the delinquent roadtest reviews see they can make up their reviews, they can change their ways. We'll see how things play out. I need to improve the review percentage.

     

    Thanks for your participation in the community.

     

    Randall

     

    If this is the case they they will contact you or be responsive when you try to contact them. Any who are completely uncontactable shouldn't be cut any slack. You need to give them firm deadlines to get back to you when you contact them and let them know the consequences if you don't hear from them. For example:

     

    Dear XYZ, Your road test review of ABC is well overdue and I have not had any communication from you despite numerous attempts to contact you. I expect to receive either your submitted road test no later than DD-MM-YYYY, or an email detailing your extenuating circumstances no later than DD-MM-YYYY. Failure to do so will result in your suspension from all current and future road test programs and require the immediate return of any equipment you received. We will arrange a courier for the return of the equipment at our expense.

     

    If you don't do something like this I can't see how the situation can significantly improve and eventually suppliers will stop being willing to partake in programs like this.

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 9 years ago

    I for one agree something needs to be done. I will not apply for a road test if I feel I can not complete it on the given schedule and also If I feel the award would be better served being given to someone else, and even then as was the case with the INA301 I may still post reviews or tutorials to help out the participants, its fun and most of the TMs like to help, it's what we're all about.

    I do get bothered though when an applicant gets a nice Scope or Analyzer or other more expensive product and then the next time you hear from them is when the next road test comes up., no review, no posts or anything in between

     

    I think your choice of dealing with this is very generous and hopefully will help weed out the collect and run types, it still won't stop the new members who sole purpose is to get a product and run, for this the only thing I have seen suggested in the past was to put min points limits on the "Better" product so if you have not been participating in the community then you dont get to review the "Big Toys" till you do.

     

    One thing that would also be bad though is if someone just posts a regurgitation of the product specs or simply a box opening, I have seen many instances in the past where the review is well to put it bluntly. Not a review. they go along the lines of "I opened the box...... it was a nice box...... The product looked like its picture and seems to meet the published specification....." you get the idea.

     

    So while I respect you measures, there may need to be more of a "Quality" check of the review, especially if from a very new member with no history of participation. A Post in the Review form does not necessarily mean a review has been done."

     

    That's my 2 cents (Pennies worth image )

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • Cancel
  • rscasny
    rscasny over 9 years ago in reply to rachaelp

    Rachael,

     

    You have a sound argument. Clearly, it appears some folks consider RoadTests a giveaway program, which it is not. We really need your professional opinions. My concern is perhaps if the delinquent roadtest reviews see they can make up their reviews, they can change their ways. We'll see how things play out. I need to improve the review percentage.

     

    Thanks for your participation in the community.

     

    Randall

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • rachaelp
    rachaelp over 9 years ago in reply to kas.lewis

    Kas Lewis wrote:

     

    I feel part of the problem of an outright suspension in that those selfish people (wether few in number or not) could generate a new account with ease. If you keep them here maybe they won't create a new account. It's a thought and I must admit not a very well thought out one, But there is always the chance of people creating multiple accounts for the larger more interesting road tests or after getting suspended creating new accounts and doing the same thing all over again.

     

    K

    I would hope that there was more to receiving expensive free kit than just a user account on this forum. I would expect there would be some sort of verification of who they are, real name, address, contact details, some form of ID as proof of who they are etc. Much harder to have lots of duplicates of all that information. I also don't think we were talking about suspending their accounts on here, just their eligibility for signing up for road tests.

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • kas.lewis
    kas.lewis over 9 years ago in reply to rachaelp

    I feel part of the problem of an outright suspension in that those selfish people (wether few in number or not) could generate a new account with ease. If you keep them here maybe they won't create a new account. It's a thought and I must admit not a very well thought out one, But there is always the chance of people creating multiple accounts for the larger more interesting road tests or after getting suspended creating new accounts and doing the same thing all over again.

     

    K

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • rachaelp
    rachaelp over 9 years ago

    Randall Scasny wrote:

     

    To solve the problem, I decided I don't want to go down the road of suspending members from the RoadTest program. Suspensions sound too much like the hard rules of the military. I was in the Navy for 10 years and I didn't like tough rules back then, but I knew they were necessary given the reality of uncomfortable shipboard conditions and potentially dangerous operations we were participating in.

     

    But this is a community. It should be a place to have some fun, meet new people, network professionally, be a mentor, or get mentored. Suspending people just is the wrong road to follow.

    Hi Randall,

     

    I see where you are coming from but to my mind If a member who hasn't completed a particular RoadTest, hasn't contacted you to tell you in advance of their extenuating circumstances, isn't responsive when you contact them, etc, then I don't personally see the downside in suspending them from the program. There has to be some way to dissuade people from signing up just to get free stuff and if its the price we have to pay to ensure suppliers continue to offer their products for free in exchange for a review then so be it.

     

    I was going to say we don't want a few selfish people spoiling it for everybody else, but sadly it seems it's not a few, for this particular supplier it's 87% which quite frankly is shameful, and those people (unless they have a very good reason why they haven't completed their reviews) should be utterly ashamed of themselves.

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up +10 Vote Down
    • Sign in to reply
    • Cancel
  • geralds
    geralds over 9 years ago in reply to rscasny

    Randall,

     

    thank you for the helpful information.

     

    Best Regards,

    Gerald

    ---

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • rscasny
    rscasny over 9 years ago in reply to geralds

    Gerald,

     

    That is correct. You only need to complete the review on the form. It will have a star that is half yellow/ half white. That designates it is an official review. that's what we look for.

     

    thanks.

     

    Randall

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • geralds
    geralds over 9 years ago in reply to rscasny

    Hi Randall,

     

    Many Thanks.

    That was what did not know - the spreadsheet behind it. I thought this but i was not sure.

    So, if I understood: a review written here in element14 (with the quote of the rank table) is the concrete reference for the suppliers.
    There is no need to write the review by e-mail. Correct?

     

    Best Regards

    Gerald

    ---

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rscasny
    rscasny over 9 years ago in reply to geralds

    Gerald,

     

    Thanks for asking the question because the answer has to do with an understanding of our internal processes.

     

    So, you go online and complete a RoadTest application.

     

    After the enrollment period of the RoadTest, all the applications are aggregated or put together in a spreadsheet. This spreadsheet has additional fields. Such as how many points have you earned as a community member or whether you have submitted all your RoadTest reviews. It is this spreadhseet that will get forwarded to the supplier.

     

    Randall

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • Cancel
<>