Products
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
RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Please Read: An Important RoadTest Program Change
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 91 replies
  • Subscribers 2754 subscribers
  • Views 9737 views
  • Users 0 members are here
Related

Please Read: An Important RoadTest Program Change

rscasny
rscasny over 9 years ago

This is the third virtual "fireside chat" that I'm writing regarding the RoadTest Program. For this one, I'd like to roll out a RoadTest Program change and explain why the change is occurring.

 

To start, I'd like to share a snippet of an email I received yesterday from a vendor who participates in the RoadTest Program:

 

"We received only 13% reviews back from the RoadTests we sponsored in 2016. I would like to know the status of each of these roadtests. Are the missing reviews still being pursued? I would also like to know if the members that failed to post a review are now being flagged so we do not chose them again."

 

It was not pleasant to respond to. I had to eat "humble pie," as we say in the US, when I responded to this vendor.

 

To solve the problem, I decided I don't want to go down the road of suspending members from the RoadTest program. Suspensions sound too much like the hard rules of the military. I was in the Navy for 10 years and I didn't like tough rules back then, but I knew they were necessary given the reality of uncomfortable shipboard conditions and potentially dangerous operations we were participating in.

 

But this is a community. It should be a place to have some fun, meet new people, network professionally, be a mentor, or get mentored. Suspending people just is the wrong road to follow.

 

The way I've chosen to resolve the problem is the program change.

 

RoadTest application reports will soon include whether a specific applicant has completed all of his/her previous RoadTest reviews. I'm told by our developers this is very easy to do. We will provide this information to the vendor with a RoadTester's application. The supplier will make the decision where to select the RoadTester or not. Given the above comment by the supplier, I think the answer is self-evident.

 

Now, this change will probably cause me more work. If someone were flagged, I will have to check to see if that person is on a current RoadTest and it's before the due date of the official review. I surely don't want to penalize a conscientious RoadTester. I will also have to ensure there are not any extenuating circumstances that have caused the person not to write the review, i.e., sickness, family issues.

 

I am ambivalent about this whole thing. There are many RoadTesters who are doing a fantastic job. But a 13% success rate is not successful. I really have no choice but to implement this change.

 

Sincerely,

 

Randall Scasny

RoadTest Program Manager

  • Sign in to reply
  • Cancel
  • gregoryfenton
    gregoryfenton over 9 years ago

    Having been chosen as a finalist for the first road test after this system has been in place (which I hope will have the desired outcome of more roadtests completed) I have an issue with the first question.

     

    Congratulations. This means you are part of the short list of applicants who will be forwarded to the supplier for their selection of the official winners.

    Your application will be forwarded as well as your answers to the following questions. Please answer the following questions by replying to this message:

    1. What is your work status? (Full time job, part time job, student, not working/retired)?

    I do not see how telling a third party my current work situation is relevant in any way, shape or form.

     

    I don't want to seem negative in any way, could the option "choose not to say" be added?

     

    Regards

     

    Greg

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • awneil
    awneil over 9 years ago in reply to hlipka

    Hendrik Lipka wrote:

     

    Some people have a good chance of always have an open review when applying

    Having an open review should not be an issue - it's having an overdue review (or reviews) that's the problem.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • hlipka
    hlipka over 9 years ago in reply to rscasny

    The number of completed reviews is also interesting. Some people have a good chance of always have an open review when applying, just because they participate in so many road tests. (Happens also to me - I still have an open review for the Raspberry DIN rail enclosure, while applying for BBBW road test). But I guess this is where Randall does the manual corrections to the spreadsheet.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 9 years ago in reply to Robert Peter Oakes

    I have seen many instances in the past where the review is well to put it bluntly. Not a review

    I recall one where the comments were along the lines  .... "Is that all".

     

     

    Randall has a plan going forward so we should see where it goes.

    I'm pretty sure there will be one or two 'mistakes' but if thats all then it is a step up from the 13% rate for one supplier.

     

     

    Mark

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 9 years ago in reply to awneil

    Not really, points are earned through community participation, not just from people liking or participating in a Road Test.

    Overall there are far more points to be earned through normal community participation, posting Howtos, Tech Tips, Helping out other members, sharing your project with the rest of us etc etc.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • rscasny
    rscasny over 9 years ago in reply to awneil

    Andy,

     

    I can see where you may interpret what I said in that way. But it's not an entirely correct assertion.

     

    We will be looking at a variety of factors to determine who will win the RoadTest and become an official Roadtester. Completing all your previous reviews is a big one but not everything. The number of points suggests to me a level of participation in the community. However, points aren't everything. I have seen some RoadTester who have accrued 3000 points yet haven't written their reviews. Basically, it's not a chicken or the egg; rather, it's competition. Not much different than winning a new job but on a smaller level. Finally, if I see someone who has a great idea and doesn't have a lot of points, I may arrange a time to speak with the person on the phone to get a better idea of who I am providing a free product to. It is your job to prove to me that you want to do it, you are committed and you value our program.

     

    Sincerely,

     

    Randall Scasny

    RoadTest Program Manager

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Cancel
  • awneil
    awneil over 9 years ago in reply to rscasny

    Randall Scasny wrote:

     

    This spreadsheet has additional fields. Such as how many points have you earned as a community member...

     

    Isn't there a chicken-and-egg problem there: if you don't have enough points, you don't get picked - so you can't gain the points to get picked ... ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • awneil
    awneil over 9 years ago in reply to michaelkellett

    Yes - that's what I was thinking

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 9 years ago in reply to awneil

    I thinks that's a good idea and it avoids the problem of bad-listing someone accidentally and them never knowing about it.

     

    MK

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • awneil
    awneil over 9 years ago

    I think the enrolment form should highlight to the applicant that they have outstanding reports - and point out that this will count against them.

     

    It would also allow the applicant to explain any extenuating circumstances ...

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
<>