RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum UPDATE: What do you think of this Debugger, the ULINKplus -- Power-Aware Debugging
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 17 replies
  • Subscribers 2751 subscribers
  • Views 3186 views
  • Users 0 members are here
  • debugger
  • ulinkplus
Related

UPDATE: What do you think of this Debugger, the ULINKplus -- Power-Aware Debugging

rscasny
rscasny over 9 years ago

When I saw this I thought it was interesting - a multi-core debugger with integrated power measurement and additional test I/O pins allowing you to control automated tests. You can control the processor, set breakpoints, and read/write memory contents, all while the processor is running at full speed.  Nice for ultra-low power applications, sensitive hardware and software validation for getting system and long battery life.  What do you think?

 

image

Here's some specs:

  • Wide target voltage range: 1.2V - 5.5V
  • Electrical isolation from the target system is integrated up to 1 kV
  • USB 2.0 High-Speed connection using the CMSIS-DAP debug protocol
  • USB powered (no power supply required)
  • 10-pin (0.05") - Cortex Debug Connector
  • Hot-plugging to running targets

 

Devices Supported:

  • JTAG support for ARM Cortex processors
  • Serial Wire Debug (SWD) support for all ARM Cortex-M processors
  • Serial Wire Viewer (SWV) support for all ARM Cortex-M processors

 

More information

ULINKplus Overview

ARM blog on the ULINKplus

 

NEW! Ulinkplus Webinar on Nov 30, 2017

 

Interested in learning more about the ULINKplus? Then sign up for the the webinar here

  • Sign in to reply
  • Cancel
Parents
  • balearicdynamics
    balearicdynamics over 9 years ago

    Honestly? I have not idea of what is the price but I love it. In an industrial context the engineering lab (firmware coding and debugging) it is frequently stabilised on the company choices to this sort of jolly maybe not an essential component. I mean, the lab already has those debugging instruments needed for test all the characteristics usually are available.

     

    In a more flexible context instead I think this is unvaluable, especially for the I/O pins for testing automation. Very useful when there is not only one micro controller but depending on the project and the kind of application some micro maybe adopted instead of others. I have spent a lot of time in past to build test automation stuff to check this of that different micro controller for a certain feature instead of another.

     

    I am curious to see how this device can work the automated testing software like Jensen. But I think to all the possibilities for the entire scenario opened by this tool.

     

    Reading the documentation also in power critical applications it sounds extremely useful. The first impression is thumb up

     

    Enrico

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • balearicdynamics
    balearicdynamics over 9 years ago

    Honestly? I have not idea of what is the price but I love it. In an industrial context the engineering lab (firmware coding and debugging) it is frequently stabilised on the company choices to this sort of jolly maybe not an essential component. I mean, the lab already has those debugging instruments needed for test all the characteristics usually are available.

     

    In a more flexible context instead I think this is unvaluable, especially for the I/O pins for testing automation. Very useful when there is not only one micro controller but depending on the project and the kind of application some micro maybe adopted instead of others. I have spent a lot of time in past to build test automation stuff to check this of that different micro controller for a certain feature instead of another.

     

    I am curious to see how this device can work the automated testing software like Jensen. But I think to all the possibilities for the entire scenario opened by this tool.

     

    Reading the documentation also in power critical applications it sounds extremely useful. The first impression is thumb up

     

    Enrico

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Workshopshed
    Workshopshed over 9 years ago in reply to balearicdynamics

    You have a link for Jensen?