RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum UPDATE: What do you think of this Debugger, the ULINKplus -- Power-Aware Debugging
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 17 replies
  • Subscribers 2751 subscribers
  • Views 3192 views
  • Users 0 members are here
  • debugger
  • ulinkplus
Related

UPDATE: What do you think of this Debugger, the ULINKplus -- Power-Aware Debugging

rscasny
rscasny over 9 years ago

When I saw this I thought it was interesting - a multi-core debugger with integrated power measurement and additional test I/O pins allowing you to control automated tests. You can control the processor, set breakpoints, and read/write memory contents, all while the processor is running at full speed.  Nice for ultra-low power applications, sensitive hardware and software validation for getting system and long battery life.  What do you think?

 

image

Here's some specs:

  • Wide target voltage range: 1.2V - 5.5V
  • Electrical isolation from the target system is integrated up to 1 kV
  • USB 2.0 High-Speed connection using the CMSIS-DAP debug protocol
  • USB powered (no power supply required)
  • 10-pin (0.05") - Cortex Debug Connector
  • Hot-plugging to running targets

 

Devices Supported:

  • JTAG support for ARM Cortex processors
  • Serial Wire Debug (SWD) support for all ARM Cortex-M processors
  • Serial Wire Viewer (SWV) support for all ARM Cortex-M processors

 

More information

ULINKplus Overview

ARM blog on the ULINKplus

 

NEW! Ulinkplus Webinar on Nov 30, 2017

 

Interested in learning more about the ULINKplus? Then sign up for the the webinar here

  • Sign in to reply
  • Cancel
Parents
  • michaelkellett
    michaelkellett over 9 years ago

    My opinion on this will depend very much on the price and the detail of the specification.

     

    Current measuring for micros is very, very difficult because of the huge dynamic range needed -  ideally at least 500mA to 1uA to cover, for example, the latest STM32F4xxx from ST. That means a resolution down to less than 100nA so you need a 24 bit ADC with 1 lsb error or fancy range range changing - the UlinkPlus has 16 bit ADC and comes in a little plastic box so I expect compromises in the current measuring area !

     

    Keil/ARMs prices for debug tools are traditionally high and I think that the simple Ulink market has been lost to them because of this - what I hope is that they will put this new device out at a sightly lower price point than the standard Ulink2 ie about£150 but I can't find prices on the web

     

    MK

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • tekmeister
    tekmeister over 9 years ago in reply to michaelkellett

    I suspect this won't be cheap. I went looking for the price earlier but didn't find one.

     

    With regard to current measuring, it looks like the sense resistor is external (ie. you provide it), so it might actually be able to measure quite accurately

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • tekmeister
    tekmeister over 9 years ago in reply to michaelkellett

    I suspect this won't be cheap. I went looking for the price earlier but didn't find one.

     

    With regard to current measuring, it looks like the sense resistor is external (ie. you provide it), so it might actually be able to measure quite accurately

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • rachaelp
    rachaelp over 9 years ago in reply to tekmeister

    tekmeister wrote:

     

    With regard to current measuring, it looks like the sense resistor is external (ie. you provide it), so it might actually be able to measure quite accurately

    It's more a case of the dynamic range required. If you need to be able to measure very low currents in the range of uA when the MCU is in a low power mode but then also be able to measure hundreds of mA when it wakes up and is busy doing things you may not be able to select a resistor which will give reasonable accuracy at both ends of that range.

     

    Best Regards,

     

    Rachael