RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum UPDATE: What do you think of this Debugger, the ULINKplus -- Power-Aware Debugging
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 17 replies
  • Subscribers 2751 subscribers
  • Views 3196 views
  • Users 0 members are here
  • debugger
  • ulinkplus
Related

UPDATE: What do you think of this Debugger, the ULINKplus -- Power-Aware Debugging

rscasny
rscasny over 9 years ago

When I saw this I thought it was interesting - a multi-core debugger with integrated power measurement and additional test I/O pins allowing you to control automated tests. You can control the processor, set breakpoints, and read/write memory contents, all while the processor is running at full speed.  Nice for ultra-low power applications, sensitive hardware and software validation for getting system and long battery life.  What do you think?

 

image

Here's some specs:

  • Wide target voltage range: 1.2V - 5.5V
  • Electrical isolation from the target system is integrated up to 1 kV
  • USB 2.0 High-Speed connection using the CMSIS-DAP debug protocol
  • USB powered (no power supply required)
  • 10-pin (0.05") - Cortex Debug Connector
  • Hot-plugging to running targets

 

Devices Supported:

  • JTAG support for ARM Cortex processors
  • Serial Wire Debug (SWD) support for all ARM Cortex-M processors
  • Serial Wire Viewer (SWV) support for all ARM Cortex-M processors

 

More information

ULINKplus Overview

ARM blog on the ULINKplus

 

NEW! Ulinkplus Webinar on Nov 30, 2017

 

Interested in learning more about the ULINKplus? Then sign up for the the webinar here

  • Sign in to reply
  • Cancel
Parents
  • Workshopshed
    Workshopshed over 9 years ago

    Probably a bit advanced for what I typically do but I can see it being a great aid for troubleshooting pesky problems. I suspect I'll eventually get to the point of inline debugging but mostly I'm in the serial print and flash LED camp.

     

    If the question is, "would you like to see someone road test this" then I'd say yes.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Workshopshed
    Workshopshed over 9 years ago

    Probably a bit advanced for what I typically do but I can see it being a great aid for troubleshooting pesky problems. I suspect I'll eventually get to the point of inline debugging but mostly I'm in the serial print and flash LED camp.

     

    If the question is, "would you like to see someone road test this" then I'd say yes.