RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum How Would You RoadTest This Wireless Power Dev Kit?
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 28 replies
  • Subscribers 2761 subscribers
  • Views 4407 views
  • Users 0 members are here
  • scasny
  • wurth electronik
  • rohm
  • dev kit
  • 760308mp
  • wireless power
  • energy_power
Related

How Would You RoadTest This Wireless Power Dev Kit?

rscasny
rscasny over 9 years ago

I'm often contacted my suppliers who are considering to participate in the RoadTest program. They ask me a lot of questions about the program and which products are the best to RoadTest. Well, it depends, right? Test equipment garners a lot of interest. So do SBCs or anything to do with IoT. So when I was contacted about this Wireless Power Dev Kit for a future RoadTest, I looked up what content the community already had on the topic. There is a some content, as expected, since wireless power solutions are only sure to grow. But I don't recall doing a RoadTest on this type of product, or at least recently. I just wondered how it would be RoadTested. So, here's my question: How would your Roadtest it?image

 

Here's a few facts about the product:

  • It's the result of the joint collaboration of Wurth Elektronik and Rohm Semiconductor.
  • It's used in devices with a large number of mating cycles to avoid connector damage such as smartphones, tablets, portable media players.
  • It comes with 5 parts: Transmitter module, Receiver module, LED load module, Quick start guide, Power adapter with EU, US and UK adapter.

 

Here's a few specs:

  • Plug & play wireless power design kit, medium power solution
  • Qi standard version 1.2 compliant with extended power profile
  • Based on the transmitter type MP-A7
  • Excellent performance due to use of litz wire coil
  • Operating temperature range from -20°C up to +105°C
  • Inductance of 12µH at 125KHz/10mA, Q-factor of 33 at 125KHz/10mA
  • Maximum rated current of 3A at ΔT = 40K, saturation current of 6A (typ)

 

More Information

Datasheet

Product Info

 

Here's a few More Photos:

image

 

image

 

image

  • Sign in to reply
  • Cancel
Parents
  • ipv1
    ipv1 over 9 years ago

    This is an upgrade to the kit we got for the BeyonD the Phone and how. Some of us received some coils to make our own circuits and it was fun. Maybe someone could use variable coil sizes and do an analysis on the efficiency and how the circuit should be changed or remain the same.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • ipv1
    ipv1 over 9 years ago

    This is an upgrade to the kit we got for the BeyonD the Phone and how. Some of us received some coils to make our own circuits and it was fun. Maybe someone could use variable coil sizes and do an analysis on the efficiency and how the circuit should be changed or remain the same.

    • Cancel
    • Vote Up +3 Vote Down