RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum How Would You RoadTest This Wireless Power Dev Kit?
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 28 replies
  • Subscribers 2761 subscribers
  • Views 4407 views
  • Users 0 members are here
  • scasny
  • wurth electronik
  • rohm
  • dev kit
  • 760308mp
  • wireless power
  • energy_power
Related

How Would You RoadTest This Wireless Power Dev Kit?

rscasny
rscasny over 9 years ago

I'm often contacted my suppliers who are considering to participate in the RoadTest program. They ask me a lot of questions about the program and which products are the best to RoadTest. Well, it depends, right? Test equipment garners a lot of interest. So do SBCs or anything to do with IoT. So when I was contacted about this Wireless Power Dev Kit for a future RoadTest, I looked up what content the community already had on the topic. There is a some content, as expected, since wireless power solutions are only sure to grow. But I don't recall doing a RoadTest on this type of product, or at least recently. I just wondered how it would be RoadTested. So, here's my question: How would your Roadtest it?image

 

Here's a few facts about the product:

  • It's the result of the joint collaboration of Wurth Elektronik and Rohm Semiconductor.
  • It's used in devices with a large number of mating cycles to avoid connector damage such as smartphones, tablets, portable media players.
  • It comes with 5 parts: Transmitter module, Receiver module, LED load module, Quick start guide, Power adapter with EU, US and UK adapter.

 

Here's a few specs:

  • Plug & play wireless power design kit, medium power solution
  • Qi standard version 1.2 compliant with extended power profile
  • Based on the transmitter type MP-A7
  • Excellent performance due to use of litz wire coil
  • Operating temperature range from -20°C up to +105°C
  • Inductance of 12µH at 125KHz/10mA, Q-factor of 33 at 125KHz/10mA
  • Maximum rated current of 3A at ΔT = 40K, saturation current of 6A (typ)

 

More Information

Datasheet

Product Info

 

Here's a few More Photos:

image

 

image

 

image

  • Sign in to reply
  • Cancel
Parents
  • Fred27
    Fred27 over 9 years ago

    Mix and match testing is definitely the way to go. I'm sure the paired kit works well and the designers have published their own accurate and detailed specs. There's not really much benefit just repeating this.

     

    What really matters is how interoperable it is. I've got two Qi chargers and 4 devices - including a couple of Nook eReaders that have had a cheap eBay receivers hacked in. This is the reality of how these devices have to work.

     

    It might be interesting to see if it could be combined with NFC or whether the two would interfere with each other. I can't actually think of a good use case right now but it sort of seems logical to be charging a device and communicating with it at the same time. Maybe a data logger that's being recharged and uploading data at the same time?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Fred27
    Fred27 over 9 years ago

    Mix and match testing is definitely the way to go. I'm sure the paired kit works well and the designers have published their own accurate and detailed specs. There's not really much benefit just repeating this.

     

    What really matters is how interoperable it is. I've got two Qi chargers and 4 devices - including a couple of Nook eReaders that have had a cheap eBay receivers hacked in. This is the reality of how these devices have to work.

     

    It might be interesting to see if it could be combined with NFC or whether the two would interfere with each other. I can't actually think of a good use case right now but it sort of seems logical to be charging a device and communicating with it at the same time. Maybe a data logger that's being recharged and uploading data at the same time?