RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum I am Creating a List of Industrial RoadTesters. Are You Interested?
  • Blogs
  • RoadTest Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 35 replies
  • Subscribers 2669 subscribers
  • Views 4395 views
  • Users 0 members are here
  • scasny
Related

I am Creating a List of Industrial RoadTesters. Are You Interested?

rscasny
rscasny over 8 years ago

Greetings RoadTesters!

 

As we ramp up offering more and more RoadTests, one of the new issues that's come up is more industrial suppliers would like their products RoadTested. This has posed a bit of a challenge for me. The community's RoadTest program has historically featured dev boards and the like for makers or electronic engineers. As such, a lot of the members of the RoadTest group are part of the makewr/bench tech/EDE type.image

 

To solve the problem, I would like to create a list of members who would be interested in being an industrial RoadTesters. How will it work? Honestly, I don't have all the details worked out. The two scenarios I see are: (A) run a regular RoadTest and if I don't get applicants, I would contact members of the Industrial RoadTest list, or (B) treat this group like a RoadTest by Invitation. I surely don't want to eliminate any member who would like to RoadTest an industrial product, but I guess I am saying I need a backup plan.

 

Who Am I looking for? I am interested in finding members who do have industrial tech or engineering experience. People who have worked in manufacturing or have been field engineers or even technicians who who worked around machinery. Even people who have worked as electrical engineers in instrumentation, wastewater treatment plants, oil/gas industry, electrical power generation, etc. If you have this background, and are interested in being placed on this call list, please message me at rscasny.image

 

Once again, I surely don't want to exclude any member from RoadTesting an industrial product even though they may not have the background. But I am being tasked by my bosses to prepare the RoadTest group for testing a broader selection of products. If you have any questions or if you have any comments, feel free to add them below.

 

 

Sincerely,

 

Randall Scasny

RoadTest Program Manager

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 8 years ago in reply to rscasny +6
    Hi Randall, That's an interesting product, the VeriSafe, by the looks of it. I will put in an application for the Verisafe and the Megger, since they both look useful, for labs at my workplace (server…
  • dougw
    dougw over 8 years ago +3
    It is not clear why this list of industrial road testers would apply or rather why they wouldn't apply if it was just a regular road test format. I guess if they don't need to do a big proposal it makes…
  • balearicdynamics
    balearicdynamics over 8 years ago in reply to Former Member +3
    Hi Lucie, correct what you say. Not all people can do it. But I also consider that not all people can write C code as well as work with proficient python scripts for embedded devices and more and more…
Parents
  • ipv1
    ipv1 over 8 years ago

    Hi rscasny,

    In terms of Industrial experience, I have spent a few years making control and test equipment however I currently do not have access to such a test setup. For testing a PID controller for example, I have a muffle furnace that is capable of 1300'C for sintering compounds but it is definitely not industrial grade. I think there are two categories here to be considered;

     

    a. People with experience in testing such stuff that do not necessarily require a setup. e.g. Automotive stuff like CAN modules, SCADA, ModBUS, etc. These can be tested in a humble DIY lab but requires the tested to have prior knowledge of the standard and extreme cases.

     

    b.  People with access to industrial test equipment such as EMI measurement tools, enchoic chambers and even high voltage sources. e.g. High frequency, RF, Microwave, Optical amplifier, fibres, etc

     

    c. People with some experience and just enough equipment. e.g the PID controller.

     

    Since a roadtest does not provide a formal certification to a product, it could be worth the effort to add people who have already used or are in possession of a competing product. Of course not all suppliers will like that idea unless they are confident about their offering.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • ipv1
    ipv1 over 8 years ago

    Hi rscasny,

    In terms of Industrial experience, I have spent a few years making control and test equipment however I currently do not have access to such a test setup. For testing a PID controller for example, I have a muffle furnace that is capable of 1300'C for sintering compounds but it is definitely not industrial grade. I think there are two categories here to be considered;

     

    a. People with experience in testing such stuff that do not necessarily require a setup. e.g. Automotive stuff like CAN modules, SCADA, ModBUS, etc. These can be tested in a humble DIY lab but requires the tested to have prior knowledge of the standard and extreme cases.

     

    b.  People with access to industrial test equipment such as EMI measurement tools, enchoic chambers and even high voltage sources. e.g. High frequency, RF, Microwave, Optical amplifier, fibres, etc

     

    c. People with some experience and just enough equipment. e.g the PID controller.

     

    Since a roadtest does not provide a formal certification to a product, it could be worth the effort to add people who have already used or are in possession of a competing product. Of course not all suppliers will like that idea unless they are confident about their offering.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Children
  • balearicdynamics
    balearicdynamics over 8 years ago in reply to ipv1

    Inderpreet, you perfectly depicted the scenario!

     

    This is the reason that I think that every product should be pre-evaluated before someone of us is reasonably sure to be able to do an independent test moving away from the bare obvious.

     

    The only thing my though differs is about how to test in industrial environment. If we should test a temperature sensor, just to make an example, it is not important to have a muffle but to setup a lab small platform with high temperature emitter instead of cold etc. This makes things easier in a lot of cases without losing value to the test.

     

    Enrico

    • Cancel
    • Vote Up +2 Vote Down