RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum RoadTest Reviews: A Discussion About The Rating System
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 19 replies
  • Subscribers 2752 subscribers
  • Views 3016 views
  • Users 0 members are here
  • scasny
Related

RoadTest Reviews: A Discussion About The Rating System

rscasny
rscasny over 9 years ago

For any RoadTest Review, the reviewer not only provides his or her personal take on the product being reviewed but also a numbered ranking (10-point scale) for 6 different questions.

 

Here is a random example:

 

image

My gut feeling is that  I haven't clarified well enough what the 10-point scale means. As a result, there may be a lack of certainty when giving a grade. In addition, a lot of RoadTesters grade these questions in similar ways. So, I'd like to revisit our grading system. To start here's my idea:

 

  • 10 points: Outstanding
  • 9 points: Very Good Satisfaction
  • 8 points: Good Satisfaction
  • 7 points: Adequate but had to work through some programs
  • 6 points: Needs Work
  • 5 points  Barely Satisfactory
  • 4 points: Below Average
  • 3 points: Unsatisfactory
  • 2 Points:Totally Unsatisfactory
  • 1 point: Time to Rethink

 

I'd like to get the RoadTester Group's opinions on the rating system. Do you think it needs more clarification? Keep it the way it is?

 

Go ahead and suggest your own. Perhaps the problem is that we need to ask different questions?

 

Sincerely,

 

Randall Scasny

RoadTest Program Manager

  • Sign in to reply
  • Cancel
Parents
  • gecoz
    gecoz over 9 years ago

    The point system proposed surely is a great improvement, as it establishes a clearly defined rating criteria, making it a reference for all.

    The problem I see with it is that most people are accustomed either to "academic-based" scoring systems, like the ones where 10 is excellence, 5 or 6 is sufficient, and anything less is unsatisfactory, or to  "expectation-based" rating systems, where 10 is given when the product/service meets the expectation and anything less than 10 denotes some negative, and if you define a different rating system, unfortunately people tend to "fall-back" to the system they are most used to, creating some ambiguity in the valutation.

    For a 5 star rating system, despite the way the star criteria are set, the most common interpretation is as a "meeting expectation" feedback system, where 5 stars = expectation fully met (NB: not necessarily meaning "excellence"), and anything less than 5 star usually has some negative element in it. Expectation are normally built by gathering information beforehand (i.e. reading the marketing and technical documentation in our case).

     

    Personally, I too would go for a 5 star rating system, something like:

     

    5 - Expectation fully met

    4 - Most important expectation met

    3 - Basic expectation met

    2 - Basic expectation NOT met

    1 - No expectation met

    0 - Not rated (impossible to assess)

     

    Besides being visual and very simple, this kind of rating is also very common, therefore most people are already accustomed to it.

    Fabio.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 9 years ago in reply to gecoz

    I have to disagree with you here Fabio, one of the concepts of modern quality assurance is the idea of "Surprise and Delight" - the feeling the customer has when the product does something good that they did not expect. The scoring system should allow for this possibility.

     

    For example, in the 70s when I was involved with a HiFi company it was not usual to provide connectors with an amplifier. We packed  power leads for the switched mains outlets, speaker connectors and some phono plugs, the idea being that it didn't cost much but really scored  a hit with every customer who would otherwise have needed a ttrip to the shops before they could try the new toy.

     

    I think this should have earned an extra star !

     

    (Recently the "Surprise and Delight" concept has got  a bit distorted and morphed somewhat into promotional activity - but the original concept is still valid.)

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • gecoz
    gecoz over 9 years ago in reply to michaelkellett

    Hi Michael,

    Perhaps I didn't explain myself well. Although I can see where you are coming from, and in principle I agree with you, my point was about what is in place now and how it is used. Unfortunately when you look around, just about all the star rating systems use the top rating for meeting expectation, and any less of a 5 rating is interpreted as somehow negative. Element14 could do differently, and use the "exceed" expectation for the 5 star, but by doing so it would generate ambiguity in the valutation, as a product meeting all the expectation would have to score only a 4 star.

    I suppose what I'm trying to say is when choosing a rating system, I think we should take into account how people are using other feedback systems out there, so that the system is more familiar and the valutation is less susceptible of interpretation.

    Fabio.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 9 years ago in reply to michaelkellett

    I too consider the top score as more of 'delights the customer' rather than 'no room for improvement', because technology always evolves.

    There are cultural differences too, for example I sometimes see the 5-point scoring results for presentations, and invariably the score is higher presented in the US, whereas it is always slightly lower in Europe. Or there is the one mean person who scores 1/5 for everything because they attended the wrong presentation for them, and the others scored 5/5 : ) So the 5 points or stars means something different depending on the audience. With the product reviews some are scored extremely low but then it becomes apparent from the text that the user didn't apply the product to the same use-cases as expected, or had some difficulties which are unique to him/her and would not generally apply to that product, e.g. faulty item.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 9 years ago in reply to michaelkellett

    I too consider the top score as more of 'delights the customer' rather than 'no room for improvement', because technology always evolves.

    There are cultural differences too, for example I sometimes see the 5-point scoring results for presentations, and invariably the score is higher presented in the US, whereas it is always slightly lower in Europe. Or there is the one mean person who scores 1/5 for everything because they attended the wrong presentation for them, and the others scored 5/5 : ) So the 5 points or stars means something different depending on the audience. With the product reviews some are scored extremely low but then it becomes apparent from the text that the user didn't apply the product to the same use-cases as expected, or had some difficulties which are unique to him/her and would not generally apply to that product, e.g. faulty item.