RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum What's Stopping You Building Your Next Project with an FPGA? (Please, Don't Blame the Cost!)
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 100 replies
  • Subscribers 2757 subscribers
  • Views 12337 views
  • Users 0 members are here
  • scasny
  • xilinx
  • fpgafeatured
Related

What's Stopping You Building Your Next Project with an FPGA? (Please, Don't Blame the Cost!)

rscasny
rscasny over 8 years ago

The community does a ton of projects with MCUs. If they do the job for you, that's great. But the element14 community is about learning, experimenting and roadtesting. In this spirit, I am proposing that you should try building your next project with an FPGA (SoC), if it suits the application, of course. What's stopping you? Oh, some members have voiced the cost issue. Granted, some FPGAs do cost a lot. But chip manufacturers are rolling out economical chipsets that most makers, pro-makers or experienced hobbyists can afford. (If you can't, then apply to a RoadTest and if you win you can get a dev board for FREE.) I think FPGA / SoCs will move into a more important place for electronic designers, especially for IoT applications. Perhaps it's time to experiement with one. What's stopping you?

 

Here's a link to a current roadtest:Digilent ARTY S7 Dev Board (Xilinx Spartan 7)   Apply today!

 

Randall Scasny

RoadTest Program Manager

  • Sign in to reply
  • Cancel
Parents
  • ntewinkel
    ntewinkel over 8 years ago

    I just noticed FPGAs can be used for HDMI output, which would be a very interesting use case: fpga4fun.com - HDMI

    But the assembly-like language used on that example website makes me run for the hills.

     

    My hope is something like this: Basic Arduino to output video and sound (https://playground.arduino.cc/Main/TVout ), with the outputs connected to an FPGA that converts it to HDMI.

     

    The ultimate goal is to show images and play mp3s from an SD card on a TV using an HDMI connection.

     

    Would this be possible? (question is to the FPGA experts image re the HDMI part - I can handle the Arduino to TV-out and Audio-out part)

     

    -Nico

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • ntewinkel
    ntewinkel over 8 years ago

    I just noticed FPGAs can be used for HDMI output, which would be a very interesting use case: fpga4fun.com - HDMI

    But the assembly-like language used on that example website makes me run for the hills.

     

    My hope is something like this: Basic Arduino to output video and sound (https://playground.arduino.cc/Main/TVout ), with the outputs connected to an FPGA that converts it to HDMI.

     

    The ultimate goal is to show images and play mp3s from an SD card on a TV using an HDMI connection.

     

    Would this be possible? (question is to the FPGA experts image re the HDMI part - I can handle the Arduino to TV-out and Audio-out part)

     

    -Nico

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
Children
  • michaelkellett
    michaelkellett over 8 years ago in reply to ntewinkel

    The Kamami Maximator board has HDMI socket. Its powered by an Altera MAX10 fpga and fairly cheap and simple.

     

    I reviewed this board in a blog on E14 which you should be able to find.

     

    If you try coding it in VHDL I'll possibly be able to help if you get stuck.

    The link you gave is using Verilog. You won't find that VHDL looks any more obvious but its pedantic insistence on being told exactly what to do will save you from many traps that Verilog will entice you into.

     

     

    MK

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Cancel
  • jc2048
    jc2048 over 8 years ago in reply to ntewinkel

    Have you tried the Arduino TVout? By the looks of that page, it can only be one bit per pixel and big, chunky pixels at that.

     

    The FPGA could do the HDMI part at 25MHz quite easily. You'd need to look at the signalling levels on the HDMI - I'm not familiar with it hardware-wise, but you could probably work with one of the many differential standards that FPGAs provide. It would need a proper PCB.

     

    A better architecture (than having the Arduino struggling to produce the video timing) would be to have a frame store in the FPGA (or a memory attached to the FPGA if there wasn't enough internal RAM going spare) that got scanned and output. The Arduino would then write to it once (setting or resetting pixels) and the FPGA would then deal with refreshing the display. It would be similar to an old CGA graphics card in a PC, except you'd be designing the graphics chip. The interface between the Arduino and the FPGA could be whatever you wanted, but SPI might work well.

     

    Another fun idea, taking a further step back in history, would be to do a vector display. The Arduino could write a sequence of line end-point pairs to the FPGA and the FPGA could draw the vectors on-screen (you might decide to get the Arduino to sort them into a favourable order first). You could then do Asteroids in it's original form.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • ntewinkel
    ntewinkel over 8 years ago in reply to ntewinkel

    ps, I do realize that a Raspberry Pi zero would make this very easy image