RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum What's Stopping You Building Your Next Project with an FPGA? (Please, Don't Blame the Cost!)
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 100 replies
  • Subscribers 2756 subscribers
  • Views 12405 views
  • Users 0 members are here
  • scasny
  • xilinx
  • fpgafeatured
Related

What's Stopping You Building Your Next Project with an FPGA? (Please, Don't Blame the Cost!)

rscasny
rscasny over 8 years ago

The community does a ton of projects with MCUs. If they do the job for you, that's great. But the element14 community is about learning, experimenting and roadtesting. In this spirit, I am proposing that you should try building your next project with an FPGA (SoC), if it suits the application, of course. What's stopping you? Oh, some members have voiced the cost issue. Granted, some FPGAs do cost a lot. But chip manufacturers are rolling out economical chipsets that most makers, pro-makers or experienced hobbyists can afford. (If you can't, then apply to a RoadTest and if you win you can get a dev board for FREE.) I think FPGA / SoCs will move into a more important place for electronic designers, especially for IoT applications. Perhaps it's time to experiement with one. What's stopping you?

 

Here's a link to a current roadtest:Digilent ARTY S7 Dev Board (Xilinx Spartan 7)   Apply today!

 

Randall Scasny

RoadTest Program Manager

  • Sign in to reply
  • Cancel
Parents
  • DAB
    DAB over 8 years ago

    If I had a good project for FPGA's I would use them.

     

    To give you a perspective, back in the 1970's I did Bit Slice design, which is kind of the precursor to FPGA's.

     

    If I was a newbie, I would first buy a Cypress Semiconductor PSOC board and use their software to learn how to build complex hardware circuits using their programmable devices, both analog and digital.

     

    You can consider the PSOC as a simple FPGA device.  It will give you a feel for the level of detail you need to understand and provide you with useful experience in implementing custom hardware.

     

    After you learn the terminology and get a feel for the design process, then you can move on to a full FPGA with a better understanding of what you are getting into.

     

    Make no mistake, you will have to be able to deal with a large amount of detailed information to go just beyond the tutorials.

     

    Why bother?  The reward in capability is HUGE!  Once you get proficient, you can make all kinds of complex hardware devices within the FPGA constraints.  You are now in the upper echelon of makers.

     

    If you are a good maker, have the basic electronics background and like to work on complex problems, then an FPGA can be very rewarding.  You will forever free from having to look for just the right chip.  You can roll your own.

     

    DAB

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • DAB
    DAB over 8 years ago

    If I had a good project for FPGA's I would use them.

     

    To give you a perspective, back in the 1970's I did Bit Slice design, which is kind of the precursor to FPGA's.

     

    If I was a newbie, I would first buy a Cypress Semiconductor PSOC board and use their software to learn how to build complex hardware circuits using their programmable devices, both analog and digital.

     

    You can consider the PSOC as a simple FPGA device.  It will give you a feel for the level of detail you need to understand and provide you with useful experience in implementing custom hardware.

     

    After you learn the terminology and get a feel for the design process, then you can move on to a full FPGA with a better understanding of what you are getting into.

     

    Make no mistake, you will have to be able to deal with a large amount of detailed information to go just beyond the tutorials.

     

    Why bother?  The reward in capability is HUGE!  Once you get proficient, you can make all kinds of complex hardware devices within the FPGA constraints.  You are now in the upper echelon of makers.

     

    If you are a good maker, have the basic electronics background and like to work on complex problems, then an FPGA can be very rewarding.  You will forever free from having to look for just the right chip.  You can roll your own.

     

    DAB

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
Children
  • johnbeetem
    johnbeetem over 8 years ago in reply to DAB

    DAB  wrote:

     

    To give you a perspective, back in the 1970's I did Bit Slice design, which is kind of the precursor to FPGA's.

     

    If I was a newbie, I would first buy a Cypress Semiconductor PSOC board and use their software to learn how to build complex hardware circuits using their programmable devices, both analog and digital.

     

    You can consider the PSOC as a simple FPGA device.  It will give you a feel for the level of detail you need to understand and provide you with useful experience in implementing custom hardware.

     

    I wouldn't recommend PSoC as a good starter device.  PSoC is really an on-chip collection of devices, which are connected by a routing network.  Those devices include a CPU (ARM Cortex M0/M3 for PSoC 4/5), a bunch of PLAs, a bunch of 8-bit bit-slice ALUs, a bunch of analog, and so on.  You don't need to learn about all the devices, but at the very least you need to learn about the CPU and the logic if you want to do FPGA-like things.  So it's at least two learning curves.

     

    For starting out, I'd go with a pure FPGA board like the Lattice iCEstick, which has a built-in USB programmer, 5 LEDs, UART connections, and enough header pins to get started.  It seems to be readily available these days for around $25.  There are plenty of other choices as well: Not-as-expensive FPGA Boards