RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum What's Stopping You Building Your Next Project with an FPGA? (Please, Don't Blame the Cost!)
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 100 replies
  • Subscribers 2757 subscribers
  • Views 12367 views
  • Users 0 members are here
  • scasny
  • xilinx
  • fpgafeatured
Related

What's Stopping You Building Your Next Project with an FPGA? (Please, Don't Blame the Cost!)

rscasny
rscasny over 8 years ago

The community does a ton of projects with MCUs. If they do the job for you, that's great. But the element14 community is about learning, experimenting and roadtesting. In this spirit, I am proposing that you should try building your next project with an FPGA (SoC), if it suits the application, of course. What's stopping you? Oh, some members have voiced the cost issue. Granted, some FPGAs do cost a lot. But chip manufacturers are rolling out economical chipsets that most makers, pro-makers or experienced hobbyists can afford. (If you can't, then apply to a RoadTest and if you win you can get a dev board for FREE.) I think FPGA / SoCs will move into a more important place for electronic designers, especially for IoT applications. Perhaps it's time to experiement with one. What's stopping you?

 

Here's a link to a current roadtest:Digilent ARTY S7 Dev Board (Xilinx Spartan 7)   Apply today!

 

Randall Scasny

RoadTest Program Manager

  • Sign in to reply
  • Cancel
Parents
  • sa-penguin
    sa-penguin over 8 years ago

    What's stopping my design? The cost.

     

    Sure, Dev boards are getting to real good prices [I have an Arty-S7 sitting on my desk] - that's not all the cost.  There's also time costs, space costs - and prototype costs.

     

    My latest ideas tend to involve RF in some form (from satellite weather decoding to general SDR) and getting high frequency signals digitized is NOT a trivial task. Some of the PMOD connectors on the S7 are "high speed" - but how high is high?

    I have to design / make / order custom PCB's for high speed ADC's then populate them, plug them in, and THEN I get to determine if my design is flawed, or the Dev board just can't handle the speed I'm clocking in data.

    The S7 claims internal clocking over 450MHz. Can the Dev board handle a 400MHz ADC / DAC?  300MHz? 200?  150? 120?

    Can I really afford to keep making PCB's to test a design, even assuming I can get the actual chips as free (or cheap) samples? That's... daunting.

     

    Not sure what the answer is. Higher speed connectors, with specified speed ratings, would sure help. As to the format- coax? optic fibre? JESD204? The only thing I know for sure is the "Arduino" connector isn't enough when you want serious speed - and serious speed is the principle reason for changing from a microcontroller design in the first place.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • sa-penguin
    sa-penguin over 8 years ago

    What's stopping my design? The cost.

     

    Sure, Dev boards are getting to real good prices [I have an Arty-S7 sitting on my desk] - that's not all the cost.  There's also time costs, space costs - and prototype costs.

     

    My latest ideas tend to involve RF in some form (from satellite weather decoding to general SDR) and getting high frequency signals digitized is NOT a trivial task. Some of the PMOD connectors on the S7 are "high speed" - but how high is high?

    I have to design / make / order custom PCB's for high speed ADC's then populate them, plug them in, and THEN I get to determine if my design is flawed, or the Dev board just can't handle the speed I'm clocking in data.

    The S7 claims internal clocking over 450MHz. Can the Dev board handle a 400MHz ADC / DAC?  300MHz? 200?  150? 120?

    Can I really afford to keep making PCB's to test a design, even assuming I can get the actual chips as free (or cheap) samples? That's... daunting.

     

    Not sure what the answer is. Higher speed connectors, with specified speed ratings, would sure help. As to the format- coax? optic fibre? JESD204? The only thing I know for sure is the "Arduino" connector isn't enough when you want serious speed - and serious speed is the principle reason for changing from a microcontroller design in the first place.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • michaelkellett
    michaelkellett over 8 years ago in reply to sa-penguin

    I think you are more blocked by the cost of deployment of a high speed ADC than of the FPGA.

     

    You don't say how fast you want the ADC to sample so I can't make very specific comments but I think that you'll have all the same problems and worse trying to interface a fast (250MHz+) ADC to a micro, or to anything.

     

    The next step up of dev boards (from the Arty level) will have some high speed connectors, for example you can buy a Lattice ECP5 VERSA dev board for £250 and it has one full duplex 3.2GHz serdes channel on SMA connectors which would get you 8 bits at 400MHz, or 12 at 250MHz.

    You'll need to make a board for the ADC.

     

    MK