RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum What's Stopping You Building Your Next Project with an FPGA? (Please, Don't Blame the Cost!)
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 100 replies
  • Subscribers 2757 subscribers
  • Views 12314 views
  • Users 0 members are here
  • scasny
  • xilinx
  • fpgafeatured
Related

What's Stopping You Building Your Next Project with an FPGA? (Please, Don't Blame the Cost!)

rscasny
rscasny over 8 years ago

The community does a ton of projects with MCUs. If they do the job for you, that's great. But the element14 community is about learning, experimenting and roadtesting. In this spirit, I am proposing that you should try building your next project with an FPGA (SoC), if it suits the application, of course. What's stopping you? Oh, some members have voiced the cost issue. Granted, some FPGAs do cost a lot. But chip manufacturers are rolling out economical chipsets that most makers, pro-makers or experienced hobbyists can afford. (If you can't, then apply to a RoadTest and if you win you can get a dev board for FREE.) I think FPGA / SoCs will move into a more important place for electronic designers, especially for IoT applications. Perhaps it's time to experiement with one. What's stopping you?

 

Here's a link to a current roadtest:Digilent ARTY S7 Dev Board (Xilinx Spartan 7)   Apply today!

 

Randall Scasny

RoadTest Program Manager

  • Sign in to reply
  • Cancel
Parents
  • Workshopshed
    Workshopshed over 8 years ago

    Hi Randall, I have been thinking about getting started with FPGAs this year. I've got myself a "TinyFPGA". I've gone for the $12 A version which is based on the Lattice Mach XO2-256. That's it's about as simple as they get.

    image

    TinyFPGA A-Series User Guide

     

    The main reasons stopping me getting going.

     

    1) The need for a change of mindshift from sequential programming to logical building blocks.

    2) Learning a whole new toolset to get these things programmed.

    3) Killer app. Given that I can do most things I need using a microcontoller I've no need to swap to FPGAs.

     

    Most of the FPGA dev boards I've seen are of the sledge hammer style. They've got masses of processing power and are suited to things like processing video signals or SDR rather than the kind of things I normally do such as flashing a few LEDs and moving some servos.

     

    I have been looking at the Arty and Digilent tools and there do look to be some good examples and tutorials. I'll maybe be applying if I can thing of a suitable task to roadtest the board.

    • Cancel
    • Vote Up +16 Vote Down
    • Sign in to reply
    • Cancel
  • ntewinkel
    ntewinkel over 8 years ago in reply to Workshopshed

    I agree. For me the reasons are the same as Andy's 1/2/3.

     

    To sum up: "Learning Curve"

     

    ps, Andy - what is the startup time for these things?

    I have a logic application (brake/signal light converter), but it needs to pretty much be instant on (so it can be powered by the brake/signal lights themselves).

     

    -Nico

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Cancel
  • hlipka
    hlipka over 8 years ago in reply to ntewinkel

    FPGA normally read their configuration from an external memory (its non-volatile), so they need some startup time for re-configuration. There are FPGA such as the Spartan-3AN that come with internal Flash memory, but even they must do a re-configuration on startup. Actel has the e.g. the ProAsic3 family for which they claim instant-on functionality, but I did not read through all data sheets to verify that.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 8 years ago in reply to ntewinkel

    If it's any consolation, I haven't actually purchased any FPGA boards  image

     

    I'm scared to count the number of others ... but zero FPGA.

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Cancel
  • ntewinkel
    ntewinkel over 8 years ago in reply to rachaelp

    Thank you, rachaelp and Workshopshed, you've convinced me to make 2018 the year I learn about FPGAs image

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • rachaelp
    rachaelp over 8 years ago in reply to hlipka

    hlipka  wrote:

     

    Actel has the e.g. the ProAsic3 family for which they claim instant-on functionality, but I did not read through all data sheets to verify that.

    I've used these a lot in the past. They are instant on. The flash in these devices is part of the configuration structure of each cell and as soon as the device is powered on, clocks running and it's out of reset it's up and running. If you are talking combinatorial logic, then you don't even need the clocks, as soon as the power is within spec it's working. This is one of the reasons Actel (now MicroSemi) are used so much in aerospace applications.

     

    Best Regards,


    Rachael

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • rachaelp
    rachaelp over 8 years ago in reply to hlipka

    hlipka  wrote:

     

    Actel has the e.g. the ProAsic3 family for which they claim instant-on functionality, but I did not read through all data sheets to verify that.

    I've used these a lot in the past. They are instant on. The flash in these devices is part of the configuration structure of each cell and as soon as the device is powered on, clocks running and it's out of reset it's up and running. If you are talking combinatorial logic, then you don't even need the clocks, as soon as the power is within spec it's working. This is one of the reasons Actel (now MicroSemi) are used so much in aerospace applications.

     

    Best Regards,


    Rachael

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
Children
  • mcb1
    mcb1 over 8 years ago in reply to ntewinkel

    If it's any consolation, I haven't actually purchased any FPGA boards  image

     

    I'm scared to count the number of others ... but zero FPGA.

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Cancel
  • ntewinkel
    ntewinkel over 8 years ago in reply to rachaelp

    Thank you, rachaelp and Workshopshed, you've convinced me to make 2018 the year I learn about FPGAs image

    • Cancel
    • Vote Up +4 Vote Down