RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum How Do You Like Working with the Matrix Creator?
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 13 replies
  • Subscribers 2752 subscribers
  • Views 1989 views
  • Users 0 members are here
  • scasny
Related

How Do You Like Working with the Matrix Creator?

rscasny
rscasny over 8 years ago

If you have experimented with or built a project with the Matrix Creator add-on board for the Raspberry Pi, how are you liking it? I wanted to get some feedback from makers, designers, etc. What have you been building with it? How do you like working with it? Thanks.image

 

Randall Scasny

RoadTest Program Manager

  • Sign in to reply
  • Cancel
Parents
  • mcb1
    mcb1 over 8 years ago

    Like rsc I also hadn't heard of them before.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 8 years ago in reply to mcb1

    Hi Mark!

    There's a short description of it here:

    Embedded World 2017 - (part of) Day 1

    I didn't get to see it in action, but it looked interesting. It is a cross between an IoT gateway, an Amazon Echo and a Sense HAT, combining (and adding to) features of all three pretty much.

    Since it is to be connected to the Pi, there is in theory the opportunity to do local processing as desired, unlike the Echo where any custom apps would need to be in the cloud.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 8 years ago in reply to mcb1

    Hi Mark!

    There's a short description of it here:

    Embedded World 2017 - (part of) Day 1

    I didn't get to see it in action, but it looked interesting. It is a cross between an IoT gateway, an Amazon Echo and a Sense HAT, combining (and adding to) features of all three pretty much.

    Since it is to be connected to the Pi, there is in theory the opportunity to do local processing as desired, unlike the Echo where any custom apps would need to be in the cloud.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • mcb1
    mcb1 over 8 years ago in reply to shabaz

    Thanks

    I'm not convinced about the shape (and size) for anything more than developing your applications.

    Sadly that doesn't really translate into multiple sales, as it would be if you made it something that can be incorporated into the final product by a maker.

     

    It obviously won't fit in any standard enclosures, and any case you add to the Pi is going to make it even harder, unless you use a cable.

     

    It does seem to have a lot of processing power onboard, so I'm not sure why they even bothered with tethering it the Pi.

    image

     

    I can't see me adding one to my collection.

     

    Cheers

    Mark

    • Cancel
    • Vote Up +4 Vote Down