RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Would You Be Interested in RoadTesting an MCU with Integrated NFC
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 22 replies
  • Subscribers 2757 subscribers
  • Views 3135 views
  • Users 0 members are here
  • scasny
Related

Would You Be Interested in RoadTesting an MCU with Integrated NFC

rscasny
rscasny over 8 years ago

Near Field Communication is growing in popularity. It's being used for more than payment processing; and it's even popping up in some of our design challengers' builds (e.g., The Cooker Connector by jschools). For the most part on the element14 community, projects that have included NFC have used an add-on expansion board or shield. But today I was sent some information on an MCU that integrates NFC.

 

It's produced by NXP, and called the LPC8N04 microcontroller.They consider it an entry-level connectivity solution for embedded applications with integrated NFC connectivity. It contains multiple features, including several power-down modes and a selectable CPU frequency of up to 8 MHz for ultra-low power consumption. The peripheral complement includes 32 kB of flash memory, 8 kB of SRAM, 4 kB of EEPROM, one I2C, one SPI/SSP, and up to 12 general purpose I/O pins. Your can read more about it by clicking here.image

 

NXP also says that it enables developers to quickly implement broad-based solutions that leverage system diagnostics or environmental conditions for a smarter tagging experience. With the added benefit of flexible communication modes, you'd have the ability to push data to an LPC8N04 MCU-based edge-node, for example, in device provisioning, configuration or customization. 

 

I think it has interesting possibilities for Board Games, Healthcare Wearables, Robotics, Industrial Uses and, of course, Secure Payments.

 

What do you think?

 

Would you be interested in roadtesting this product? What would you like to test or build?

 

 

  • Sign in to reply
  • Cancel
Parents
  • cghaba
    cghaba over 8 years ago

    On the device page, it says that it is in preproduction phase. What does this mean?

    I saw NFC technology used in Finder digital time switches. One can use the smartphone to program the time switch and load the programmed configuration using NFC. It comes very easy if you have to program several time switches with the same configuration or with a different configuration. Using the smartphone, you can also read the configuration from a time switch, already programmed, and transfer the configuration to another time switch, using NFC.

    I would roadtest it in a project that would create a thermostat that can be programmed using NFC.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • rscasny
    rscasny over 8 years ago in reply to cghaba

    Good Question.

     

    Thanks for asking. My gut feeling is perhaps the page is not up to date. However, I don't know at this moment. But I will check for you on Monday.

     

    Usually, when I am contacted, the product is near release to just after launch.

     

    So, let me get back to you.

     

    Thanks.

     

    Randall Scasny

    RoadTest Program Manager

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • rscasny
    rscasny over 8 years ago in reply to cghaba

    Good Question.

     

    Thanks for asking. My gut feeling is perhaps the page is not up to date. However, I don't know at this moment. But I will check for you on Monday.

     

    Usually, when I am contacted, the product is near release to just after launch.

     

    So, let me get back to you.

     

    Thanks.

     

    Randall Scasny

    RoadTest Program Manager