RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Would You Be Interested in RoadTesting an MCU with Integrated NFC
  • Blogs
  • RoadTest Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 22 replies
  • Subscribers 2669 subscribers
  • Views 2799 views
  • Users 0 members are here
  • scasny
Related

Would You Be Interested in RoadTesting an MCU with Integrated NFC

rscasny
rscasny over 8 years ago

Near Field Communication is growing in popularity. It's being used for more than payment processing; and it's even popping up in some of our design challengers' builds (e.g., The Cooker Connector by jschools). For the most part on the element14 community, projects that have included NFC have used an add-on expansion board or shield. But today I was sent some information on an MCU that integrates NFC.

 

It's produced by NXP, and called the LPC8N04 microcontroller.They consider it an entry-level connectivity solution for embedded applications with integrated NFC connectivity. It contains multiple features, including several power-down modes and a selectable CPU frequency of up to 8 MHz for ultra-low power consumption. The peripheral complement includes 32 kB of flash memory, 8 kB of SRAM, 4 kB of EEPROM, one I2C, one SPI/SSP, and up to 12 general purpose I/O pins. Your can read more about it by clicking here.image

 

NXP also says that it enables developers to quickly implement broad-based solutions that leverage system diagnostics or environmental conditions for a smarter tagging experience. With the added benefit of flexible communication modes, you'd have the ability to push data to an LPC8N04 MCU-based edge-node, for example, in device provisioning, configuration or customization. 

 

I think it has interesting possibilities for Board Games, Healthcare Wearables, Robotics, Industrial Uses and, of course, Secure Payments.

 

What do you think?

 

Would you be interested in roadtesting this product? What would you like to test or build?

 

 

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 8 years ago +4
    NFC is definitely on my list of technologies to become proficient with. It is already widely used but the applications are still in their infancy relative to what will be implemented in the next few years…
  • mcb1
    mcb1 over 8 years ago +3
    Would you be interested in roadtesting this product? I've had a play with NFC and have a phone that has some great NFC features BUT they only supplied two sticker tags, and have no blanks or anything else…
  • shabaz
    shabaz over 8 years ago +2
    Hi Randall, From what I've seen, NXP's NFC technology is second-to-none. There are extremely sophisticated things that can be done with it, I hope the Design Challenge entrants make use of their NFC boards…
Parents
  • awneil
    awneil over 8 years ago

    Yes, definitely interesting ...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • awneil
    awneil over 8 years ago

    Yes, definitely interesting ...