RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Would You Be Interested in RoadTesting an MCU with Integrated NFC
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 22 replies
  • Subscribers 2758 subscribers
  • Views 3121 views
  • Users 0 members are here
  • scasny
Related

Would You Be Interested in RoadTesting an MCU with Integrated NFC

rscasny
rscasny over 8 years ago

Near Field Communication is growing in popularity. It's being used for more than payment processing; and it's even popping up in some of our design challengers' builds (e.g., The Cooker Connector by jschools). For the most part on the element14 community, projects that have included NFC have used an add-on expansion board or shield. But today I was sent some information on an MCU that integrates NFC.

 

It's produced by NXP, and called the LPC8N04 microcontroller.They consider it an entry-level connectivity solution for embedded applications with integrated NFC connectivity. It contains multiple features, including several power-down modes and a selectable CPU frequency of up to 8 MHz for ultra-low power consumption. The peripheral complement includes 32 kB of flash memory, 8 kB of SRAM, 4 kB of EEPROM, one I2C, one SPI/SSP, and up to 12 general purpose I/O pins. Your can read more about it by clicking here.image

 

NXP also says that it enables developers to quickly implement broad-based solutions that leverage system diagnostics or environmental conditions for a smarter tagging experience. With the added benefit of flexible communication modes, you'd have the ability to push data to an LPC8N04 MCU-based edge-node, for example, in device provisioning, configuration or customization. 

 

I think it has interesting possibilities for Board Games, Healthcare Wearables, Robotics, Industrial Uses and, of course, Secure Payments.

 

What do you think?

 

Would you be interested in roadtesting this product? What would you like to test or build?

 

 

  • Sign in to reply
  • Cancel
Parents
  • dougw
    dougw over 8 years ago

    NFC is definitely on my list of technologies to become proficient with. It is already widely used but the applications are still in their infancy relative to what will be implemented in the next few years. I have experimented with RFID and a little NFC trying to get the range out to 1 foot. I could get about 9 inches reliably. I don't know if this road test would fit in my schedule as the dates aren't set, but I would follow the road test activity for sure.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • awneil
    awneil over 8 years ago in reply to dougw

    Remember that the 'N' in "NFC" stands for Near - so NFC is never going to work for "long" range.

     

    Passive RFID is also essentially relies upon near-field effects - which is quite different from the far-field effects of "conventional" radio links.

    It basically relies upon induction: https://en.wikipedia.org/wiki/Near-field_communication#Overview

     

    If you want long range - which, in this context, probably is about 9 inches or more - then you should probably be looking at active RFID tags.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 8 years ago in reply to awneil

    relies upon near-field effects

    I read somewhere that Near Field is within one wavelength.

    https://en.wikipedia.org/wiki/Near_and_far_field

     

    13.5 MHz is about 22.2m (71.6 ft)

    125 Khz is about 2400m (7740 ft)

     

     

    I'm thinking they would need to be active for anywhere close to those distances. image

     

    mark

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • genebren
    genebren over 8 years ago in reply to mcb1

    I worked with fish tags on a fish survey package.  The tags were passive and even with a pretty powerful antenna (RF and Power) the tags would only read reliably at a distance of a few inches.  Notable in this case, the fish tags were very tiny (approximately the size of a DO-214AC diode), which likely limited the ability to receive power (also the return packet was several digits, requiring longer active times).

    Gene

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 8 years ago in reply to dougw

    dougw

    There are some interesting setups used for detecting fish.

    It involved feeding a few amps through the coil which spanned a large stream.

     

     

     

    Tags are either passive and they use parasitic power which then powers the processor, or powered with an on-board power source.

    The range of passive is limited by the power and the size of the tag antenna.

    Obviously tags designed to go under the skin can't be as large as keyfob or card tags, so the detection and more importantly the influence on the transmitter antenna is less.

     

     

    There are also some interesting tag hacks, where they use a processor and coil to simulate the tag.

    These are not passive ... or legal image

     

    Mark.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • mcb1
    mcb1 over 8 years ago in reply to dougw

    dougw

    There are some interesting setups used for detecting fish.

    It involved feeding a few amps through the coil which spanned a large stream.

     

     

     

    Tags are either passive and they use parasitic power which then powers the processor, or powered with an on-board power source.

    The range of passive is limited by the power and the size of the tag antenna.

    Obviously tags designed to go under the skin can't be as large as keyfob or card tags, so the detection and more importantly the influence on the transmitter antenna is less.

     

     

    There are also some interesting tag hacks, where they use a processor and coil to simulate the tag.

    These are not passive ... or legal image

     

    Mark.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Children
  • genebren
    genebren over 8 years ago in reply to mcb1

    I worked with fish tags on a fish survey package.  The tags were passive and even with a pretty powerful antenna (RF and Power) the tags would only read reliably at a distance of a few inches.  Notable in this case, the fish tags were very tiny (approximately the size of a DO-214AC diode), which likely limited the ability to receive power (also the return packet was several digits, requiring longer active times).

    Gene