RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Would You Be Interested in RoadTesting an MCU with Integrated NFC
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 22 replies
  • Subscribers 2753 subscribers
  • Views 3160 views
  • Users 0 members are here
  • scasny
Related

Would You Be Interested in RoadTesting an MCU with Integrated NFC

rscasny
rscasny over 8 years ago

Near Field Communication is growing in popularity. It's being used for more than payment processing; and it's even popping up in some of our design challengers' builds (e.g., The Cooker Connector by jschools). For the most part on the element14 community, projects that have included NFC have used an add-on expansion board or shield. But today I was sent some information on an MCU that integrates NFC.

 

It's produced by NXP, and called the LPC8N04 microcontroller.They consider it an entry-level connectivity solution for embedded applications with integrated NFC connectivity. It contains multiple features, including several power-down modes and a selectable CPU frequency of up to 8 MHz for ultra-low power consumption. The peripheral complement includes 32 kB of flash memory, 8 kB of SRAM, 4 kB of EEPROM, one I2C, one SPI/SSP, and up to 12 general purpose I/O pins. Your can read more about it by clicking here.image

 

NXP also says that it enables developers to quickly implement broad-based solutions that leverage system diagnostics or environmental conditions for a smarter tagging experience. With the added benefit of flexible communication modes, you'd have the ability to push data to an LPC8N04 MCU-based edge-node, for example, in device provisioning, configuration or customization. 

 

I think it has interesting possibilities for Board Games, Healthcare Wearables, Robotics, Industrial Uses and, of course, Secure Payments.

 

What do you think?

 

Would you be interested in roadtesting this product? What would you like to test or build?

 

 

  • Sign in to reply
  • Cancel
Parents
  • mcb1
    mcb1 over 8 years ago
    Would you be interested in roadtesting this product?

    I've had a play with NFC and have a phone that has some great NFC features BUT they only supplied two sticker tags, and have no blanks or anything else.

     

    We utilise NFC prox tags for security at work, and they are a great way to provide low maintenance access in a very small package.

     

    One suggestion I'd make with this Road Test make sure there are plenty of compatible tags to go with the reader.

    The stickers are a great use and can be almost hidden, while providing the desired effect.

     

     

    I was lucky to mentor a group of pupils in a Neighbourhood Engineer, in aproject to assist the elderly.

    Their idea was to identify the right key for the door, and their idea was a card reader BUT in reverse.!

    The prox tag was on the door and the reader was handheld.

     

    What would you like to test or build?

    I might be able to build something to make use of this.

      imageimage

    Cheers

    Mark

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • Fred27
    Fred27 over 8 years ago in reply to mcb1

    I've only quickly scanned the details, but I believe this MCU is set up to be a tag, not a reader. On particular it can be powered by the NFC field to work without a battery.

     

    ST's  M24LR-DISCOVERYM24LR-DISCOVERY is a similar concept although not a single IC solution like this

     

    Also, real men have their NFC tag on the *inside* of their hand. ;-)

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • rsc
    rsc over 8 years ago in reply to Fred27

    You may be correct, the block diagram says "NFC Tag"

    The data sheet doesn't have much information about the NFC interface.

    I can imagine a few things that could be done with a programmable NFC tag.

    The tag could change information based on time or status of a sensor.

    Data could be encrypted/decrypted with a transmitted "key"

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • rsc
    rsc over 8 years ago in reply to Fred27

    You may be correct, the block diagram says "NFC Tag"

    The data sheet doesn't have much information about the NFC interface.

    I can imagine a few things that could be done with a programmable NFC tag.

    The tag could change information based on time or status of a sensor.

    Data could be encrypted/decrypted with a transmitted "key"