RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum How Would You RoadTest: Isolated Digital USB 3.0 I/O Module
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 18 replies
  • Subscribers 2756 subscribers
  • Views 2367 views
  • Users 0 members are here
  • scasny
Related

How Would You RoadTest: Isolated Digital USB 3.0 I/O Module

rscasny
rscasny over 8 years ago

Today I was approached about roadtesint this USB 3.0 I/O Module. so, I wanted to take a moment to introduce it to you, mention a few salient points, and ask the RoadTester group how they would roadtest it. Here goes:

 

This is a 16-channel isolated digital input and output USB 3.0 I/O module. It has a built in USB hub that supports a daisy chain topology. All digital input and digital output channels are protected by 2,500 VDC isolation. A few other points are:

image

  • USB 3.0 SuperSpeed
  • Daisy chainable by built in USB hub
  • 16-ch digital input and 16-ch digital output with 2,500 VDC isolation
  • Wide input voltage range (10 ~ 30 VDC)
  • Wide output voltage range (5 ~ 40 VDC) and high output current (350 mA/ch)
  • Quick removable European type connector
  • LED indicators for I/O status
  • Supported operating systems: Windows XP/7/8/10 and Linux

 

 

Would you be interested in RoadTesting this product? What would you like to test or build?

Attachments:
image
  • Sign in to reply
  • Cancel
Parents
  • dougw
    dougw over 8 years ago

    The voltage capabilities of this module lend themselves well to automotive power.

    Modern smart phones have USB 3 and can manage multiple video sources.

    I'm thinking some complex system that runs off vehicle power where a smart phone is the logical choice for the brains of the system.

    For example a high-tech camping system that provides all the luxuries of home while out in the boonies.

    Power management would be a big application.

    If you had some solar panels, batteries, a weather station, lighting, heating, cooling, security a couple of dozen appliances and entertainment systems to manage and a nice app to automatically figure out how to optimally provide the services needed with the power available, a device like this would definitely be useful.

    I'm not actually designing something like this, just speculating if I ever get the resources to build a high-tech cottage....

    Maybe there would be good applications in a normal house if aspects of it are running off low voltage solar power.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dougw
    dougw over 8 years ago

    The voltage capabilities of this module lend themselves well to automotive power.

    Modern smart phones have USB 3 and can manage multiple video sources.

    I'm thinking some complex system that runs off vehicle power where a smart phone is the logical choice for the brains of the system.

    For example a high-tech camping system that provides all the luxuries of home while out in the boonies.

    Power management would be a big application.

    If you had some solar panels, batteries, a weather station, lighting, heating, cooling, security a couple of dozen appliances and entertainment systems to manage and a nice app to automatically figure out how to optimally provide the services needed with the power available, a device like this would definitely be useful.

    I'm not actually designing something like this, just speculating if I ever get the resources to build a high-tech cottage....

    Maybe there would be good applications in a normal house if aspects of it are running off low voltage solar power.

    • Cancel
    • Vote Up +3 Vote Down