RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum What is a RoadTest by Invitation?
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 11 replies
  • Subscribers 2751 subscribers
  • Views 1748 views
  • Users 0 members are here
  • scasny
Related

What is a RoadTest by Invitation?

rscasny
rscasny over 8 years ago

I noticed that there were some comments regarding a new RoadTest I posted, STEM micro:bit - Minode Kit

 

This is a special kind of roadtest. It's called a RoadTest by Invitation. So what does that term mean?

 

Well, the best way to describe it is to talk about this roadtest on the Minode Inventor's Kit. This kit has a microbit and a bunch of electronic parts for building basic projects. It's a product for schools. One of my colleagues had been working with some educators and he suggested offering them these kits so see how well they worked in the classroom, as I understand the situation. So we were looking for a specific kind of roadtester to try out these products. Since we knew whom we wanted to provide the kits to, there was no need for an enrollment period. This is a common use for a RoadTest by Invitation.

 

Other uses for the RoadTest by Invitation would be that the supplier was seeking people with a specific background, or they wanted to get a review in a few weeks instead of 60 days.

 

For some RoadTests by Invitation, the pre-selection process can be more rigorous than a standard RoadTest application. I may contact members I believe are a good fit for a certain type of test, but I may ask them pointed questions about the product as well as their ability to complete the roadtest as per my requirements. And I also consider commitment, participation and professionalism when I recommend a RoadTester by Invitation.

 

I will admit there is one drawback for a RoadTest by Invitation: a first-time roadtester will probably not be selected for it.

 

I personally don't care for RoadTest by Invitations that much. I like the open competition of enrollment. However, I think it is a RoadTest type that is appropriate in some situations.

 

If you have any questions or comments, feel free to put them in the Comments section below. I will monitor this discussion closely for a week. I want to make sure everyone who has questions, get's a personal answer from me.

 

Randall Scasny

RoadTest Program Manager

  • Sign in to reply
  • Cancel
Parents
  • rscasny
    rscasny over 8 years ago

    To all Commenters:

     

    I appreciate all your comments. I've been studying RoadTest by Invitations and I am trying to rethink how e14 does them. So everyone's input is being considered.

     

    I think they have value is some situations. Specifically, when a special skill is needed. But the way we produce them to the community should be improved.

     

    My personal preference is to called them Special Roadtests rather than by Invitation and open them up to the community but for a shorter enrollment period. Experienced roadtesters would probably be preferred over first-time roadtesters to do these roadtests.

     

    Special Roadtests would be used in the following situations:

     

    1. a special skill is needed

    2. the roadtest review must be produced in less than 60 days

    3. A pre-launch product: this is when a supplier has the product but the date it is introduced to the marketplace is in the near future.

    4. a reference design: not an openly marketed product

    5. a special solution is needed for a particular product

     

    These are my thoughts only. I am still working through the ideas and offering proposals to my bosses.

     

    Randall Scasny

    RoadTest Program Manager

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 8 years ago in reply to rscasny

    I appreciate all your comments. I've been studying RoadTest by Invitations and I am trying to rethink how e14 does them. So everyone's input is being considered.

    Thanks.

     

    The RoadTest by Invitation does have special considerations, and it may be only open to certain people. (which is fine)

    The current problem is that it's visible to everyone in order to make it fit the existing framework on the site.

     

     

    I was wondering if you can have a special place that is hidden to the general membership, but is open to those whom you decide are being considered.

    Something akin to the TM area.

     

    For the Test you would create the necessary paging in that area, and add those memebers considered as potential applicants.

    Once the applications have been taken, the participants chosen and announced, then make it visible to the full membership.

    To everyone else the RT would appear as if they have been away for a month and the applications closed before they could apply.

     

     

    Mark

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 8 years ago in reply to mcb1

    Hi Mark,

    Just speculating, the software vendor may not have anticipated this use-case and justifying development with them for a thing that is infrequent might not be easy to do.

     

    (At one place where I worked in the past, I had to jump through hoops for internal orders for example - the system was crazy complicated, about 50 fields to fill in across multiple web pages before the system timed out - one error and the order would be rejected and start over! And the system got more complicated each year as finance/legal rules changed, and the changes were 'bolted on'. But no-one could justify the effort to create a project to streamline the process, because internal orders were rare for that company).

     

    There is a benefit, I guess if some people did accidentally apply for a roadtest-by-invite without noticing the closing date was so soon, perhaps if the application is very good, the vendor might consider and include them. Never say never I guess.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 8 years ago in reply to mcb1

    Hi Mark,

    Just speculating, the software vendor may not have anticipated this use-case and justifying development with them for a thing that is infrequent might not be easy to do.

     

    (At one place where I worked in the past, I had to jump through hoops for internal orders for example - the system was crazy complicated, about 50 fields to fill in across multiple web pages before the system timed out - one error and the order would be rejected and start over! And the system got more complicated each year as finance/legal rules changed, and the changes were 'bolted on'. But no-one could justify the effort to create a project to streamline the process, because internal orders were rare for that company).

     

    There is a benefit, I guess if some people did accidentally apply for a roadtest-by-invite without noticing the closing date was so soon, perhaps if the application is very good, the vendor might consider and include them. Never say never I guess.