RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum How Would You RoadTest This System on Module (SOM) for Embedded Linux Applications?
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 2751 subscribers
  • Views 1628 views
  • Users 0 members are here
  • scasny
Related

How Would You RoadTest This System on Module (SOM) for Embedded Linux Applications?

rscasny
rscasny over 8 years ago

I was handed some information on Microchip's new SOM  (PN: ATSAMA5D27-SOM1) for embedded Linux applications. The SOM can be used in Microchip's ATSAMA5D27-SOM1-EK1 dev board or place the module onto your application board.image

 

Featuring an ARM-based MPU, the module is a small-single sided PCB, 40mm x 38mm, industrial temperature grade (-40/+85C) and requires a single 3.3V power supply for operation.

 

Microchip calls is a "ready to go" Linux solution. It's is supplied with in-house Linux support.

 

Here are the key features:

 

System-In-Package (SAMA5D27C-D1G-CU) including:

  • Arm Cortex-A5 processor-based SAMA5D2 MPU
  • 1Gbit DDR2 SDRAM

On-Board Power Management Unit (MIC2800-G1JJYML)image

1Kb Serial EEPROM with EUI-48Tm Node Identity (24AA02E48T-I/OT)

64Mb Serial Quad I/O Flash Memory (SST26VF064BT-104I/MF)

10Base-T/100Base-TX Ethernet PHY (KSZ8081RNAIA)

40 x 38 mm Module, Pitch 0.8mm, solderable by hand

103 I/Os

Up to 7 Tampers

One USB Device, one USB Host and one HSIC Interface

Shutdown and Reset Control Pins

Independent Power Supplies Available for Camera Sensor, for SD Card and for Backup depending on

Voltage Domains

Operational Specifications:

  • Main operating voltage: 3.3V ± 5%
  • Temperature range: -40°C to 85°C
  • Integrated crystals, internal voltage regulators
  • Multiple interfaces and I/Os for easy application development

 

So, what are your thoughts about roadtesting this baby? Feel free to offer your comments below.

 

(Here's a link to the technical manual.)

  • Sign in to reply
  • Cancel
Parents
  • 14rhb
    14rhb over 8 years ago

    Looking at the Microchip documentation that board has a great range of peripherals including:

    • CAN bus
    • mikroBUS x2
    • PMOD x1
    • LCD Interface
    • Camera Interface

     

    The Linux distro setup for the board is available at this link http://www.at91.com/linux4sam/bin/view/Linux4SAM/Sama5d27Som1EKMainPage#Demo_archives - this cool site also provides other SAM based board Linux distros so well worth a browse !

     

    To answer the Roadtest question - I guess once Linux is setup and running it would be to try and make something fun/novel based on components/modules available to the tester.

     

    Rod

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • 14rhb
    14rhb over 8 years ago

    Looking at the Microchip documentation that board has a great range of peripherals including:

    • CAN bus
    • mikroBUS x2
    • PMOD x1
    • LCD Interface
    • Camera Interface

     

    The Linux distro setup for the board is available at this link http://www.at91.com/linux4sam/bin/view/Linux4SAM/Sama5d27Som1EKMainPage#Demo_archives - this cool site also provides other SAM based board Linux distros so well worth a browse !

     

    To answer the Roadtest question - I guess once Linux is setup and running it would be to try and make something fun/novel based on components/modules available to the tester.

     

    Rod