RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum RoadTest Application "What Am I Supposed to Write?"
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 19 replies
  • Subscribers 2754 subscribers
  • Views 2668 views
  • Users 0 members are here
  • scasny
Related

RoadTest Application "What Am I Supposed to Write?"

rscasny
rscasny over 8 years ago

Part of my job at element14 is to read the RoadTest applications and make recommendations to the supplier for who should be selected as the official roadtesters. I just spent an hour going through applications for a roadtest. A high number of them were one sentence applications, which I do not consider competitive applications. In this sub-group I received a higher number number than usual which stated as his application: "What am I supposed to Write Here?"

 

It's a curious response, from my point of view. If this were a job application or a job interview, and the employer asked why do you want this job, would you answer, "What am I supposed to say?" My guess is probably not. If I were competing with other people for a product, I guess I would want to show them my I was the best and what I would do with it. Perhaps adding in something I did in the past was tangible proof I could do the job would help.

 

If you still do not know what to write in a roadtest application, please take the 15-munutes to listen to my webinar: Webinar Recording: How To Write a Winning RoadTest Application.

 

There was a previous discussion that memebers began on the chances of getting selected: https://www.element14.com/community/message/241787/l/re-commenting-in-roadtest-and-chances-of-getting-selected#241787

 

There is a 100% chance you will not get selected when: (a) you only write 1 sentence in the comments of the application or (b) you ask, What am I supposed to write here?

 

Randall Scasny

RoadTest Program Manager

  • Sign in to reply
  • Cancel
Parents
  • gecoz
    gecoz over 8 years ago

    Hi Randall,

     

    It is a tough act to balance. On one side, there is the push to make the selection process more strict, so that you get better odds of good reviews published, but on the flip side you need to give chance to newcomers to prove themselves.

     

    I think that you are doing a great job with the program, which I feel has noticeably improved in the last year. One thing we need to accept and live with is that a 100% success rate on all the Roadtests, as nice as it would be, it is just impossible, as there will always be someone who will play the system to their own benefit.

     

    Making the enrolment process too strict it might result in reducing the number of applicants to the usual group of very reliable active members, which surely would provide excellent reviews, but would make the Roadtest group feel like a closed group, compromising the chance of further grow.

     

    One possible way to try improve the quality of the application could be to add a short mandatory questionnaire as part of the enrolment process: the questionnaire would be based on the information given in the webinar you have published (a bit like the format used for the quiz of Essentials learning modules). Nothing overly complicated, just couple of questions (the ones that cover the points you made at the end of your post).

     

    Probably, to be more effective, the questionnaire should be put as first step of the enrolment. The rest of the process I think works well just as it is now.

     

    Just my 2p.

     

    Fabio

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • rscasny
    rscasny over 7 years ago in reply to gecoz

    I understand that sometimes I won't get all the reviews back. People get ill, or a family issue comes up. Or even someone gets laid off and now is looking for a full time job. These are valid reasons. When these things do arise, I tell the supplier and they always understand and are compassionate about these things.

     

    In every roadtest, I try to reserve a spot for a new/first time roadtester, because we always need new people in the program. But a new person still needs to write a reasonable application and I have to feel they can do the job. I have had several roadtests where ad no first timer write a reasonable application. I had no choice but to rely an experienced roadtesters.

     

    Am I too strict? I reflect on that a lot. I surely don't want to dissuade anyone from the program. But I need someone who has a genuine interest. So, if people don't complete the application or when I ask them to tell me about how they would roadtest and they say, "I dunno. I'll figure it out when I get the thing ion my hands." I have to think twice before sending it to that person when another applicant writes a good testing procedure.

     

    Randall

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • rscasny
    rscasny over 7 years ago in reply to gecoz

    I understand that sometimes I won't get all the reviews back. People get ill, or a family issue comes up. Or even someone gets laid off and now is looking for a full time job. These are valid reasons. When these things do arise, I tell the supplier and they always understand and are compassionate about these things.

     

    In every roadtest, I try to reserve a spot for a new/first time roadtester, because we always need new people in the program. But a new person still needs to write a reasonable application and I have to feel they can do the job. I have had several roadtests where ad no first timer write a reasonable application. I had no choice but to rely an experienced roadtesters.

     

    Am I too strict? I reflect on that a lot. I surely don't want to dissuade anyone from the program. But I need someone who has a genuine interest. So, if people don't complete the application or when I ask them to tell me about how they would roadtest and they say, "I dunno. I'll figure it out when I get the thing ion my hands." I have to think twice before sending it to that person when another applicant writes a good testing procedure.

     

    Randall