RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Reminder to RF specialists--Antenna RoadTest Needs You
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 2751 subscribers
  • Views 860 views
  • Users 0 members are here
  • scasny
Related

Reminder to RF specialists--Antenna RoadTest Needs You

rscasny
rscasny over 8 years ago

I know I am running a lot of interesting roadtests at the moment. But if you have RF or antenna expertise, I'd appreciate if you'd take a look at the antenna roadtest I am enrolling for:

 

Molex 2.4GHz / 5GHz Antenna Kit

 

I'd say it's probably the most important roadtest that's running right now. Perhaps we may forget how important an antenna (or I should say a good antenna) is to a wireless system. So, seeing a roadtest on antennas is important (and a good learning experience too).

 

This is the first antenna roadtest we have done. So, if you would be interested and are in need of something extra to perform the test, please contact me at rscasny

 

Sincerely,

 

Randall Scasny

RoadTest Program Manager

  • Sign in to reply
  • Cancel
Parents
  • mcb1
    mcb1 over 8 years ago

    I spent a number of years in, around, fixing, and site testing antennas and RF systems.

     

    While the theory transposes to the higher frequencies, the equipment to test these is a little harder.

    As others have commented, the interfacing between connectors may well have the greater influence, than the actual antenna.

     

    I note that the chip style are going to be on a breakout board, which hopefully has the same connector.

    If this is the situation, then swapping and repeating the same experiment, should should advantages.

     

    Testers should be able to test the radiation pattern of the antenna, but care is needed so that the fixture holding it doesn't influence the readings.

     

    In theory all these antenna are omni-directional, and presumably they all have the same gain, so while this provides a comparison, I'm thinking that the manufacturer already has these published.

     

    Whatever the testers do or use, they will need access to RSSI or the ability to antenuate the signal to a known point, and the ability to communicate with the device under test.

     

     

    In terms of importance, yes the antenna is one of the critical elements, however the design, testing and other requirements probably mean that most makers and users here will opt for COTS (Commercial Off The Shelf) designs, rather than scratch building a 2.4/5GHz device.

    It's not hard at these frequencies to have the wrong pcb characteristic destroy all the careful work you've done laying ot put and adding the matching components between transmitter and antenna.

     

     

    Good luck to the testers, but sorry this is one I don't have the equipment for.

    Mark

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • mcb1
    mcb1 over 8 years ago

    I spent a number of years in, around, fixing, and site testing antennas and RF systems.

     

    While the theory transposes to the higher frequencies, the equipment to test these is a little harder.

    As others have commented, the interfacing between connectors may well have the greater influence, than the actual antenna.

     

    I note that the chip style are going to be on a breakout board, which hopefully has the same connector.

    If this is the situation, then swapping and repeating the same experiment, should should advantages.

     

    Testers should be able to test the radiation pattern of the antenna, but care is needed so that the fixture holding it doesn't influence the readings.

     

    In theory all these antenna are omni-directional, and presumably they all have the same gain, so while this provides a comparison, I'm thinking that the manufacturer already has these published.

     

    Whatever the testers do or use, they will need access to RSSI or the ability to antenuate the signal to a known point, and the ability to communicate with the device under test.

     

     

    In terms of importance, yes the antenna is one of the critical elements, however the design, testing and other requirements probably mean that most makers and users here will opt for COTS (Commercial Off The Shelf) designs, rather than scratch building a 2.4/5GHz device.

    It's not hard at these frequencies to have the wrong pcb characteristic destroy all the careful work you've done laying ot put and adding the matching components between transmitter and antenna.

     

     

    Good luck to the testers, but sorry this is one I don't have the equipment for.

    Mark