RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Preview of Upcoming RoadTest: MicroChip SAML10/11 Xplained Pro Evaluation Kits
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 2754 subscribers
  • Views 1010 views
  • Users 0 members are here
  • scasny
Related

Preview of Upcoming RoadTest: MicroChip SAML10/11 Xplained Pro Evaluation Kits

rscasny
rscasny over 8 years ago

In the next month or so, I will be roadtesting the Microchip SAML10/L11 Xplained Pro Evaluation Kits. I want to take this opportunity to give you a bit of information on them as well as some source information.

 

Let's start with the SAML10. Here's a few facts: The SAM L10 Xplained Pro evaluation kit is ideal for evaluating and prototyping with the ultra low power SAML10 ARMRegistered CortexRegistered-M23 based microcontrollers. The SAM L10  MCU features general purpose embedded control capabilities with enhanced peripheral touch controller and advanced analog. It comes (interestingly enough) with some demos:image

  • water tolerant touch
  • keypad touch
  • low power weather station
  • SleepWalking (Yes, that is correct, sleepwalking)

For more information on the SAML10, go here.

 


The SAML11 is a variant, and appears to offer more in the way of security features. Here's the facts: The SAML11 Xplained Pro evaluation kit is ideal for evaluating and prototyping with the ultra low power SAML11 ARMRegistered CortexRegistered-M23 based microcontrollers integrating robust security which includes ARMRegistered TrustZoneRegistered, secure boot, crypto acceleration, secure key storage and chip-level tamper detection. In addition to security the SAM L11 MCU features general purpose embedded control capabilities with enhanced peripheral touch controller and advanced analog. It also has its own unique demos:

  • trusted execution environment
  • secure LoRa IoT node
  • Amazon Web Services (AWS) enrollment using Trustonic Kinibi-M
  • water tolerant touch
  • keypad touch demos

 

As expected, both versions come with some common features, such as:

  • Xplained Pro extension headers
  • mikroBUS socket
  • X32 header
  • Embedded debugger
  • XAM with Data Visualizer support for real-time power measurement
  • ATECC508A Crypto Authentication IC
  • USB powered

For more information on the SAML11, go here.

 

I'd encourage you to take a local at what these boards have to offer. If you have the time, please live a comment or what you might like to build with it.

 

 

 

 

 

 

  • Sign in to reply
  • Cancel
Parents
  • david.long
    david.long over 8 years ago

    I bought one of these a few weeks ago - it's a great little board if you are looking to learn more about Arm TrustZone and building a secure application. As far as I know, this is the only Cortex-M23 development board currently available but I am sure other vendors will release M23-based MCUs soon.

    There are several examples available for this board within Atmel Studio, which automatically detects the board when you plug it in. Alternatively, you can use the more commonly used (at least in industry) Keil uVision IDE - they have created a TrustZone tutorial for the SAM L11 which you can download from here Application Note 314: Microchip SAM L11 Cortex-M23 TrustZone Tutorial . You will need to make sure you are using the latest version of uVision.

     

    Dave

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • david.long
    david.long over 8 years ago

    I bought one of these a few weeks ago - it's a great little board if you are looking to learn more about Arm TrustZone and building a secure application. As far as I know, this is the only Cortex-M23 development board currently available but I am sure other vendors will release M23-based MCUs soon.

    There are several examples available for this board within Atmel Studio, which automatically detects the board when you plug it in. Alternatively, you can use the more commonly used (at least in industry) Keil uVision IDE - they have created a TrustZone tutorial for the SAM L11 which you can download from here Application Note 314: Microchip SAM L11 Cortex-M23 TrustZone Tutorial . You will need to make sure you are using the latest version of uVision.

     

    Dave