RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum UpComing RoadTest: What Can You Build with the PSoC®︎ 6 WiFi-BT Pioneer Kit?
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 14 replies
  • Subscribers 2755 subscribers
  • Views 2253 views
  • Users 0 members are here
  • scasny
Related

UpComing RoadTest: What Can You Build with the PSoC®︎ 6 WiFi-BT Pioneer Kit?

rscasny
rscasny over 8 years ago

The roll out of new products and kits to help you develop IoT-based products is a trend that is just not stopping! Last year we roadtested Cypress's PSoCRegistered 6 BLE Pioneer Kit. And this year they are releasing the PSoCRegistered 6 WiFi-BT Pioneer Kit to help you develop PSoC 6 MCU + WiFi applications. With the growth of Wi-Fi-enabled devices in and out of the home, new dev kits in this mix shouldn't be surprising. So, let's look at this kit and see what you can build with it.

 

Let's start with the PSoc 62 which is featured in this dev board.

 

A few facts: The PSoC 62 MCU: a single- or dual-core MCU, with an ArmRegistered CortexRegistered-M4 and ArmRegistered CortexRegistered-M0+, 1MB of Flash, 288KB of SRAM, 104 GPIO, 7 programmable analog blocks, 56 programmable digital blocks, Full-Speed USB, a serial memory interface, a PDM-PCM digital microphone interface, and industry-leading capacitive-sensing with CapSenseTm. image

 

The CPU subsystem in the PSoC 62 consists of two ARM Cortex cores and their associated busses and memories: M4 with Floating-point unit and Memory Protection Units (FPU and MPU) and an M0+ with an MPU. The Cortex M4 and M0+ have 8-KB Instruction Caches (I-Cache) with 4-way set associativity. This subsystem also includes independent DMA controllers with 32 channels each, a Cryptographic accelerator block, 1 MB of on-chip Flash, 288 KB of SRAM, and 128 KB of ROM.

 

The Cortex M0+ provides a secure, un-interruptible Boot function. This guarantees that post-Boot, system integrity is checked and privileges enforced. Shared resources can be accessed through the normal ARM multi-layer bus arbitration and exclusive accesses are supported by an Inter-Processor Communication (IPC) scheme, which implements hardware semaphores and protection. Active power consumption for the Cortex M4 is 26 µA/MHz and 17 µA/MHz for the Cortex M0+, both at 3V chip supply voltage with the internal buck enabled and at 0.9V internal supply.

 

Now let's look at some of the features on the PSoCRegistered 6 WiFi-BT Pioneer Kit.

 

The PSoC 6 WiFi-BT Pioneer board offers compatibility with ArduinoTm shields. The board features a PSoC 6 MCU, a 512-Mb NOR flash, an onboard programmer/debugger (KitProg2), a 2.4-GHz WLAN and Bluetooth functionality module (CYW4343W), a USB Type-C power delivery system (EZPDTm CCG3), a five-segment CapSense slider, two CapSense buttons, one CapSense proximity sensing header, an RGB LED, two user LEDs, USB host and device features, and one push button. The board supports operating voltages from 1.8 V to 3.3 V for the PSoC 6 MCU. image

 

The CY8CKIT-062-WiFi-BT package includes a CY8CKIT-028-TFT Display Shield that contains a 2.4-inch TFT display, a motion sensor, ambient light sensor, a 32-bit audio codec, and a PDM microphone. The PSoC 6 WiFi-BT Pioneer Kit features the Murata LBEE5KL1DX module, that provides IEEE 802.11a/b/g/n WLAN + Bluetooth, best-in-class power consumption, and enables small form factors for IoT devices.

 

The PSoC 6 WiFi-BT Pioneer Kit base board includes a Cypress EZ-PD CCG3 power delivery system. It comes preprogrammed and can deliver power from a Type-C port to an on-board header while simultaneously charging a 3.7-V lithium-ion polymer battery. In addition, the power delivery system can provide power to a Type-C peripheral such as a cell phone with power derived from an external source.

 

To develop a PSoC 6 MCU + WiFi application, WICEDTm Studio 6.1 or later must be used. WICED Studio is Cypress' integrated development environment (IDE) for developing WiFi applications. If you are not adding WiFi to your design then you can develop and debug PSoC 6 MCU project using PSoC CreatorTm. PSoC Creator supports exporting your designs to other third-party firmware development tools.

 

What can you build with the PSoCRegistered 6 WiFi-BT Pioneer Kit?

 

Depends...on you. But it's made for IoT applications and wearable devices, which makes sense since this PSoC is ultra low power.  But one needs to remembers that this kit has a high-performance PSoC 6 MCU. More facts: It has a programmable embedded system-on-chip, integrating a 150-MHz ArmRegistered CortexRegistered-M4 as the primary application processor, a 100-MHz Arm Cortex-M0+ that supports lowpower operations, up to 1MB Flash and 288KB SRAM, CapSenseRegistered touch-sensing, and programmable analog and digital peripherals that allow higher flexibility and in-field tuning of the design.

 

I think the question isn't what you can build with this kit, but what can you build that really needs a high performance MCU? You tell me.

 

So think about it and when I launch the roadtest in September, write me a high-performance roadtest application that tells it all.

 

Additional Information

  • https://uk.farnell.com/cypress-semiconductor/cy8ckit-062-wifi-bt/pioneer-kit-psoc6-cortex-m0-cortex/dp/2857060
  • https://www.farnell.com/datasheets/2606746.pdf?_ga=2.265667014.816149048.1535644907-1716107964.1507669740
  • Sign in to reply
  • Cancel
Parents
  • Instructorman
    Instructorman over 8 years ago

    I have a very good idea about what I would do with this kit.  It has every feature I need to achieve the functions I want to incorporate into a home theater lighting controller, including WiFi, cap sense, and Bluetooth.  I haven't checked but I'm sure it has enough PWM channels to handle all the dimming zones.  I have previously used a PSoC 4 pioneer kit to drive WS2812 RGB LED strings, so I can port that to the PSoC 6.  Also, I really like the Cypress development environment (PSoC creator).  I have never used WICED Studio, but if it was developed by the same team that made Creator, I think it will be straightforward to learn and use.

     

    Will there be a webinar on this kit?

     

    I am not planning to apply for this Road Test because I do not want to compete against others and risk not getting selected.  At about $128 CAD from Mouser ($169 CAD from Newark - and UK stock only!), the PSoC 6 WiFi-BT Pioneer kit is reasonably priced for experimental applications.

     

    I will take a closer look, but your post has inspired me to seriously consider ordering this kit.

     

    Thanks Randall and Cypress!

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 8 years ago in reply to Instructorman

    Very interesting application. I'm sure it would stand an excellent chance of winning, even with just the description you already provided. I don't see a down side to applying as long as you intend to post a blog about he project, and I hope you blog about it in any event..

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • Instructorman
    Instructorman over 8 years ago in reply to dougw

    Thanks Doug for the encouragement!

     

    I would like to blog about the development journey for this project.  I am, however, concerned about the time it will take me to get this project done.

    Until I retire I have limited time, and energy, to devote to home brew projects.  Seems to take me forever to make progress.

     

    Out of consideration for the audience, if I were to take the Road Test route, I would like to maintain steady progress.   I doubt I'd get this project done in the typical 2 month Road Test window.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 8 years ago in reply to Instructorman

    I agree this project is much more than a road test and would take a major effort to complete. If your initial blog covered set up and initial test of system resources, I think that would be enough to satisfy the road test obligation and it would be a good head start on the larger project. I'm not trying to put pressure on, just looking for a way for everyone to win. I'm sure Cypress would love it if you blog about the bigger project however long it takes. This module is way overkill for a simple little project and it is a much more compelling solution for bigger projects that flex its abilities.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dougw
    dougw over 8 years ago in reply to Instructorman

    I agree this project is much more than a road test and would take a major effort to complete. If your initial blog covered set up and initial test of system resources, I think that would be enough to satisfy the road test obligation and it would be a good head start on the larger project. I'm not trying to put pressure on, just looking for a way for everyone to win. I'm sure Cypress would love it if you blog about the bigger project however long it takes. This module is way overkill for a simple little project and it is a much more compelling solution for bigger projects that flex its abilities.

    • Cancel
    • Vote Up +3 Vote Down