RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Need Someone for a Project: Cypress PSoc6 BLE kit +  Honeywell Pressure Sensor Shield
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 103 replies
  • Subscribers 2756 subscribers
  • Views 14567 views
  • Users 0 members are here
  • scasny
Related

Need Someone for a Project: Cypress PSoc6 BLE kit +  Honeywell Pressure Sensor Shield

rscasny
rscasny over 7 years ago

I was contacted by a supplier who is interested in giving hardware for free to someone who could do a project for them featuring  Cypress's PSoc6 BLE kit +  Honeywell Pressure Sensor Shield.

 

They would like the person to do the following:

 

Interface the pressure sensors of the Honeywell Sensor Shield with the PSoC 6 analog/digital peripherals and then transmit data via BLE or showcasing it on the E-ink display of the PSoC 6 BLE Kit. The project should have some kind of medical application. For example, measuring pressure in some kind of health/medical application.

 

Just to refresh your mind, here are the parts involved:

 

image

Click here for more information or review the roadtest we did on this product: https://www.element14.com/community/roadTests/1862/l/cypress-psoc-6-ble-pioneer-kit-cy8ckit-062-ble#comment-117223

 

image

Click here for more information on this Honeywell Sensor Shield. I have not roadtested this product.

 

I would like to do this sometime in October. I'd like to get it accomplished in a month--the shorter time period is why I am not offering it as a roadtest.

 

If you are interested, feel free to comment below.

 

thanks.

 

Randall Scasny

RoadTest Program Manager

  • Sign in to reply
  • Cancel
Parents
  • rscasny
    rscasny over 7 years ago

    Hi All,

     

    I'm taking your names and providing them to the supplier. He spoke to me about a "medical application."

     

    Could you all provide me a 1-2 sentence on that?

     

    Thanks.

     

    Randall

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • BigG
    BigG over 7 years ago in reply to rscasny

    Hi Randall, I'm assuming this is more road test than design challenge. 

     

    As such, my aim would be to focus on the kit's ease of use and added functionality when combined with a PSoC 6. Although it seems that this kit is targeted at Arduino with the provision of a HEX file, which is not much use here, it is just as easy to DIY using I2C Serial Communication Blocks (SCB's), for example, and then showing sensor values on the eInk display as well as provide (time permitting) a BLE demo using the blood pressure GATT service (or possibly an adaption thereof).

     

    Having read through the kit's datasheet, I immediately linked this kit to sleep apnea or PAP/CPAP therapy. Having witnessed my daughter undergo a sleep study (as well has having had CPAP from time to time), I could immediately see that this market has a long way to go to get it right. With all the wires and sensors etc. strapped to the body for it is more like a "how long can a person be kept awake due to discomfort and annoyance before eventually dropping off out of shear exhaustion" type studies. So maybe a design challenge in this area would be a good thing to consider as a future event.

     

    Anyway, I recently came across these baby smart socks for SATS monitoring and, as such, felt that this could make for a relatively simple application to demonstrate the use of a pressure sensor (through a pressure sock or arm band or hand glove etc). Otherwise I would be looking at using multiple pressure sensors for a smart mat to monitor the dynamic changes of a person's sleep position.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • BigG
    BigG over 7 years ago in reply to rscasny

    Hi Randall, I'm assuming this is more road test than design challenge. 

     

    As such, my aim would be to focus on the kit's ease of use and added functionality when combined with a PSoC 6. Although it seems that this kit is targeted at Arduino with the provision of a HEX file, which is not much use here, it is just as easy to DIY using I2C Serial Communication Blocks (SCB's), for example, and then showing sensor values on the eInk display as well as provide (time permitting) a BLE demo using the blood pressure GATT service (or possibly an adaption thereof).

     

    Having read through the kit's datasheet, I immediately linked this kit to sleep apnea or PAP/CPAP therapy. Having witnessed my daughter undergo a sleep study (as well has having had CPAP from time to time), I could immediately see that this market has a long way to go to get it right. With all the wires and sensors etc. strapped to the body for it is more like a "how long can a person be kept awake due to discomfort and annoyance before eventually dropping off out of shear exhaustion" type studies. So maybe a design challenge in this area would be a good thing to consider as a future event.

     

    Anyway, I recently came across these baby smart socks for SATS monitoring and, as such, felt that this could make for a relatively simple application to demonstrate the use of a pressure sensor (through a pressure sock or arm band or hand glove etc). Otherwise I would be looking at using multiple pressure sensors for a smart mat to monitor the dynamic changes of a person's sleep position.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Children
  • BigG
    BigG over 7 years ago in reply to rscasny

    Ok, thanks for the clarification. Just to add that I still have some equipment at home, such as a nebuliser, an oxygen cylinder, tubing and an oxygen mask (see pics). What I don't have is a means to attach pressure sensor to tubing etc. So, if someone can advise, and/or provide the necessary attachments etc. then it should be quite straightforward to demonstrate pressure measurement etc. on the PSoC 6

     

    image

     

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • rscasny
    rscasny over 7 years ago in reply to BigG

    My apologies if I gave the impression this was a design challenge. It was more a of project where the supplier wanted something specific as far as functionality.

     

    Randall