RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Need Someone for a Project: Cypress PSoc6 BLE kit +  Honeywell Pressure Sensor Shield
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 103 replies
  • Subscribers 2756 subscribers
  • Views 14584 views
  • Users 0 members are here
  • scasny
Related

Need Someone for a Project: Cypress PSoc6 BLE kit +  Honeywell Pressure Sensor Shield

rscasny
rscasny over 7 years ago

I was contacted by a supplier who is interested in giving hardware for free to someone who could do a project for them featuring  Cypress's PSoc6 BLE kit +  Honeywell Pressure Sensor Shield.

 

They would like the person to do the following:

 

Interface the pressure sensors of the Honeywell Sensor Shield with the PSoC 6 analog/digital peripherals and then transmit data via BLE or showcasing it on the E-ink display of the PSoC 6 BLE Kit. The project should have some kind of medical application. For example, measuring pressure in some kind of health/medical application.

 

Just to refresh your mind, here are the parts involved:

 

image

Click here for more information or review the roadtest we did on this product: https://www.element14.com/community/roadTests/1862/l/cypress-psoc-6-ble-pioneer-kit-cy8ckit-062-ble#comment-117223

 

image

Click here for more information on this Honeywell Sensor Shield. I have not roadtested this product.

 

I would like to do this sometime in October. I'd like to get it accomplished in a month--the shorter time period is why I am not offering it as a roadtest.

 

If you are interested, feel free to comment below.

 

thanks.

 

Randall Scasny

RoadTest Program Manager

  • Sign in to reply
  • Cancel
Parents
  • rscasny
    rscasny over 7 years ago

    re: breakout boards

     

    I spoke with our sales manager. Doesn't look like the breakout boards are available yet.

     

    I'm placing the sensors part order now. I'll keep a watch out and if they come available, I'll order and send them to you.

     

    jomoenginer

    balearicdynamics

    BigG

    geralds

    dougw

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • balearicdynamics
    balearicdynamics over 7 years ago in reply to rscasny

    Sorry for my silence about the breakout boards issues in these days, I followed the thread by email but It was impossible to write back a decent comment.

     

    I see two options, here. The first is designing a small breadboard with just the pins expanded to the 2,5 mm distance but as rscasnyand other say it's a pain to solder the non-exposed pins. In cases like this, where the distance is not terrible but pins are not exposed I adopted a bit delicate but efficient solution, using a wire-wrapping wire to create the pins and gluing the small footprint on an isolated zone of a PCB breadboard. After this small effort, the resulting home-made breakout is almost stable and always worked fine for me. The image below shows my last try to apply this technique to a chip with a pins distance shorten than our case. I just stopped when I discovered a 4 Euro breakout board I bought the next day.

    image

    IMHO, the best solution of ever (I think Randall can be helpful in this case) is buying pre-built breakout boards like the example below. When I lived in Fremont, CA I found plenty of these stuff with many different configurations but here in Europe I never found this.

    What about making some footprint design for a micro-production? It will cost a few dollars I think. Let me know if this has sense I can try to provide if 30 days to have the stuff ready to ship is acceptable.

     

    Enrico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • balearicdynamics
    balearicdynamics over 7 years ago in reply to rscasny

    Sorry for my silence about the breakout boards issues in these days, I followed the thread by email but It was impossible to write back a decent comment.

     

    I see two options, here. The first is designing a small breadboard with just the pins expanded to the 2,5 mm distance but as rscasnyand other say it's a pain to solder the non-exposed pins. In cases like this, where the distance is not terrible but pins are not exposed I adopted a bit delicate but efficient solution, using a wire-wrapping wire to create the pins and gluing the small footprint on an isolated zone of a PCB breadboard. After this small effort, the resulting home-made breakout is almost stable and always worked fine for me. The image below shows my last try to apply this technique to a chip with a pins distance shorten than our case. I just stopped when I discovered a 4 Euro breakout board I bought the next day.

    image

    IMHO, the best solution of ever (I think Randall can be helpful in this case) is buying pre-built breakout boards like the example below. When I lived in Fremont, CA I found plenty of these stuff with many different configurations but here in Europe I never found this.

    What about making some footprint design for a micro-production? It will cost a few dollars I think. Let me know if this has sense I can try to provide if 30 days to have the stuff ready to ship is acceptable.

     

    Enrico