RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Need Someone for a Project: Cypress PSoc6 BLE kit +  Honeywell Pressure Sensor Shield
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 103 replies
  • Subscribers 2752 subscribers
  • Views 14816 views
  • Users 0 members are here
  • scasny
Related

Need Someone for a Project: Cypress PSoc6 BLE kit +  Honeywell Pressure Sensor Shield

rscasny
rscasny over 8 years ago

I was contacted by a supplier who is interested in giving hardware for free to someone who could do a project for them featuring  Cypress's PSoc6 BLE kit +  Honeywell Pressure Sensor Shield.

 

They would like the person to do the following:

 

Interface the pressure sensors of the Honeywell Sensor Shield with the PSoC 6 analog/digital peripherals and then transmit data via BLE or showcasing it on the E-ink display of the PSoC 6 BLE Kit. The project should have some kind of medical application. For example, measuring pressure in some kind of health/medical application.

 

Just to refresh your mind, here are the parts involved:

 

image

Click here for more information or review the roadtest we did on this product: https://www.element14.com/community/roadTests/1862/l/cypress-psoc-6-ble-pioneer-kit-cy8ckit-062-ble#comment-117223

 

image

Click here for more information on this Honeywell Sensor Shield. I have not roadtested this product.

 

I would like to do this sometime in October. I'd like to get it accomplished in a month--the shorter time period is why I am not offering it as a roadtest.

 

If you are interested, feel free to comment below.

 

thanks.

 

Randall Scasny

RoadTest Program Manager

  • Sign in to reply
  • Cancel
Parents
  • dougw
    dougw over 7 years ago

    I received a sensor package with 3 sensors and the SEK002 shield:

    image

    The sensors are the ones we specified, although we will need to do some level shifting on the 5V part to interface it to the PSoC6.

    There was no PSoC6 and my partner on this project glennvanderveer didn't get a PSoC6 either. I don't need a PSoC6 but he does - he can't participate without it.

    We have a pretty interesting test rig ready to test the sensors, but the hold up right now is the MCU.

    We will likely have to interface directly to the PSoC6 without using the SEK002 because the carrier shield won't fit in our test setup.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dougw
    dougw over 7 years ago

    I received a sensor package with 3 sensors and the SEK002 shield:

    image

    The sensors are the ones we specified, although we will need to do some level shifting on the 5V part to interface it to the PSoC6.

    There was no PSoC6 and my partner on this project glennvanderveer didn't get a PSoC6 either. I don't need a PSoC6 but he does - he can't participate without it.

    We have a pretty interesting test rig ready to test the sensors, but the hold up right now is the MCU.

    We will likely have to interface directly to the PSoC6 without using the SEK002 because the carrier shield won't fit in our test setup.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Children
  • jomoenginer
    jomoenginer over 7 years ago in reply to dougw

    I received the package today as well and the items look similar to the others.  However, I did receive a PSoC 6 BLE Kit but I already have one.   Perhaps I can send the one I have recently received to someone who needs it? 

    • Cancel
    • Vote Up +5 Vote Down