RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum What Do You Think of This Dev board:  NXP Layerscape LS1012A Freeway
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 2751 subscribers
  • Views 1625 views
  • Users 0 members are here
  • scasny
  • scasny_web
Related

What Do You Think of This Dev board:  NXP Layerscape LS1012A Freeway

rscasny
rscasny over 8 years ago


The Layerscape LS1012A Freeway (FRWY-LS1012A) board is an ultra-low-cost development platform for LS1012A. The board provides connectivity support for SPI, UART, and I2C based mikroBUSTm connector. Also, the FRWY-LS1012A supports 512 MB of DDR3L memory, two 1 Gbit/s Ethernet ports, one USB 3.0 port, Audio in/out and mic interface, and PCIe Gen1/2 M.2 Type E modules. The dimensions of the board are 83x90 mm. .image

 

The LS1012A processor is built on the LS architecture combining one ArmRegistered A53 processor core with the data path acceleration and network, peripheral interfaces required for networking, wireless infrastructure, and the general-purpose embedded applications.

 

FRWY-LS1012A comes loaded with Layerscape SDK, which is the next generation of Linux enablement software for Layerscape family of processors. It provides all the necessary drivers, tools and libraries required to enable all features of the ArmRegistered based Layerscape processors. Click Here for more information.

 

If you are interesting in playing around with this dev board, then sign up for the IoT Webinar: Computing at the Edge - When, Why and How

 

I have two boards to giveaway for attendees of the webinar.The best two questions asked during the webinar wins the board for FREE.

  • Sign in to reply
  • Cancel
Parents
  • hlipka
    hlipka over 8 years ago

    I'm wondering about the combination of functionality. Having two Ethernet ports suggests it's more targeted towards routing functionality (and the ref manual also suggests so). But then why has it a Mikrobus header and audio connectors?

    Interestingly the official target applications list 'NAS' systems, but the board has no SATA connectors...

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • hlipka
    hlipka over 8 years ago

    I'm wondering about the combination of functionality. Having two Ethernet ports suggests it's more targeted towards routing functionality (and the ref manual also suggests so). But then why has it a Mikrobus header and audio connectors?

    Interestingly the official target applications list 'NAS' systems, but the board has no SATA connectors...

    • Cancel
    • Vote Up +3 Vote Down