RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Have any helpful maker tips? Send them my way!
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 58 replies
  • Subscribers 2760 subscribers
  • Views 6944 views
  • Users 0 members are here
  • scasny
Related

Have any helpful maker tips? Send them my way!

danzima
danzima over 7 years ago

Hello RoadTest!

I'm working with our community team on a second volume of our Essential Tips for Makers eBook series (you can see the original here). Our fearless RoadTest leader rscasny suggested that I reach out to our wonderful group here and see if anyone might have some useful tips they've picked up that they'd be willing to contribute.

 

We'll be printing this eBook for distribution at Electronica 2018, and of course it'll live on in perpetuity on the community as well. If you have any ideas you'd like to share, please leave them in this thread! Also feel free to reach out to me directly if you have any questions.

 

Thanks everyone!

  • Sign in to reply
  • Cancel
Parents
  • DAB
    DAB over 7 years ago

    I encourage everyone to have a notebook and write all of your plans and ideas down before you try to build them.

    The planning process enables you to think about the steps involved, which usually triggers additional steps and ideas.

    The actual plan can be very rough, but it is the process that best prepares you to succeed,  because it lets you establish the full scope of what you want to do.

     

    DAB

    • Cancel
    • Vote Up +9 Vote Down
    • Sign in to reply
    • Cancel
  • Gough Lui
    Gough Lui over 7 years ago in reply to DAB

    I find having a notebook to be a good idea at first, but it tends to fall apart for me because the way one thinks and refines things is not linear by nature.

     

    So I tend to prefer loose scraps of paper (I know, bad idea) and pencil (which is probably even worse thanks to the graphite dust). I would draw things out, scribble, cross things out, grab another sheet, draw it neater, change things up, etc. Having it to hand and not having the restriction of "bound" books with pages in order is highly useful especially when drawing parts of circuits on each page and re-ordering/re-drawing/replacing one page here or there. Pencil can also be erased, which I find helpful, along with the pressure-sensitive nature of the medium which allows some variation in thickness/darkness of lines to help distinguish "messes" of wires crossing over each other. But doing things by hand rather than drawing it on a PC the first time can be quite helpful.

     

    Another thing is just to build things - while some people like breadboards, I've gotten over it myself and I prefer veroboard. Sometimes my first iterations are soldered straight to board - cut traces jumpered over (whoops), bits desoldered here and there. Having desoldering tools is very important, but the durability of veroboard has helped reduce the number of times things work "if I jiggle this wire a little". Don't be afraid to build on something more permanent.

     

    Adding in features to debug the circuit (whether deliberately, or accidentally) is useful - things like breaking out every leg of an IC even though you might not use it, or adding test point connections (I know, it's been mentioned before) is useful if it doesn't compromise signal integrity. Adding idiot-proofing features is also handy (if your circuit allows) for common errors like reverse polarity, missing connections, etc. Using keyed connectors can work as a double-safeguard. Just sprinkling header pins can be handy.

     

    Having a decent hot air gun and soldering station helps, along with making sure you take care of it and don't abuse the tip. Powering down when not actively in use helps save the life of the bit. Having a scope, PSU, DMM within reach of the soldering station also helps reduce the pain of having to move between debugging and soldering. Just don't get tempted to do both at the same time or risk a soldering-iron induced short.

     

    Keep an emergency metal tin or sturdy pot nearby in case your experiments with batteries go horribly wrong. Some are quite volatile, so being safe is best.

     

    Have a can of canned air or similar around as you can use it to do some quick thermal-inspired troubleshooting.

     

    Print out datasheets and annotate them by hand. Read them over and over - it's probably your best friend. Likewise, print out schematics, stick them to the bench/wall.

     

    I don't know ... most of these things are probably not "tips" as such - my benches aren't exactly highly exciting or special. But I just make do with what I have.

     

    - Gough

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Gough Lui
    Gough Lui over 7 years ago in reply to DAB

    I find having a notebook to be a good idea at first, but it tends to fall apart for me because the way one thinks and refines things is not linear by nature.

     

    So I tend to prefer loose scraps of paper (I know, bad idea) and pencil (which is probably even worse thanks to the graphite dust). I would draw things out, scribble, cross things out, grab another sheet, draw it neater, change things up, etc. Having it to hand and not having the restriction of "bound" books with pages in order is highly useful especially when drawing parts of circuits on each page and re-ordering/re-drawing/replacing one page here or there. Pencil can also be erased, which I find helpful, along with the pressure-sensitive nature of the medium which allows some variation in thickness/darkness of lines to help distinguish "messes" of wires crossing over each other. But doing things by hand rather than drawing it on a PC the first time can be quite helpful.

     

    Another thing is just to build things - while some people like breadboards, I've gotten over it myself and I prefer veroboard. Sometimes my first iterations are soldered straight to board - cut traces jumpered over (whoops), bits desoldered here and there. Having desoldering tools is very important, but the durability of veroboard has helped reduce the number of times things work "if I jiggle this wire a little". Don't be afraid to build on something more permanent.

     

    Adding in features to debug the circuit (whether deliberately, or accidentally) is useful - things like breaking out every leg of an IC even though you might not use it, or adding test point connections (I know, it's been mentioned before) is useful if it doesn't compromise signal integrity. Adding idiot-proofing features is also handy (if your circuit allows) for common errors like reverse polarity, missing connections, etc. Using keyed connectors can work as a double-safeguard. Just sprinkling header pins can be handy.

     

    Having a decent hot air gun and soldering station helps, along with making sure you take care of it and don't abuse the tip. Powering down when not actively in use helps save the life of the bit. Having a scope, PSU, DMM within reach of the soldering station also helps reduce the pain of having to move between debugging and soldering. Just don't get tempted to do both at the same time or risk a soldering-iron induced short.

     

    Keep an emergency metal tin or sturdy pot nearby in case your experiments with batteries go horribly wrong. Some are quite volatile, so being safe is best.

     

    Have a can of canned air or similar around as you can use it to do some quick thermal-inspired troubleshooting.

     

    Print out datasheets and annotate them by hand. Read them over and over - it's probably your best friend. Likewise, print out schematics, stick them to the bench/wall.

     

    I don't know ... most of these things are probably not "tips" as such - my benches aren't exactly highly exciting or special. But I just make do with what I have.

     

    - Gough

    • Cancel
    • Vote Up +7 Vote Down