RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Have any helpful maker tips? Send them my way!
  • Blogs
  • RoadTest Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 58 replies
  • Subscribers 2664 subscribers
  • Views 5542 views
  • Users 0 members are here
  • scasny
Related

Have any helpful maker tips? Send them my way!

danzima
danzima over 7 years ago

Hello RoadTest!

I'm working with our community team on a second volume of our Essential Tips for Makers eBook series (you can see the original here). Our fearless RoadTest leader rscasny suggested that I reach out to our wonderful group here and see if anyone might have some useful tips they've picked up that they'd be willing to contribute.

 

We'll be printing this eBook for distribution at Electronica 2018, and of course it'll live on in perpetuity on the community as well. If you have any ideas you'd like to share, please leave them in this thread! Also feel free to reach out to me directly if you have any questions.

 

Thanks everyone!

  • Sign in to reply
  • Cancel

Top Replies

  • fmilburn
    fmilburn over 7 years ago +11
    A bit of extra care with the enclosure and user interface can give a finished and professional look to a project. In the example below a PCB was designed and used as a faceplate.
  • luislabmo
    luislabmo over 7 years ago +10
    Most of the my tips are for easy bread-boarding/prototyping, I will update with pictures later on: Solder current limiting resistors to LEDs to save some space and time.... and use a big resistor (lets…
  • jc2048
    jc2048 over 7 years ago in reply to shabaz +10
    One thing to watch with old books is that sometimes the circuits were redrawn by graphic designers from scrappy, hand-drawn originals. A classic mistake was adding additional dots where there shouldn't…
Parents
  • littleben1
    littleben1 over 7 years ago

    Don't skimp on a good soldering station. Melting this tin solder is a pain and a good soldering station is essential.

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Cancel
  • gpolder
    gpolder over 7 years ago in reply to littleben1

    fully agree, and connected to that, if you are far from a water tap, keep a small bottle with water close by, for watering the sponge.

    image

    • Cancel
    • Vote Up +8 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 7 years ago in reply to gpolder

    At work we use one of those one time use water bottles....(you know the ones that people buy from a shop because they don't think our beautiful tap water is worth drinking.)

     

    However wet sponges is a good way to destroy tips, and I have changed to the brass type dish scrubbers from your local supermarket or other retailer.

    They are a dollar or so each and IMO do just as good a job.

     

    Mark

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • mcb1
    mcb1 over 7 years ago in reply to gpolder

    At work we use one of those one time use water bottles....(you know the ones that people buy from a shop because they don't think our beautiful tap water is worth drinking.)

     

    However wet sponges is a good way to destroy tips, and I have changed to the brass type dish scrubbers from your local supermarket or other retailer.

    They are a dollar or so each and IMO do just as good a job.

     

    Mark

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • Cancel
Children
  • gpolder
    gpolder over 7 years ago in reply to mcb1

    I never destroyed my tips, but thanks for the tip, I will try the dish scrubber from our kitchen.

    (two type of tips in the sentence above, as a non native speaker english language is still difficult to me)

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • luislabmo
    luislabmo over 7 years ago in reply to gpolder

    Tecnically a wet sponge doesn't destroy tips, but makes their lifespan shorter due to oxidation also, sudden changes on the Tip's temperature (from very hot to cold when using the sponge) will cause cracks to the tip's coating in the long term, a good explanation here. I agree with others, the brass sponge is good enough and does an excellent job.

     

    Luis

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 7 years ago in reply to gpolder

    A great benefit is it never seems to need cleaning/emptying. Since I've had the wire springy stuffy, I've never emptied it in a few years.. I don't know where the waste flux/solder/dirt off the iron falls.. probably falls through to the bottom of the pot eventually, but if I don't look there, the problem doesn't exist : )

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • Gough Lui
    Gough Lui over 7 years ago in reply to shabaz

    I personally still use the damp sponge method with no major issues. I tried getting into the brass-wool stuff, and while it's nice not to need the occasional topping up of water, I found that sometimes it wasn't quite as clean and the really "fresh" springy stuff has a habit (if you're a bit vigorous or in a hurry) of occasionally flicking hot solder which in itself could be a hazard or a minor inconvenience.

     

    - Gough

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 7 years ago in reply to Gough Lui

    Gough Lui  wrote:

     

    I personally still use the damp sponge method with no major issues. I tried getting into the brass-wool stuff, and while it's nice not to need the occasional topping up of water, I found that sometimes it wasn't quite as clean and the really "fresh" springy stuff has a habit (if you're a bit vigorous or in a hurry) of occasionally flicking hot solder which in itself could be a hazard or a minor inconvenience.

     

    - Gough

    The trick with the brass is:

    1. push tip in
    2. turn 90°
    3. tip out.

    No frantic poking required.

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • Cancel
  • luislabmo
    luislabmo over 7 years ago in reply to Jan Cumps

    I can confirm this is the right procedure but I'd add, if after these steps tip is not coming pristine clean, add some fresh solder and repeat the steps. Everytime I do it with some fresh solder, tip comes shinny and looking like new.

     

    Luis

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 7 years ago in reply to Jan Cumps

    Ahh.. I'll have to try step 2.. it makes sense, to get different bits of metal in contact.

    Currently I do step 1+3 twice or so.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 7 years ago in reply to shabaz

    shabaz  wrote:

     

    Ahh.. I'll have to try step 2.. it makes sense, to get different bits of metal in contact.

    Currently I do step 1+3 twice or so.

    I learned it from a Weller youtube tutorial.

    • Cancel
    • Vote Up +2 Vote Down