RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum What Do You Think About This Product: Coeur CST High-Current Interconnect System
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 17 replies
  • Subscribers 2756 subscribers
  • Views 3177 views
  • Users 0 members are here
  • scasny
Related

What Do You Think About This Product: Coeur CST High-Current Interconnect System

rscasny
rscasny over 7 years ago

I often don't think about connectors and connection system reliability. I like many people assume a connector from a quality company works reliably to connect wire-to-board and board-to-board applications. But what happens when there are is a misalignment between the two members that are being interconnected? Contact stresses can occur. Stresses can impede ideal contact/pin mating and in some situations increase contact resistance. When currents run higher and higher, in the hundreds of amps, undesirable thermal conditions can occur.image

 

So, when I was introduced to this connection system -- Coeur CST High-Current Interconnect System -- which provides a degree of float to accommodate any misalignment, I found it interesting and wanted to share it with the rest of you.

 

The Coeur CST High-Current Interconnect System provides up to 1.0mm of float due to its wave spring float mechanism so entire core socket assembly moves within the float housing.I am told that it doesn't add stress on contacts in float position and it offers low mating forces. There's also no risk of resistance increase due to high contact beam deflection.image

 

It's rated between 30.0 and 200.0A connects PCBs, bus bars and cable. It's used in data centers, PDUs, electric vehicles. When I saw them, I thought they could be used in any number of power converter types, load center terminations, battery banks, and more.

 

I'm not sure how they could be roadtested, but I could get some sample kits if someone has a decent way to test them. I've been told they've gone through rigorous testing already. But maybe a roadtest could be fashioned more along the lines of experimenting and observing its floating mechanism. If you have any ideas, leave a comment.

 

Randall Scasny

RoadTest Program Manager

  • Sign in to reply
  • Cancel
Parents
  • 14rhb
    14rhb over 7 years ago

    Looks like a useful product to know about at least; I could see it being popular in robotics, R/C vehicles or car-audio:- where they strive for compact designs, currents can be high and the ability to easily swap parts would be beneficial. This Coeur system reminds me of OSP/OSSP RF connectors in their usefulness for producing neat solutions.

     

    From a testing point of view a lead-acid car battery could be utilised to generate the required currents but some thought would be needed in the load selection/cooling of that load. Roadtesters would also likely need a clamp-current meter. <Safety Hat On>: the use of limiting fuses if using a car battery and eye protection against molten metal would seem appropriate as well !

     

    Rod

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • 14rhb
    14rhb over 7 years ago

    Looks like a useful product to know about at least; I could see it being popular in robotics, R/C vehicles or car-audio:- where they strive for compact designs, currents can be high and the ability to easily swap parts would be beneficial. This Coeur system reminds me of OSP/OSSP RF connectors in their usefulness for producing neat solutions.

     

    From a testing point of view a lead-acid car battery could be utilised to generate the required currents but some thought would be needed in the load selection/cooling of that load. Roadtesters would also likely need a clamp-current meter. <Safety Hat On>: the use of limiting fuses if using a car battery and eye protection against molten metal would seem appropriate as well !

     

    Rod

    • Cancel
    • Vote Up +5 Vote Down