RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum What Do You Think About This Product: Coeur CST High-Current Interconnect System
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 17 replies
  • Subscribers 2756 subscribers
  • Views 3177 views
  • Users 0 members are here
  • scasny
Related

What Do You Think About This Product: Coeur CST High-Current Interconnect System

rscasny
rscasny over 7 years ago

I often don't think about connectors and connection system reliability. I like many people assume a connector from a quality company works reliably to connect wire-to-board and board-to-board applications. But what happens when there are is a misalignment between the two members that are being interconnected? Contact stresses can occur. Stresses can impede ideal contact/pin mating and in some situations increase contact resistance. When currents run higher and higher, in the hundreds of amps, undesirable thermal conditions can occur.image

 

So, when I was introduced to this connection system -- Coeur CST High-Current Interconnect System -- which provides a degree of float to accommodate any misalignment, I found it interesting and wanted to share it with the rest of you.

 

The Coeur CST High-Current Interconnect System provides up to 1.0mm of float due to its wave spring float mechanism so entire core socket assembly moves within the float housing.I am told that it doesn't add stress on contacts in float position and it offers low mating forces. There's also no risk of resistance increase due to high contact beam deflection.image

 

It's rated between 30.0 and 200.0A connects PCBs, bus bars and cable. It's used in data centers, PDUs, electric vehicles. When I saw them, I thought they could be used in any number of power converter types, load center terminations, battery banks, and more.

 

I'm not sure how they could be roadtested, but I could get some sample kits if someone has a decent way to test them. I've been told they've gone through rigorous testing already. But maybe a roadtest could be fashioned more along the lines of experimenting and observing its floating mechanism. If you have any ideas, leave a comment.

 

Randall Scasny

RoadTest Program Manager

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    shabaz over 7 years ago

    Interesting item. From speaking in the past to an engineer working on high-power connections in computer server modules (like disk drive caddys etc) where there is a connector with hundreds of low-power pins, but several large high-current pins) they called it 'gatherability', where the connector would be able to align, even if there was an offset initially. It's important for servers etc because the people rapidly push and swap the cards, and so coarse and fine gatherability is needed in the connection method (coarse getting it roughly aligned as the connectors begin to approach each other, and fine gatherability as the connectors mate).

    This particular contact is press-fit, which makes it versatile I think.. the documentation mentions it can be press-fitted into a PCB, or metal bus-bars. One could even make custom battery packs in this way, with nice high-power connectors. Roadtesters would need some drilling experience, or PCB creating experience, and at least a vice/vise, if not a small arbor press. As Rod says, it could also have uses for R/C, high-power car audio (the amount of junk fuse-holders out there is ridiculous.. one could design a much nicer holder with these connectors).

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 7 years ago

    Interesting item. From speaking in the past to an engineer working on high-power connections in computer server modules (like disk drive caddys etc) where there is a connector with hundreds of low-power pins, but several large high-current pins) they called it 'gatherability', where the connector would be able to align, even if there was an offset initially. It's important for servers etc because the people rapidly push and swap the cards, and so coarse and fine gatherability is needed in the connection method (coarse getting it roughly aligned as the connectors begin to approach each other, and fine gatherability as the connectors mate).

    This particular contact is press-fit, which makes it versatile I think.. the documentation mentions it can be press-fitted into a PCB, or metal bus-bars. One could even make custom battery packs in this way, with nice high-power connectors. Roadtesters would need some drilling experience, or PCB creating experience, and at least a vice/vise, if not a small arbor press. As Rod says, it could also have uses for R/C, high-power car audio (the amount of junk fuse-holders out there is ridiculous.. one could design a much nicer holder with these connectors).

    • Cancel
    • Vote Up +6 Vote Down