RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum What Do You Think About This Product: Coeur CST High-Current Interconnect System
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 17 replies
  • Subscribers 2752 subscribers
  • Views 3204 views
  • Users 0 members are here
  • scasny
Related

What Do You Think About This Product: Coeur CST High-Current Interconnect System

rscasny
rscasny over 7 years ago

I often don't think about connectors and connection system reliability. I like many people assume a connector from a quality company works reliably to connect wire-to-board and board-to-board applications. But what happens when there are is a misalignment between the two members that are being interconnected? Contact stresses can occur. Stresses can impede ideal contact/pin mating and in some situations increase contact resistance. When currents run higher and higher, in the hundreds of amps, undesirable thermal conditions can occur.image

 

So, when I was introduced to this connection system -- Coeur CST High-Current Interconnect System -- which provides a degree of float to accommodate any misalignment, I found it interesting and wanted to share it with the rest of you.

 

The Coeur CST High-Current Interconnect System provides up to 1.0mm of float due to its wave spring float mechanism so entire core socket assembly moves within the float housing.I am told that it doesn't add stress on contacts in float position and it offers low mating forces. There's also no risk of resistance increase due to high contact beam deflection.image

 

It's rated between 30.0 and 200.0A connects PCBs, bus bars and cable. It's used in data centers, PDUs, electric vehicles. When I saw them, I thought they could be used in any number of power converter types, load center terminations, battery banks, and more.

 

I'm not sure how they could be roadtested, but I could get some sample kits if someone has a decent way to test them. I've been told they've gone through rigorous testing already. But maybe a roadtest could be fashioned more along the lines of experimenting and observing its floating mechanism. If you have any ideas, leave a comment.

 

Randall Scasny

RoadTest Program Manager

  • Sign in to reply
  • Cancel
Parents
  • rscasny
    rscasny over 7 years ago

    Hi Everyone.

     

    An Update.

     

    I've been told that I am received 3 sample kits of this CST connector. I don't have much more information than that (e.g., sizes, etc.)

     

    I would like to get three people who would be interested in receive the sample kit and writing a blog, giving your impressions of it and how you would use this type of connector. I'm not necessarily looking for the level of a roadtest (unless you had a plan and were interested in trying it out.) I guess I am looking for some feedback about the product. So it's kind of an open ended feedback. My goal is to let three people have some samples and then give some feedback to the community.

     

    Previously, I read that a number of you were interested in doing this. So, if you are really interested, you can leave a comment so I can see who is most interested in doing this blog.

     

    Thanks.

     

    Randall

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • three-phase
    three-phase over 7 years ago in reply to rscasny

    rscasny I am happy to test a set, but am also happy to act as a reserve, so if there are three others that are really keen, feel free to utilise them instead of me.

     

    Kind regards.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • three-phase
    three-phase over 7 years ago in reply to rscasny

    rscasny I am happy to test a set, but am also happy to act as a reserve, so if there are three others that are really keen, feel free to utilise them instead of me.

     

    Kind regards.