RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum RoadTest request: ICs that manage the power up sequence of a board
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 2750 subscribers
  • Views 1933 views
  • Users 0 members are here
Related

RoadTest request: ICs that manage the power up sequence of a board

Jan Cumps
Jan Cumps over 7 years ago

Many designs require that the power rails are enabled (and at shutdown disabled) in a certain sequence.

The controller voltage may have to be stablilised before the I/O voltage is activated, etc.

A lot of the development boards we use day-to-day have such a power management chip on-board. They are used for microcontrollers, FPGAs and many single board computers: Raspberry Pi uses one, the BeagleBone, several LaunchPads, Papilio FPGA boards...

 

Maybe, rscasny , you can ask IC suppliers if they are interested to run a RoadTest where such a solution can be validated?

It does not have to be an evaluation kit. The Road Test kit could be the raw IC, and the components you need to sense and switch rails?

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    shabaz over 7 years ago

    Hi Jan,

     

    Not to divert from your suggestion, this is just some info if it helps you in a design - I looked for a simple-to-use one recently, and went with LM3881. It doesn't have any features hehe, only does power sequencing (with no sensing of voltages), for up to 3 rails. It is an easy-to-solder package which was also another reason for me. I figured if I needed to monitor voltages, then (similar as michaelkellett mentions) I figured I could use a microcontroller to monitor the sequence and monitor the rails with an internal ADC, and signal to the LM3881 to reverse and shut down (but I'm not doing that for my current circuit).

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 7 years ago

    Hi Jan,

     

    Not to divert from your suggestion, this is just some info if it helps you in a design - I looked for a simple-to-use one recently, and went with LM3881. It doesn't have any features hehe, only does power sequencing (with no sensing of voltages), for up to 3 rails. It is an easy-to-solder package which was also another reason for me. I figured if I needed to monitor voltages, then (similar as michaelkellett mentions) I figured I could use a microcontroller to monitor the sequence and monitor the rails with an internal ADC, and signal to the LM3881 to reverse and shut down (but I'm not doing that for my current circuit).

    • Cancel
    • Vote Up +5 Vote Down