PICOSCOPE 5444D MSO -  USB Oscilloscope

Table of contents

image

 

{tabbedtable} Tab LabelTab Content
About

The PICOSCOPE 5444D MSO -  USB Oscilloscope is part of the PicoScope 5000D Series FlexRes oscilloscopes that provide 8 to 16 bits ofvertical resolution, with up to 200 MHz bandwidth and 1 GS/s sampling speed. You select the most appropriate hardware resolution for the requirements of each measurement.

image

PicoScopes include advanced features such as mask limit testing, serial decoding, advanced triggering, automatic measurements, math channels (including the ability to plot frequency and duty cycle against time), XY mode and segmented memory.  The PicoScope 5000D Series also benefits from Pico’s award-winning DeepMeasure™ feature and FlexRes

flexible resolution.

 

Features

  • Deep capture memory – from 128 million to 512 million samples
  • 2 or 4 analog channels • Mixed-signal models add 16 digital channels
  • Serial decoding – analyze 18 protocols • USB 3.0 connection for continuous high-speed data streaming
  • Small, light and portable
  • Supported by the free and regularly updated PicoScope 6 software, these devices offer an ideal, cost-effective package for many applications, including design, research, test, education, service and repair.

 

Pico FlexRes flexible resolution oscilloscopes allow you to reconfigure the scope hardware to increase either the sampling rate or the resolution. This means you can reconfigure the hardware to be either a fast (1 GS/s) 8-bit oscilloscope for looking at digital signals or a high-resolution 16-bit oscilloscope for audio work and other analog applications. Whether you’re capturing and decoding fast digital signals or looking for distortion in sensitive analog signals, FlexRes oscilloscopes are the answer.

Important Dates

Enrollment Begin: Aug 17 1018

Enrollment Ends: Sept 27 2018

RoadTesters Selected: Oct 24 2018

Product Shipped: Oct 26 2018

RoadTesting Begins: Nov 2 2018

Reminder/Update Email: Dec 2 2018*

Submit Reviews By: Jan 2 2019*

*The element14 RoadTest Staff will send this reminder/update email.

**If a RoadTester is unable to meet the deadline, please notify the RoadTest Program Lead, , as soon as possible before the deadline.

RoadTesters

T&Cs

PICOSCOPE 5444D MSO -  USB Oscilloscope

RoadTest

Terms and Conditions

These are the terms and conditions which govern the PICOSCOPE 5444D MSO -  USB Oscilloscope RoadTest contest. This Contest requires participants to submit an application indicating their previous experience with this type of equipment/component, information on what they would do to test the equipment/component, and the applicant’s desire to post a thorough review of their experience with images, photos, or other supplemental materials. Participants will be required to meet the Conditions for Participation.  The winners of this RoadTest will receive the item(s) listed below. RoadTest Reviews are due no later than 60 days after the receipt of the item(s). No other prizes are offered.

The Principal terms of the Competition:

The following words and phrases are used in these terms and conditions and have the meanings given to them below.

PICOSCOPE 5444D MSO -  USB Oscilloscope

(RoadTest or Contest)

Key dates:

Applications Close: midnight (GMT) on Sept 27 2018

Announcement of Winner (estimated): Oct 4 2018

Prize: PICOSCOPE 5444D MSO -  USB Oscilloscope

Additional Prizes: none

Competition Site: https://www.element14.com/community/groups/roadtest?ICID=menubar_resources_roadtest

Site or element14 Community: www.element14.com/community

Judges: members of the element14 community team chosen at the Organiser’s discretion.

Judging Criteria, All of the following which will have equal weighting:

· Demonstrated competence with the technologies including links or descriptions of past projects

· Qualifications as indicated by current job role and/or schooling/vocational training;

· A thorough description of how the prize would be tested;

· Likelihood that the Applicant will blog about the prize and provide a review on element14.com;

· Originality;

· Innovation.

Organiser: Premier Farnell plc (registered in England and Wales under company number 876412) whose registered office is at Farnell House, Forge Lane, Leeds, UK

Conditions for Qualification: in addition to meeting the requirements of these terms, all persons applying to take part in the Contest (each one an Applicant) must:

· Provide a RoadTest application describing what he/she would do if awarded the Prize including similar previous projects, product experience and qualifications

Terms: these terms and conditions which govern the Competition and to which the Organiser reserves the right to make changes from time to time and the latest version of these Terms from time to time will be posted to the Site.

  1. Eligibility
  2. Applications:
  3. Selecting Winners:
  4. Liability:
  5. General:

1.1 Save as set out in these Terms, the Contest is open to any natural or legal person, firm or company or group of natural persons or unincorporated body.

1.2 All Applicants must be aged at least 18 at the time of their application.

1.3 Applicants must not enter the RoadTest if doing so or taking part may:

1.3.1 cause the Organiser and/or themselves to be in breach of any agreement (including but not limited to any contract of employment) to which they are a party or in breach of any law, regulation or rule having the force of law to which the Organiser or the Applicant may be subject or any policy of the Organiser or the Sponsor;

1.3.2 Require the Organiser to obtain any licence, authorisation or permission to deal with the Applicant; or

1.3.3 Be in breach of any policy or practice of their employer. Some employers prohibit or restrict their employees from taking part in competitions such as these or receiving prizes under them and the Organiser respects those policies and practices.

The Organiser reserves the right to disqualify any Application made in breach of these Terms and to reject any Application which it reasonably believes may be or become in breach. The Organiser reserves the right to require evidence in such form as the Organiser may reasonably require of any Applicant’s compliance with any of these Terms and to disqualify any Applicant or Participant who cannot provide such evidence reasonably promptly.

1.4 Multiple applications are not permitted.

1.5 Applications may not be submitted by an agent whether acting on behalf of an undisclosed principal or otherwise.

1.6 The Contest is NOT open to:

1.6.1 Any person or entity who is a resident or national of any country which is subject to sanctions, embargoes or national trade restrictions of the United States of America, the European Union or the United Kingdom;

1.6.2 Any employee, director, member, shareholder (as appropriate) or any of their direct families (parents, siblings, spouse, partner, children) (“Direct Families”) of the Organiser and Sponsors; or

2.1 Each Applicant must fully complete and submit a RoadTest Application by the Application Close.

2.2 By submitting a Registration Form, each Applicant:

2.2.1 Authorises the Organiser to use his or her personal data (as defined in the Data Protection Act 1998) for the purposes of running and promoting the RoadTest;

2.2.2 Authorises the Organizer to copy, reproduce and publish their application should they be accepted as a Participant;

2.2.3 Will be deemed to have read, accepted and agree to be bound by these Terms. Applicants are advised to print and keep safe these Terms;

2.2.4 Authorises the Organiser to copy, reproduce and use the Application and/or Review for the purposes of the RoadTest and as otherwise contemplated by these Terms. The Organiser will not be responsible for any inaccuracy, error or omission contained in any reproduction or use of the Project Blogs.

2.2.5 Licenses the Organiser to use the intellectual property in the Project (IP) for the purposes of this Contest. As between the Applicant and the Organiser the IP remains owned by the Applicant.

2.2.6 Grants the Organiser the right to use his or her likeness, photographs, logos, trademarks, audio or video recordings without restriction for the purposes of Contest or the promotion of it or the Site;

2.2.7 Agrees to participate positively in all publicity surrounding the Contest;

2.2.8 Agrees to be responsible for all expenses and costs incurred by him or her in preparing for, entering and participating in the Contest (save for any expenses expressly agreed by the Organiser to be borne by it in these Terms);

2.2.9 Confirms that he or she owns all IP used in his or her application or Project or Blogs and indemnifies the Organiser from any claim by a third party that use of any material provided by an Applicant to the Organiser infringes the intellectual property rights of any third party;

2.2.10 Agrees not to act in any way or fail to act in any way or be associated with any cause or group which would have a negative impact on the reputation of the Organiser and/or the RoadTest.

2.3 All applications submitted to this RoadTest must meet the following criteria:

2.3.1 Applicants must be the author, creator and owner of the proposed review idea. Applicants must not submit someone else’s idea;

2.3.2 The proposed application must be reasonably achievable by the within the time constraints of the Contest;

2.3.3 Applications must not include or propose any of the following, the inclusion of which shall render any proposed application ineligible:

(a) Applications which relate to socially taboo topics, such as illicit drug use or sexual gratification;

(b) Applications that are or could reasonably be considered to be illegal, immoral, discriminatory or offensive as determined by the Organiser;

(c) Applications in relation to them which if accepted would infringe or breach any of the policies or terms of access or use of the Site.

2.4 No Application may contain any of the hazardous substances identified by Article 4 of Directive 2002/95/EC of the European Parliament on the Restrictions on the Use of Substances in Electronic and Electrical Equipment ("the Directive") or the use of such hazardous substances in the in any such Project must not exceed the maximum concentration values set out in the Directive.

3.1 Winners will be selected by the Organiser on the basis of the quality of his or her application and its adherence to these Terms.

3.2 The total number of Winners selected will be at least the minimum number set out above but the actual number is at the sole discretion of the Organizer and/or the Sponsor, if applicable.

3.3 The Organiser will use all reasonable efforts to announce the Winners via an update to the RoadTest page by the date listed above.

3.4 Winners agree to take part in all publicity which the Organiser or the Sponsor wishes to use to promote the RoadTest, the Products featured or other Contests with which the Organiser may be connected from time to time.

3.5 Details of the Winners may also be published in the media.

3.6 Winners are responsible for all applicable taxes, duties or other charges payable in relation to any prize.

3.7

4.1 The Organiser hereby excludes all and any Liability arising out of the Contest or the acceptance, use, quality, condition, suitability or performance of any Prize, even where that Liability may arise from the Organiser’s negligence.

4.2 Nothing in these Terms will affect any Liability of the Organiser for death or personal injury arising from its negligence, for breach of Part II of the Consumer Protection Act 1987 (in the event that any entrant is entitled to claim rights under the Consumer Protection Act 1987) or for any matter in relation to which it would be illegal for the Organiser to exclude or to attempt to exclude its Liability.

4.3 Subject to 4.2, neither the Organiser, any parent company nor any subsidiary of the Organiser or such parent company or any of their directors, officers and employees (together referred to in these terms and the ‘Associates’) makes any guarantee, warranty or representation of any kind, express or implied, with respect to this Competition or the Prizes potentially available under it. Neither the Organiser nor any of its Associates shall be responsible for any Liability that may arise out of or in connection with person’s participation in this Competition, the claiming, redemption or value of any prizes under it, the use or enjoyment of such prizes or any events or circumstances arising out of or in connection with any of them. Any implied warranties of condition, merchantability or suitability or fitness for purpose of any of them are hereby expressly excluded. Wherever used in these Terms, ‘Liability’ shall mean any and all costs, expenses, claims, damages, actions, proceedings, demands, losses and other liabilities (including legal fees and costs on a full indemnity basis) arising directly or indirectly out of or in connection with the matter concerned.

5.1 The RoadTest is organised and sponsored by the Organiser. The Organiser reserves the right to delegate all or any of its powers, rights and obligations arising in relation to the RoadTest to any Associate and certain such rights and powers are assumed by the Organiser on behalf of itself and each Associate. Reference to “Organiser” shall be deemed to include reference to each Associate.

5.2 The RoadTest may be terminated at any time if there are, in the sole opinion of the Organiser, an insufficient number of entries, or if the Applications are not of an appropriate standard for a competition of this nature. The Organiser has the right to cancel or suspend the RoadTest at any time due to circumstances outside its reasonable control.

5.3 The Organiser shall have the sole discretion to disqualify (without correspondence or right of appeal) any Applicant it considers to be adversely affecting the process or the operation of the RoadTest or to be in breach of these Terms or to be acting in a disruptive manner or with intent to annoy, abuse, threaten or harass any other Applicant or Participant.

5.4 The Organiser has the right to amend or add to these Terms from time to time. Revised Terms and Conditions will be posted on the Contest Site and it is a condition of entry to the RoadTest that Applicants agree to comply with these Terms and, if appropriate, such Terms as amended from time to time.

5.5 Headings are for convenience only and do not affect the interpretation or construction of these Terms and Conditions.

5.6 These Terms and the operation of the Contest shall be governed by and construed in accordance with English Law and any claim or matter arising under these Terms shall be subject to the exclusive jurisdiction of the English courts.

Comment List
Anonymous
  • Randall,

     

    I know you have a tough task and get many suggestions, but maybe the next best step would be to send to those 63 incomplete applicants a note telling them their applications were incomplete so they won't continue to send in incomplete entries.  You don't have to be detailed, but a thumbs up or down may be useful.

     

    Gordon

  • Update

     

    I went through all the applications. of the 94 applications, 31 (or 33%) submitted complete applications. Thanks.

     

    In these 31 applications, there are experience roadtesters, teachers, researchers and 2 new members/roadtesters.

     

    What's the difference between an incomplete versus a complete application:

     

    A complete application provides answers to these questions:

     

    (a) What is your background?

    (b) Why you are applying for this roadtest?

    (c) What is your testing procedure?

    (d) Give some examples of your element14 community participation

    (e) Please verify that you can complete the testing and review writing on element14 within 60 days from the receipt of the product.

  • I extended this for a day already. I think I ran this roadtest 10 days longer than usual. so, people had enough time to apply.

     

    Randall Scasny

    RoadTest Program Manager

  • Is it possible to extend by few hours, The link expire two hours before the deadline.

  • I find that USB Scopes are easier to use when it comes to quickly analyzing something and exporting data: emailing a screenshot, saving the data to a local file for later analysis, or automating some testing using SDK features.

    They also occupy less space, so they can be permanently kept on the desk, which in turn means that they're a lot quicker to turn on and use if required. As you mentioned, the sample depth is certainly nice to have.

     

    Navigation on a scope is definitely easier because of the knobs/buttons, but I've used some desktop software which comes pretty close in terms of navigation using keyboard shortcuts + the mouse scrollwheel .

  • I agree with Gough. Although i used to work at Agilent (now Keysight) and have used both its box and modular (USB similar to picoscope) type, i have to say there are occasion a USB scope is more relevant. In an actual scenario i have developed an industrial automation tester (not at Agilent) to collect sampled signal of brushless dc motor for 30s. due to the relatively high sample rate, the memory depth of a box instrument is not feasible. in addition, we need multiple channels (one BLDC motor have UVW for example) and a box instrument will quickly take up the rack space and not practical to place more than one of them. I have in facted used 3 pieces of picoscope and it is much more space saving than a single box oscillopscope and at the same time provide more than 10x memory depth of a box scope, and at a price cheaper than the box scope too. On the hindsight, the picoscope i used back then doesn't the VISA interface and we have to use the software SDK way to control it.

     

    At a glance the 5444 has continued the picoscope tradition of high memory depth. there are multiple features on current generation like MSO and serial decoding capability which i think is easier to deal with on a PC screen than on a crowded box scope screen. i would still think for many use cases especially industrial automation and troubleshooting the small size picoscope have a lot strength. it is also interesting to find that all of the other capabilities of 5444 such as serial decoding, MSO, function generator, spectrum analyzer doesn't need extra paid option, whereas for box instrument many are $$$ option.

  • Ah, I see. I've no answer to that that you won't have already thought of. image

     

    Hope all is good otherwise .image

     

    Carl

  • Yes, the scope was supplied with x1/x10 probes but the apparatus and environment where I work means that I rarely use these for the connection methodology.

     

    Kind regards

  • Hi Donald,

    Good to hear that your PicoScope 3404A is proving it's worth for you.

     

    I think the probes supplied with the 3404A were x1/x10 switchable so using in x10 and setting the probes scale accordingly means the range of the scope becomes +/-200V

     

    Best regards

    Carl - Pico.

  •   wrote:

    How's the PicoScope software? Waveforms (by Digilent for the AD2) has tons of features.

    You can download and use the PicoScope software offline to get an idea for yourself. It is a fully featured scope software. Its capabilities are on-par with high-end Windows-based benchtop instruments. The only limitations are the limits of the acquisition hardware. When I reviewed the lower BW PicoScope, I was very surprised to see the software competed well with a high-end Agilent Infiniium.

     

    Advanced math. Custom math. User definable probes settings. Flexible viewports. FFT. Serial decoding. Plus all of the standard stuff you'd expect a Windows-based scope to support.