Avnet Ultra96 Dev Board

View table of contents ...  

image

Join the Webinar: What Can I Do with Programmable Logic?

 

{tabbedtable} Tab LabelTab Content
About

Ultra96™ is an ARM-based, Xilinx Zynq UltraScale+™ MPSoC development board based on the Linaro 96Boards specification.

image

The 96Boards’ specifications are open and define a standard board layout for development platforms that can be used by software application, hardware device, kernel, and other system software developers.Ultra96 represents a unique position in the 96Boards community with a wide range of potential peripherals and acceleration engines in the programmable logic that is not available from other offerings.

 

Ultra96 boots from the provided Delkin 16 GB MicroSD card, pre-loaded with PetaLinux. Engineers have options of connecting to Ultra96 through a Webserver using integrated wireless access point capability or to use the provided PetaLinux desktop environment which can be viewed on the integrated Mini DisplayPort video output. Multiple application examples and on-board development options are provided as examples.

 

Ultra96 provides four user-controllable LEDs. Engineers may also interact with the board through the 96Boards compatible low-speed and high-speed expansion connectors by adding peripheral accessories such as those included in Seed Studio’s Grove Starter Kit for 96Boards.

 

Micron LPDDR4 memory provides 2 GB of RAM in a 512M x 32 configuration. Wireless options include 802.11b/g/n Wi-Fi and Bluetooth 4.2 (provides both Bluetooth Classic and Low Energy (BLE)). UARTs are accessible on a header as well as through the expansion connector. JTAG is available through a header (external USB-JTAG required). I2C is available through the expansion connector.

 

Ultra96 provides one upstream (device) and two downstream (host) USB 3.0 connections. A USB 2.0 downstream (host) interface is provided on the high speed expansion bus. Two Microchip USB3320 USB 2.0 ULPI Transceivers and one Microchip USB5744 4-Port SS/HS USB Controller Hub are specified. The integrated power supply generates all on-board voltages from an external 12V supply (available as an accessory).

 

FEATURES

  • Xilinx Zynq UltraScale+ MPSoC ZU3EG A484
  • Micron 2 GB (512M x32) LPDDR4 Memory
  • Delkin 16 GB MicroSD card + adapter
  • Pre-loaded with PetaLinux environment
  • Wi-Fi / Bluetooth
  • Mini DisplayPort (MiniDP or mDP)
  • 1x USB 3.0 Type Micro-B upstream port
  • 2x USB 3.0, 1x USB 2.0 Type A downstream ports
  • 40-pin 96Boards Low-speed expansion header
  • 60-pin 96Boards High speed expansion header
  • 85mm x 54mm form factor
  • Linaro 96Boards Consumer Edition compatible

 

CONTENTS

  • Ultra96 development board
  • 16 GB pre-loaded MicroSD card + adapter
  • Voucher for SDSoC license from Xilinx
  • Quick-start instruction card
  • External 12V @ 2.0A power supply (provided by element14)
  • USB-to-JTAG/UART pod (provided by element14)
Important Dates

Enrollment Begin: Aug 21 1018

Enrollment Ends: Oct 24 2018

RoadTesters Selected: Oct 29 2018

Product Shipped: Oct 30 2018

RoadTesting Begins: Nov 6 2018

Reminder/Update Email: Dec 6 2018*

Submit Reviews By: Jan 6 2019*

*The element14 RoadTest Staff will send this reminder/update email.

**If a RoadTester is unable to meet the deadline, please notify the RoadTest Program Lead, , as soon as possible before the deadline.

RoadTesters

T&Cs

Avnet Ultra96 Dev Board

RoadTest

Terms and Conditions

These are the terms and conditions which govern the Avnet Ultra96 Dev Board RoadTest contest. This Contest requires participants to submit an application indicating their previous experience with this type of equipment/component, information on what they would do to test the equipment/component, and the applicant’s desire to post a thorough review of their experience with images, photos, or other supplemental materials. Participants will be required to meet the Conditions for Participation.  The winners of this RoadTest will receive the item(s) listed below. RoadTest Reviews are due no later than 60 days after the receipt of the item(s). No other prizes are offered.

The Principal terms of the Competition:

The following words and phrases are used in these terms and conditions and have the meanings given to them below.

Avnet Ultra96 Dev Board

(RoadTest or Contest)

Key dates:

Applications Close: midnight (GMT) on Oct 24 2018

Announcement of Winner (estimated): Oct 26 2018

Prize: Avnet Ultra96 Dev Board

Additional Prizes: none

Competition Site: https://www.element14.com/community/groups/roadtest?ICID=menubar_resources_roadtest

Site or element14 Community: www.element14.com/community

Judges: members of the element14 community team chosen at the Organiser’s discretion.

Judging Criteria, All of the following which will have equal weighting:

· Demonstrated competence with the technologies including links or descriptions of past projects

· Qualifications as indicated by current job role and/or schooling/vocational training;

· A thorough description of how the prize would be tested;

· Likelihood that the Applicant will blog about the prize and provide a review on element14.com;

· Originality;

· Innovation.

Organiser: Premier Farnell plc (registered in England and Wales under company number 876412) whose registered office is at Farnell House, Forge Lane, Leeds, UK

Conditions for Qualification: in addition to meeting the requirements of these terms, all persons applying to take part in the Contest (each one an Applicant) must:

· Provide a RoadTest application describing what he/she would do if awarded the Prize including similar previous projects, product experience and qualifications

Terms: these terms and conditions which govern the Competition and to which the Organiser reserves the right to make changes from time to time and the latest version of these Terms from time to time will be posted to the Site.

  1. Eligibility
  2. Applications:
  3. Selecting Winners:
  4. Liability:
  5. General:

1.1 Save as set out in these Terms, the Contest is open to any natural or legal person, firm or company or group of natural persons or unincorporated body.

1.2 All Applicants must be aged at least 18 at the time of their application.

1.3 Applicants must not enter the RoadTest if doing so or taking part may:

1.3.1 cause the Organiser and/or themselves to be in breach of any agreement (including but not limited to any contract of employment) to which they are a party or in breach of any law, regulation or rule having the force of law to which the Organiser or the Applicant may be subject or any policy of the Organiser or the Sponsor;

1.3.2 Require the Organiser to obtain any licence, authorisation or permission to deal with the Applicant; or

1.3.3 Be in breach of any policy or practice of their employer. Some employers prohibit or restrict their employees from taking part in competitions such as these or receiving prizes under them and the Organiser respects those policies and practices.

The Organiser reserves the right to disqualify any Application made in breach of these Terms and to reject any Application which it reasonably believes may be or become in breach. The Organiser reserves the right to require evidence in such form as the Organiser may reasonably require of any Applicant’s compliance with any of these Terms and to disqualify any Applicant or Participant who cannot provide such evidence reasonably promptly.

1.4 Multiple applications are not permitted.

1.5 Applications may not be submitted by an agent whether acting on behalf of an undisclosed principal or otherwise.

1.6 The Contest is NOT open to:

1.6.1 Any person or entity who is a resident or national of any country which is subject to sanctions, embargoes or national trade restrictions of the United States of America, the European Union or the United Kingdom;

1.6.2 Any employee, director, member, shareholder (as appropriate) or any of their direct families (parents, siblings, spouse, partner, children) (“Direct Families”) of the Organiser and Sponsors; or

2.1 Each Applicant must fully complete and submit a RoadTest Application by the Application Close.

2.2 By submitting a Registration Form, each Applicant:

2.2.1 Authorises the Organiser to use his or her personal data (as defined in the Data Protection Act 1998) for the purposes of running and promoting the RoadTest;

2.2.2 Authorises the Organizer to copy, reproduce and publish their application should they be accepted as a Participant;

2.2.3 Will be deemed to have read, accepted and agree to be bound by these Terms. Applicants are advised to print and keep safe these Terms;

2.2.4 Authorises the Organiser to copy, reproduce and use the Application and/or Review for the purposes of the RoadTest and as otherwise contemplated by these Terms. The Organiser will not be responsible for any inaccuracy, error or omission contained in any reproduction or use of the Project Blogs.

2.2.5 Licenses the Organiser to use the intellectual property in the Project (IP) for the purposes of this Contest. As between the Applicant and the Organiser the IP remains owned by the Applicant.

2.2.6 Grants the Organiser the right to use his or her likeness, photographs, logos, trademarks, audio or video recordings without restriction for the purposes of Contest or the promotion of it or the Site;

2.2.7 Agrees to participate positively in all publicity surrounding the Contest;

2.2.8 Agrees to be responsible for all expenses and costs incurred by him or her in preparing for, entering and participating in the Contest (save for any expenses expressly agreed by the Organiser to be borne by it in these Terms);

2.2.9 Confirms that he or she owns all IP used in his or her application or Project or Blogs and indemnifies the Organiser from any claim by a third party that use of any material provided by an Applicant to the Organiser infringes the intellectual property rights of any third party;

2.2.10 Agrees not to act in any way or fail to act in any way or be associated with any cause or group which would have a negative impact on the reputation of the Organiser and/or the RoadTest.

2.3 All applications submitted to this RoadTest must meet the following criteria:

2.3.1 Applicants must be the author, creator and owner of the proposed review idea. Applicants must not submit someone else’s idea;

2.3.2 The proposed application must be reasonably achievable by the within the time constraints of the Contest;

2.3.3 Applications must not include or propose any of the following, the inclusion of which shall render any proposed application ineligible:

(a) Applications which relate to socially taboo topics, such as illicit drug use or sexual gratification;

(b) Applications that are or could reasonably be considered to be illegal, immoral, discriminatory or offensive as determined by the Organiser;

(c) Applications in relation to them which if accepted would infringe or breach any of the policies or terms of access or use of the Site.

2.4 No Application may contain any of the hazardous substances identified by Article 4 of Directive 2002/95/EC of the European Parliament on the Restrictions on the Use of Substances in Electronic and Electrical Equipment ("the Directive") or the use of such hazardous substances in the in any such Project must not exceed the maximum concentration values set out in the Directive.

3.1 Winners will be selected by the Organiser on the basis of the quality of his or her application and its adherence to these Terms.

3.2 The total number of Winners selected will be at least the minimum number set out above but the actual number is at the sole discretion of the Organizer and/or the Sponsor, if applicable.

3.3 The Organiser will use all reasonable efforts to announce the Winners via an update to the RoadTest page by the date listed above.

3.4 Winners agree to take part in all publicity which the Organiser or the Sponsor wishes to use to promote the RoadTest, the Products featured or other Contests with which the Organiser may be connected from time to time.

3.5 Details of the Winners may also be published in the media.

3.6 Winners are responsible for all applicable taxes, duties or other charges payable in relation to any prize.

3.7

4.1 The Organiser hereby excludes all and any Liability arising out of the Contest or the acceptance, use, quality, condition, suitability or performance of any Prize, even where that Liability may arise from the Organiser’s negligence.

4.2 Nothing in these Terms will affect any Liability of the Organiser for death or personal injury arising from its negligence, for breach of Part II of the Consumer Protection Act 1987 (in the event that any entrant is entitled to claim rights under the Consumer Protection Act 1987) or for any matter in relation to which it would be illegal for the Organiser to exclude or to attempt to exclude its Liability.

4.3 Subject to 4.2, neither the Organiser, any parent company nor any subsidiary of the Organiser or such parent company or any of their directors, officers and employees (together referred to in these terms and the ‘Associates’) makes any guarantee, warranty or representation of any kind, express or implied, with respect to this Competition or the Prizes potentially available under it. Neither the Organiser nor any of its Associates shall be responsible for any Liability that may arise out of or in connection with person’s participation in this Competition, the claiming, redemption or value of any prizes under it, the use or enjoyment of such prizes or any events or circumstances arising out of or in connection with any of them. Any implied warranties of condition, merchantability or suitability or fitness for purpose of any of them are hereby expressly excluded. Wherever used in these Terms, ‘Liability’ shall mean any and all costs, expenses, claims, damages, actions, proceedings, demands, losses and other liabilities (including legal fees and costs on a full indemnity basis) arising directly or indirectly out of or in connection with the matter concerned.

5.1 The RoadTest is organised and sponsored by the Organiser. The Organiser reserves the right to delegate all or any of its powers, rights and obligations arising in relation to the RoadTest to any Associate and certain such rights and powers are assumed by the Organiser on behalf of itself and each Associate. Reference to “Organiser” shall be deemed to include reference to each Associate.

5.2 The RoadTest may be terminated at any time if there are, in the sole opinion of the Organiser, an insufficient number of entries, or if the Applications are not of an appropriate standard for a competition of this nature. The Organiser has the right to cancel or suspend the RoadTest at any time due to circumstances outside its reasonable control.

5.3 The Organiser shall have the sole discretion to disqualify (without correspondence or right of appeal) any Applicant it considers to be adversely affecting the process or the operation of the RoadTest or to be in breach of these Terms or to be acting in a disruptive manner or with intent to annoy, abuse, threaten or harass any other Applicant or Participant.

5.4 The Organiser has the right to amend or add to these Terms from time to time. Revised Terms and Conditions will be posted on the Contest Site and it is a condition of entry to the RoadTest that Applicants agree to comply with these Terms and, if appropriate, such Terms as amended from time to time.

5.5 Headings are for convenience only and do not affect the interpretation or construction of these Terms and Conditions.

5.6 These Terms and the operation of the Contest shall be governed by and construed in accordance with English Law and any claim or matter arising under these Terms shall be subject to the exclusive jurisdiction of the English courts.

RoadTest Reviews
Comments
Anonymous
  • The UltraZed-EV also supports the VCU.  I believe it also costs less than a ZCU104.  It is still much more than a Ultra96, but it is certainly an option as the IO for this has many video standards built in.

     

    --Dan

  • Hi Cheah Wei,

     

    Try the VCP Drivers from https://www.ftdichip.com/Drivers/VCP.htm

    Choose the correct driver based on your Windows version (32-bit or 64-bit).

  • The included driver on the board seems to be linux only. Attempting to update driver in the device manager pointing to the 'linux driver' will have this problem

    do you know where we can download this driver?

    image

    image

     

    Anyway, i am doing some blogs to capture my experiment with the ultra96

    A first taste of Zynq UltraScale+ MPSoC #overview of the family

  • Hey Cliff, Sorry was busy with my exams ;(

    I am not really sure what you are asking here. You want to send a text  message from one core of the CPU to another?

    I  don't see the point of such a task. Cause I believe both the cores would be sharing the same memory. Probably each of them would have individual caches. I am not sure if there is any pre-defined function for each of them, you might have to give it a try in assembly using threads (worst case scenario)

  • Hi Eashan, sorry for the long delay.

    Thanks for the information on the debugger - I really hope that the Hardware (System) Debugger is still alive and well in Vivado 2018.x.  It's a great way to do what I want to do.

    See my post from a few moments ago to Joshua Foster if you'd like to see what I am trying to accomplish - any suggestions you may have that I can get working quickly would be greatly appreciated.

    Thanks again for your help.

    Cliff

  • Hi Joshua, sorry for the long delay in getting back to you.  Bronchitis is not my friend...

    My goal in using the hardware (system) debugger was to test messaging between cores of the A53 and the R5.  Dual multi-core processors on the same silicon is a big strength of the Ultrascale+ MPSOC.  I wanted to use the hardware (system) debugger to display messages sent and received between the cores.

    I'm expecting displays of messages like: "A53 Core 1 sending to R5 Core 1 'test message'", then "R5 Core 1 received from A53 Core 1 "Test Message".  It's a poor man's IPC but it is enough for now.

    If there is another way to have messages displayed on a console (TeraTerm, Vivado, or any other easily adapted software) I'll be glad to try that.

    Thanks again for your help.

    Cliff

  • Hi Josh,

     

    Pads were lifted (severed from the traces) and the board did not boot-up from the SD card.

    I left the board idle for a week to find some tools.

     

    Current workaround  hack was to solder two 100 ohm resistors 0603 to the GND pad of the fan. Kind of dangerous since 12 V pad is close to it.

     

    That's all.

    Dimiter

  • Hi,

    Did you install the included driver? If not please try that.

     

    Thanks,

    -Josh

  • Hi Dimiterk,

     

    Can you please inform me on the manufacturing defect a bit more. Are the pads still intact on the switch? Does it look like the switch simply lifted away from them during the manufacturing process?

     

    I will pass this along to manufacturing.


    Thank you,

    Josh

  • When I received the board I found the JTAG/SD boot switch was knocked out somehow. pins were slanted at a weird angle. Kind of surprised this passed QA. I notified Element 14 guys about this then.

    Anyways , I managed to fix it by soldering two resistors between pins and fan GND pin. Kind of flaky though.

    image

     

    image

     

    Some minor beefs with this , Compiling  a small design with this board taken anywhere from 70 to 120 minutes initially.

     

    Another important thing is that mini-Display to VGA adapters from Ebay won't work since they have to be active ones. Thanks to Canada Post strike I don't have time to test one.

     

    I plan to post a review in a couple of weeks. Board is quite powerful but there are some minor points which make the experience less smooth than it should be.

  • i do face a small problem, i am using windows 8.1, the serial port driver is not successfully installed.

    i forever see the "installing device" window on the windows.this is with regards to https://ultra96-pynq.readthedocs.io/en/latest/getting_started.html

     

    When the USB cable is connected, an Ethernet device should be detected automatically on the host computer (Windows/Linux). A driver should already be available in Windows 10 and Linux. In Windows 7 a driver should start to install automatically when the board is connected.

  • i have tried the board too and it is certainly fun enough. was surprise to get the webcam up easily.

  • Hi Cliff,

    Yes that is correct. We do not include a TCl file to set the parameters. After the Board Defenition Files are installed, when you go to create a new project you will be prompted to choose either a device to target or you may choose a board to target. Select the board tab and look for the Ultra96.

    -Josh

  • Thanks Josh, I was able to locate the board definition file and was looking for a tcl file to set board parameters.  Is that done through the xml file now?

    Thanks Again

  • Hello Cliff, Randall had mentioned that he has 2 boards for project builds. My query was about those.

     

    Thanks,

    Nitin

  • Hi Cliff,

    You can find the board definition file for the Ultra96 and how to install in located on this web page.

     

    Thanks!

    Josh

  • I do remember hitting into one of these errors long  before. I suggest the following :

    a) Install the correct windows drivers. If in linux, check the connection with the board through dmesg and minicom.

    b) Use one of the other options. That is to say, use Launch on Hardware (GDB). I have heard that from 2017+ onwards, SDK has removed support for System Debugger.

    I am sure one of the two options can fix your problem. Do update us on the results.

  • Is there a "presets" script for the Ultra96 board, similar to the one for the MicroZed?  I'm hoping that there is and that it provides something that is obviously missing from my configuration.

    Thanks

     

    cross-posted to the Xilinx forum

  • Hi Cliff,

     

    Does the JTAG Pod enumerate in teraterm? Or some other serial console?

    Also in Vivados hardware manager when your U96 is connected to the JTAG POD, and is also configured for JTAG boot, can you see the zynq MPSoC device in the JTAG chain?

     

    -Josh

  • Hello Nitin, thanks for your reply.

    I'm not sure what you meant.  Can you restate your reply?

    Thanks

    Cliff