3 Series MDO Mixed Domain Oscilloscope

Table of contents

image

 

{tabbedtable} Tab LabelTab Content
About

The 3 Series MDO minimizes rack or bench space by integrating multiple instrument, which combines analog, digital, and RF measurements with a signal source in a single, small (5.9 in., 149 mm deep) instrument. The combination of a small instrument and high level of integration aids in the teaching of various electronics principles as well as in its usage for more sophisticated lab experiments. Fully upgradable bandwidths and options enable adding functionality over time.

image

Installed Options

  • 1GHz bandwidth for analog channels
  • Arbitrary Function Generator
  • 16-digital channels
  • Spectrum analyzer, input frequency range 9khz to 3 Ghz and capture bandwidth 3 Ghz
  • Embedded serial triggering and analysis (I2C and SPI)

 

Main Features

  • 4 analog channel model
  • Large 11.6" (1920 x 1080 HD resolution) capacitive touch display, highly intuitive user interface
  • 1 GHz bandwidth version installed
  • Up to 5 GS/s sample rate
  • 10 M record length on all channels
  • >280,000 wfm/s maximum waveform capture rate
  • Standard passive voltage probes with 3.9 pF capacitive loading and 250 MHz or 500 MHz analog bandwidth
  • A DVM/frequency counter added at no cost following product registration
  • Option to add spectrum analyzer hardware at 1GHz or 3GHz
  • Debug complicated embedded designs with a wide range of serial decodes
  • 6-in-1 instrument integration

 

Applications

  • Aerospace, Defence, Military, Electronics Design, Embedded Design & Development, Lighting, Motor Drive & Control, Power Management, Power Supplies, Research & Development, Sensing & Instrumentation, Wireless

 

Contents

  • MDO34, One TPP0500 500 MHz passive probe per analog channel, Power cord, Calibration certificate documenting traceability to National Metrology Institute(s) and ISO9001/ISO17025 quality system registration, 3-year warranty covering all parts and labor on the instrument. 1-year warranty, parts and labor, on included probes.

 

Additional Information

Important Dates

Enrollment Begin: Sept 24 2019

Enrollment Ends: Oct 30 2019

RoadTesters Selected: Nov 21 2019

Product Shipped: Nov 21 2019

RoadTesting Begins: Nov 29 2019

Reminder/Update Email: Dec 29 2019

Submit Reviews By: Jan 29 2020

*The element14 RoadTest Staff will send this reminder/update email.

**If a RoadTester is unable to meet the deadline, please notify the RoadTest Program Lead, , as soon as possible before the deadline.

RoadTesters

Terms and Conditions

 

Roadtest

Terms and Conditions

Tektronix 3 Series MDO Mixed Domain Oscilloscope

 

These are the terms and conditions which govern the Tektronix 3 Series MDO

Mixed Domain Oscilloscope contest. This Contest requires participants to submit an application indicating their previous experience with this type of equipment/component, information on what they would do to test the equipment/component, and the applicant’s desire to post a thorough review of their experience with images, photos, or other supplemental materials. Participants will be required to meet the Conditions for Participation.  The winners of this RoadTest will receive the item(s) listed below. RoadTest Reviews are due no later than 60 days after the receipt of the item(s). No other prizes are offered.

 

The Principal terms of the Competition:

The following words and phrases are used in these terms and conditions and have the meanings given to them below.

(RoadTest or Contest)

Key dates:

Applications Close: midnight (GMT) on Oct 30 2019

Announcement of Winner (estimated): Nov 10 2019

Prize:

3 Series MDO Mixed Domain Oscilloscope

 

Additional Prizes: none

Competition Site: https://www.element14.com/community/groups/roadtest?ICID=menubar_resources_roadtest

Site or element14 Community: www.element14.com/community

Judges: members of the element14 community team chosen at the Organiser’s discretion.

Judging Criteria, All of the following which will have equal weighting:

· Demonstrated competence with the technologies including links or descriptions of past projects

· Qualifications as indicated by current job role and/or schooling/vocational training;

· A thorough description of how the prize would be tested;

· Likelihood that the Applicant will blog about the prize and provide a review on element14.com;

· Originality;

· Innovation.

Organiser: Premier Farnell plc (registered in England and Wales under company number 876412) whose registered office is at Farnell House, Forge Lane, Leeds, UK

Conditions for Qualification: in addition to meeting the requirements of these terms, all persons applying to take part in the Contest (each one an Applicant) must:

· Provide a RoadTest application describing what he/she would do if awarded the Prize including similar previous projects, product experience and qualifications

Terms: these terms and conditions which govern the Competition and to which the Organiser reserves the right to make changes from time to time and the latest version of these Terms from time to time will be posted to the Site.

  1. Eligibility
  2. Applications:
  3. Selecting Winners:
  4. Liability:
  5. General:

1.1 Save as set out in these Terms, the Contest is open to any natural or legal person, firm or company or group of natural persons or unincorporated body.

1.2 All Applicants must be aged at least 18 at the time of their application.

1.3 Applicants must not enter the RoadTest if doing so or taking part may:

1.3.1 cause the Organiser and/or themselves to be in breach of any agreement (including but not limited to any contract of employment) to which they are a party or in breach of any law, regulation or rule having the force of law to which the Organiser or the Applicant may be subject or any policy of the Organiser or the Sponsor;

1.3.2 Require the Organiser to obtain any licence, authorisation or permission to deal with the Applicant; or

1.3.3 Be in breach of any policy or practice of their employer. Some employers prohibit or restrict their employees from taking part in competitions such as these or receiving prizes under them and the Organiser respects those policies and practices.

The Organiser reserves the right to disqualify any Application made in breach of these Terms and to reject any Application which it reasonably believes may be or become in breach. The Organiser reserves the right to require evidence in such form as the Organiser may reasonably require of any Applicant’s compliance with any of these Terms and to disqualify any Applicant or Participant who cannot provide such evidence reasonably promptly.

1.4 Multiple applications are not permitted.

1.5 Applications may not be submitted by an agent whether acting on behalf of an undisclosed principal or otherwise.

1.6 The Contest is NOT open to:

1.6.1 Any person or entity who is a resident or national of any country which is subject to sanctions, embargoes or national trade restrictions of the United States of America, the European Union or the United Kingdom;

1.6.2 Any employee, director, member, shareholder (as appropriate) or any of their direct families (parents, siblings, spouse, partner, children) (“Direct Families”) of the Organiser and Sponsors; or

2.1 Each Applicant must fully complete and submit a RoadTest Application by the Application Close.

2.2 By submitting a Registration Form, each Applicant:

2.2.1 Authorises the Organiser to use his or her personal data (as defined in the Data Protection Act 1998) for the purposes of running and promoting the RoadTest;

2.2.2 Authorises the Organizer to copy, reproduce and publish their application should they be accepted as a Participant;

2.2.3 Will be deemed to have read, accepted and agree to be bound by these Terms. Applicants are advised to print and keep safe these Terms;

2.2.4 Authorises the Organiser to copy, reproduce and use the Application and/or Review for the purposes of the RoadTest and as otherwise contemplated by these Terms. The Organiser will not be responsible for any inaccuracy, error or omission contained in any reproduction or use of the Project Blogs.

2.2.5 Licenses the Organiser to use the intellectual property in the Project (IP) for the purposes of this Contest. As between the Applicant and the Organiser the IP remains owned by the Applicant.

2.2.6 Grants the Organiser the right to use his or her likeness, photographs, logos, trademarks, audio or video recordings without restriction for the purposes of Contest or the promotion of it or the Site;

2.2.7 Agrees to participate positively in all publicity surrounding the Contest;

2.2.8 Agrees to be responsible for all expenses and costs incurred by him or her in preparing for, entering and participating in the Contest (save for any expenses expressly agreed by the Organiser to be borne by it in these Terms);

2.2.9 Confirms that he or she owns all IP used in his or her application or Project or Blogs and indemnifies the Organiser from any claim by a third party that use of any material provided by an Applicant to the Organiser infringes the intellectual property rights of any third party;

2.2.10 Agrees not to act in any way or fail to act in any way or be associated with any cause or group which would have a negative impact on the reputation of the Organiser and/or the RoadTest.

2.3 All applications submitted to this RoadTest must meet the following criteria:

2.3.1 Applicants must be the author, creator and owner of the proposed review idea. Applicants must not submit someone else’s idea;

2.3.2 The proposed application must be reasonably achievable by the within the time constraints of the Contest;

2.3.3 Applications must not include or propose any of the following, the inclusion of which shall render any proposed application ineligible:

(a) Applications which relate to socially taboo topics, such as illicit drug use or sexual gratification;

(b) Applications that are or could reasonably be considered to be illegal, immoral, discriminatory or offensive as determined by the Organiser;

(c) Applications in relation to them which if accepted would infringe or breach any of the policies or terms of access or use of the Site.

2.4 No Application may contain any of the hazardous substances identified by Article 4 of Directive 2002/95/EC of the European Parliament on the Restrictions on the Use of Substances in Electronic and Electrical Equipment ("the Directive") or the use of such hazardous substances in the in any such Project must not exceed the maximum concentration values set out in the Directive.

3.1 Winners will be selected by the Organiser on the basis of the quality of his or her application and its adherence to these Terms.

3.2 The total number of Winners selected will be at least the minimum number set out above but the actual number is at the sole discretion of the Organizer and/or the Sponsor, if applicable.

3.3 The Organiser will use all reasonable efforts to announce the Winners via an update to the RoadTest page by the date listed above.

3.4 Winners agree to take part in all publicity which the Organiser or the Sponsor wishes to use to promote the RoadTest, the Products featured or other Contests with which the Organiser may be connected from time to time.

3.5 Details of the Winners may also be published in the media.

3.6 Winners are responsible for all applicable taxes, duties or other charges payable in relation to any prize.

3.7

4.1 The Organiser hereby excludes all and any Liability arising out of the Contest or the acceptance, use, quality, condition, suitability or performance of any Prize, even where that Liability may arise from the Organiser’s negligence.

4.2 Nothing in these Terms will affect any Liability of the Organiser for death or personal injury arising from its negligence, for breach of Part II of the Consumer Protection Act 1987 (in the event that any entrant is entitled to claim rights under the Consumer Protection Act 1987) or for any matter in relation to which it would be illegal for the Organiser to exclude or to attempt to exclude its Liability.

4.3 Subject to 4.2, neither the Organiser, any parent company nor any subsidiary of the Organiser or such parent company or any of their directors, officers and employees (together referred to in these terms and the ‘Associates’) makes any guarantee, warranty or representation of any kind, express or implied, with respect to this Competition or the Prizes potentially available under it. Neither the Organiser nor any of its Associates shall be responsible for any Liability that may arise out of or in connection with person’s participation in this Competition, the claiming, redemption or value of any prizes under it, the use or enjoyment of such prizes or any events or circumstances arising out of or in connection with any of them. Any implied warranties of condition, merchantability or suitability or fitness for purpose of any of them are hereby expressly excluded. Wherever used in these Terms, ‘Liability’ shall mean any and all costs, expenses, claims, damages, actions, proceedings, demands, losses and other liabilities (including legal fees and costs on a full indemnity basis) arising directly or indirectly out of or in connection with the matter concerned.

5.1 The RoadTest is organised and sponsored by the Organiser. The Organiser reserves the right to delegate all or any of its powers, rights and obligations arising in relation to the RoadTest to any Associate and certain such rights and powers are assumed by the Organiser on behalf of itself and each Associate. Reference to “Organiser” shall be deemed to include reference to each Associate.

5.2 The RoadTest may be terminated at any time if there are, in the sole opinion of the Organiser, an insufficient number of entries, or if the Applications are not of an appropriate standard for a competition of this nature. The Organiser has the right to cancel or suspend the RoadTest at any time due to circumstances outside its reasonable control.

5.3 The Organiser shall have the sole discretion to disqualify (without correspondence or right of appeal) any Applicant it considers to be adversely affecting the process or the operation of the RoadTest or to be in breach of these Terms or to be acting in a disruptive manner or with intent to annoy, abuse, threaten or harass any other Applicant or Participant.

5.4 The Organiser has the right to amend or add to these Terms from time to time. Revised Terms and Conditions will be posted on the Contest Site and it is a condition of entry to the RoadTest that Applicants agree to comply with these Terms and, if appropriate, such Terms as amended from time to time.

5.5 Headings are for convenience only and do not affect the interpretation or construction of these Terms and Conditions.

5.6 These Terms and the operation of the Contest shall be governed by and construed in accordance with English Law and any claim or matter arising under these Terms shall be subject to the exclusive jurisdiction of the English courts.

Tax IssuesIf you are a U.S. taxpayer, you will be required to complete a W-9 form and we will issue you a 1099 form. If you are not a U.S. tax payer, you need to follow the tax laws in your country as per the terms & conditions of this contest.
RoadTest Reviews
Comment List
Anonymous
  • Ha Ha.

     

    Everyone in the e14 office knows Randall is not the best typist!

     

    cat = cut

  • I always like to extend the functionality of test equipment,  for instance on my DMM6500 I performed a rudimentary IV plot of diodes and added support to custom thermistors (I still have to blog about it, but Keithley already integrated my TSP program into their main github branch (https://github.com/tektronix/keithley/tree/master/Application_Specific/Custom_Thermistor )).

     

    I noticed that this oscilloscope doesn't perform frequency response analysis (like Keysight 1000 series oscilloscopes). So I wrote code to compute the frequency response and phase shift to generate a Bode plot. As I didn't have access to the oscilloscope when I wrote the code, I just added a dummy function that simulates the oscilloscope probing of an

    RC filter plus noise, this function would have to be adapted to send oscilloscopes commands to set the oscilloscope, perform the probing and then read back the data. The code basically compares an input and an output signal, and then uses Fourier to computes the gain and phase shift. The program worked pretty good with synthetic noisy signals, so it should be robust enough to work ok with the oscilloscope.

     

    If any of the roadtesters wants to try the code letme know, as I don't have any use for it...

  • I wish to send out a congratulations to: and .image

    So lets get this party started!!

  •   wrote:

    The applicants in the final cat got two more readings.

    I wonder if any of the applications involved using the oscilloscope to do something with a cat. Bonus internet points if they did!

     

    Congrats and !

     

    - Gough

  • Congratulation Donald and Gerrit!  I hope that you both enjoy your well deserved instruments and that you both produce excellent reviews (as we all know that you can)!

  • Congratulations - that is a beast of an instrument.

  • This is great news, many thanks to and tektronix for selecting my application.

    I also appreciate the kind words and support from my fellow applicants.

    I'm used to start my review with a copy of the application, so , stay tuned.

     

    Congratulations also to fellow roadtester .

     

    I will do my utmost to come up with a sound review.

     

    Kind regards.

    Gerrit.

  • Congratulations and on getting your hands on this great product. While we've been waiting I've had a visit from the local Tek rep complete with the 6-Series scope...many of the features he was pointing out are also in your top spec units so I know you'll be having lots of fun there. He was talking about each channel having both time and frequency measurement but only recently has the software been released although the hardware has essentially been there the whole time.....will be interesting to see that explained please :-)

     

    Of course the rest of us will now not have an excuse to dodge any seasonal festivities image

  • wow, many thanks to and tektronix for selecting my application. Many thanks to all of you for your kind words and support and my commiserations to those that applied and have missed out on this occasion.

     

    Congratulations to fellow roadster

     

    It looks like I have a few weeks of hard work ahead of me!

     

    Kind regards.

  • Well done and ! You beat 111 other people to the golden prize. Looking forward to your reviews.