Cmod S7: Breadboardable Spartan-7 FPGA Module

View table of contents ...  

image

 

{tabbedtable} Tab LabelTab Content
About

The Digilent Cmod S7 is a small, 48-pin DIP form factor board populated with 36 pins and built around a Xilinx Spartan-7 FPGA. The 32 FPGA digital I/O signals, 2 FPGA analog input signals, an external power input rail, and ground are routed to 100-mil-spaced through-hole pins, making the Cmod S7 well-suited for use with solderless breadboards. At just 0.7” by 3.05” inches, it can be loaded in a standard socket and used in embedded systems. The board also includes a programming ROM, clock source, USB programming and data transfer circuit, power supplies, LEDs, and buttons.

image

Features:

Xilinx Spartan-7 FPGA (XC7S25-1CSGA225C)

  • 3,650 slices containing four 6-input LUTs and 8 flip-flops
  • 1,620 Kbits of fast block RAM
  • Three clock management tile, each with a phase-locked loop and mixed-mode clock manager
  • 80 DSP slices
  • Internal clock speeds exceeding 450 MHz
  • On-chip analog-to-digital converter (XADC)
  • Programmable over JTAG and Quad-SPI Flash

Memory

  • 4 MB Quad-SPI Flash

Power

  • Powered from USB or 5V external supply connected to DIP pin 24 (micro USB cable NOT included)

USB

  • USB-JTAG programming circuitry
  • USB-UART bridge

Push-buttons and LEDs

  • 2 Buttons
  • 4 LEDs
  • 1 RGB LED

Expansion Connectors

  • 1 Pmod connector
  • 8 total FPGA I/O

48-pin DIP form-factor headers

 

Contents

  • Cmod S7
  • Digilent cardboard packaging with protective foam inserts

 

Additional Information

Important Dates

Enrollment Begin:Mar 9 2020

Enrollment Ends: Apr 14 2020

RoadTesters Selected: Apr 21 2020

Product Shipped: May 29 2020

RoadTesting Begins: June 5 2020

Reminder/Update Email: July 5 2020

Submit Reviews By: Aug 5 2020

*The element14 RoadTest Staff will send this reminder/update email.

**If a RoadTester is unable to meet the deadline, please notify the RoadTest Program Lead, , as soon as possible before the deadline.

RoadTesters

expected August 12

Terms and Conditions

RoadTest: Terms and Conditions

Digilent CMOD S7

 

These are the terms and conditions which govern the Digilent CMOD S7 contest. This Contest requires participants to submit an application indicating their previous experience with this type of equipment/component, information on what they would do to test the equipment/component, and the applicant’s desire to post a thorough review of their experience with images, photos, or other supplemental materials. Participants will be required to meet the Conditions for Participation.  The winners of this RoadTest will receive the item(s) listed below. RoadTest Reviews are due no later than 60 days after the receipt of the item(s). No other prizes are offered.

The Principal terms of the Competition:

The following words and phrases are used in these terms and conditions and have the meanings given to them below.

(RoadTest or Contest)

Key dates:

Applications Close: midnight (GMT) on Apr 14 2019

Announcement of Winner (estimated): Apr 16 2019

Prize: Digilent CMOD S7

Additional Prizes: none

Competition Site: https://www.element14.com/community/groups/roadtest?ICID=menubar_resources_roadtest

Site or element14 Community: www.element14.com/community

Judges: members of the element14 community team chosen at the Organiser’s discretion.

Judging Criteria, All of the following which will have equal weighting:

· Demonstrated competence with the technologies including links or descriptions of past projects

· Qualifications as indicated by current job role and/or schooling/vocational training;

· A thorough description of how the prize would be tested;

· Likelihood that the Applicant will blog about the prize and provide a review on element14.com;

· Originality;

· Innovation.

Organiser: Premier Farnell plc (registered in England and Wales under company number 876412) whose registered office is at Farnell House, Forge Lane, Leeds, UK

Conditions for Qualification: in addition to meeting the requirements of these terms, all persons applying to take part in the Contest (each one an Applicant) must:

· Provide a RoadTest application describing what he/she would do if awarded the Prize including similar previous projects, product experience and qualifications

Terms: these terms and conditions which govern the Competition and to which the Organiser reserves the right to make changes from time to time and the latest version of these Terms from time to time will be posted to the Site.

  1. Eligibility
  2. Applications:
  3. Selecting Winners:
  4. Liability:
  5. General:

1.1 Save as set out in these Terms, the Contest is open to any natural or legal person, firm or company or group of natural persons or unincorporated body.

1.2 All Applicants must be aged at least 18 at the time of their application.

1.3 Applicants must not enter the RoadTest if doing so or taking part may:

1.3.1 cause the Organiser and/or themselves to be in breach of any agreement (including but not limited to any contract of employment) to which they are a party or in breach of any law, regulation or rule having the force of law to which the Organiser or the Applicant may be subject or any policy of the Organiser or the Sponsor;

1.3.2 Require the Organiser to obtain any licence, authorisation or permission to deal with the Applicant; or

1.3.3 Be in breach of any policy or practice of their employer. Some employers prohibit or restrict their employees from taking part in competitions such as these or receiving prizes under them and the Organiser respects those policies and practices.

The Organiser reserves the right to disqualify any Application made in breach of these Terms and to reject any Application which it reasonably believes may be or become in breach. The Organiser reserves the right to require evidence in such form as the Organiser may reasonably require of any Applicant’s compliance with any of these Terms and to disqualify any Applicant or Participant who cannot provide such evidence reasonably promptly.

1.4 Multiple applications are not permitted.

1.5 Applications may not be submitted by an agent whether acting on behalf of an undisclosed principal or otherwise.

1.6 The Contest is NOT open to:

1.6.1 Any person or entity who is a resident or national of any country which is subject to sanctions, embargoes or national trade restrictions of the United States of America, the European Union or the United Kingdom;

1.6.2 Any employee, director, member, shareholder (as appropriate) or any of their direct families (parents, siblings, spouse, partner, children) (“Direct Families”) of the Organiser and Sponsors; or

2.1 Each Applicant must fully complete and submit a RoadTest Application by the Application Close.

2.2 By submitting a Registration Form, each Applicant:

2.2.1 Authorises the Organiser to use his or her personal data (as defined in the Data Protection Act 1998) for the purposes of running and promoting the RoadTest;

2.2.2 Authorises the Organizer to copy, reproduce and publish their application should they be accepted as a Participant;

2.2.3 Will be deemed to have read, accepted and agree to be bound by these Terms. Applicants are advised to print and keep safe these Terms;

2.2.4 Authorises the Organiser to copy, reproduce and use the Application and/or Review for the purposes of the RoadTest and as otherwise contemplated by these Terms. The Organiser will not be responsible for any inaccuracy, error or omission contained in any reproduction or use of the Project Blogs.

2.2.5 Licenses the Organiser to use the intellectual property in the Project (IP) for the purposes of this Contest. As between the Applicant and the Organiser the IP remains owned by the Applicant.

2.2.6 Grants the Organiser the right to use his or her likeness, photographs, logos, trademarks, audio or video recordings without restriction for the purposes of Contest or the promotion of it or the Site;

2.2.7 Agrees to participate positively in all publicity surrounding the Contest;

2.2.8 Agrees to be responsible for all expenses and costs incurred by him or her in preparing for, entering and participating in the Contest (save for any expenses expressly agreed by the Organiser to be borne by it in these Terms);

2.2.9 Confirms that he or she owns all IP used in his or her application or Project or Blogs and indemnifies the Organiser from any claim by a third party that use of any material provided by an Applicant to the Organiser infringes the intellectual property rights of any third party;

2.2.10 Agrees not to act in any way or fail to act in any way or be associated with any cause or group which would have a negative impact on the reputation of the Organiser and/or the RoadTest.

2.3 All applications submitted to this RoadTest must meet the following criteria:

2.3.1 Applicants must be the author, creator and owner of the proposed review idea. Applicants must not submit someone else’s idea;

2.3.2 The proposed application must be reasonably achievable by the within the time constraints of the Contest;

2.3.3 Applications must not include or propose any of the following, the inclusion of which shall render any proposed application ineligible:

(a) Applications which relate to socially taboo topics, such as illicit drug use or sexual gratification;

(b) Applications that are or could reasonably be considered to be illegal, immoral, discriminatory or offensive as determined by the Organiser;

(c) Applications in relation to them which if accepted would infringe or breach any of the policies or terms of access or use of the Site.

2.4 No Application may contain any of the hazardous substances identified by Article 4 of Directive 2002/95/EC of the European Parliament on the Restrictions on the Use of Substances in Electronic and Electrical Equipment ("the Directive") or the use of such hazardous substances in the in any such Project must not exceed the maximum concentration values set out in the Directive.

3.1 Winners will be selected by the Organiser on the basis of the quality of his or her application and its adherence to these Terms.

3.2 The total number of Winners selected will be at least the minimum number set out above but the actual number is at the sole discretion of the Organizer and/or the Sponsor, if applicable.

3.3 The Organiser will use all reasonable efforts to announce the Winners via an update to the RoadTest page by the date listed above.

3.4 Winners agree to take part in all publicity which the Organiser or the Sponsor wishes to use to promote the RoadTest, the Products featured or other Contests with which the Organiser may be connected from time to time.

3.5 Details of the Winners may also be published in the media.

3.6 Winners are responsible for all applicable taxes, duties or other charges payable in relation to any prize.

3.7

4.1 The Organiser hereby excludes all and any Liability arising out of the Contest or the acceptance, use, quality, condition, suitability or performance of any Prize, even where that Liability may arise from the Organiser’s negligence.

4.2 Nothing in these Terms will affect any Liability of the Organiser for death or personal injury arising from its negligence, for breach of Part II of the Consumer Protection Act 1987 (in the event that any entrant is entitled to claim rights under the Consumer Protection Act 1987) or for any matter in relation to which it would be illegal for the Organiser to exclude or to attempt to exclude its Liability.

4.3 Subject to 4.2, neither the Organiser, any parent company nor any subsidiary of the Organiser or such parent company or any of their directors, officers and employees (together referred to in these terms and the ‘Associates’) makes any guarantee, warranty or representation of any kind, express or implied, with respect to this Competition or the Prizes potentially available under it. Neither the Organiser nor any of its Associates shall be responsible for any Liability that may arise out of or in connection with person’s participation in this Competition, the claiming, redemption or value of any prizes under it, the use or enjoyment of such prizes or any events or circumstances arising out of or in connection with any of them. Any implied warranties of condition, merchantability or suitability or fitness for purpose of any of them are hereby expressly excluded. Wherever used in these Terms, ‘Liability’ shall mean any and all costs, expenses, claims, damages, actions, proceedings, demands, losses and other liabilities (including legal fees and costs on a full indemnity basis) arising directly or indirectly out of or in connection with the matter concerned.

5.1 The RoadTest is organised and sponsored by the Organiser. The Organiser reserves the right to delegate all or any of its powers, rights and obligations arising in relation to the RoadTest to any Associate and certain such rights and powers are assumed by the Organiser on behalf of itself and each Associate. Reference to “Organiser” shall be deemed to include reference to each Associate.

5.2 The RoadTest may be terminated at any time if there are, in the sole opinion of the Organiser, an insufficient number of entries, or if the Applications are not of an appropriate standard for a competition of this nature. The Organiser has the right to cancel or suspend the RoadTest at any time due to circumstances outside its reasonable control.

5.3 The Organiser shall have the sole discretion to disqualify (without correspondence or right of appeal) any Applicant it considers to be adversely affecting the process or the operation of the RoadTest or to be in breach of these Terms or to be acting in a disruptive manner or with intent to annoy, abuse, threaten or harass any other Applicant or Participant.

5.4 The Organiser has the right to amend or add to these Terms from time to time. Revised Terms and Conditions will be posted on the Contest Site and it is a condition of entry to the RoadTest that Applicants agree to comply with these Terms and, if appropriate, such Terms as amended from time to time.

5.5 Headings are for convenience only and do not affect the interpretation or construction of these Terms and Conditions.

5.6 These Terms and the operation of the Contest shall be governed by and construed in accordance with English Law and any claim or matter arising under these Terms shall be subject to the exclusive jurisdiction of the English courts.

RoadTest Reviews
Comments
Anonymous
  • The following applicants have been selected as official roadtesters:

     

  • To all applicants...

     

    During my first read, I had to eliminate 5 applications as ineligible because they didn't answer any of the questions on the applicantion form. That leaves 32 applications that will be forwarded to the sponsor, along with my recommendations.

     

    Randall Scasny

    RoadTest Program Manager

  • Really wanted to try this. Never got a chance to play with an FPGA earlier. Unfortunately, I am already in another roadtest which is also an awesome module. So sadly stepping out.

  • I can release a set of Physical Unclonable Function, PUF + create a video brief of board and share it with our FPGA Developers Community - www.fpga-systems.ru and push it on our youtube channel

  • I found this to be a good way to learn and practice some Verilog without even needing any hardware.

    https://hdlbits.01xz.net/wiki/Main_Page

  • Gary it depends on how you want to use the FPGA and on what FPGA you are interested in. For instance Zynqs add an ARM processor, if you want to use the ARM + the programmable logic (PL) it can get more complex. What I've done so far is play mostly with the PL through Verilog (which is one of the 2 main hardware description languages). There are too many workflows available to program FPGAs, but I'm mostly familiar with the Verilog HDL. HDL's are what's closest to the FPGA hardware, so its useful to learn to actually understand how FPGAs work. I think its similar to learning assembly, before learning assembly, CPUs seem to do magic.

     

    If you check other FPGA roadtests many run examples or build simple designs with the IP designer. The latter is kinda like connecting nodes that are visual representations of HDL code. I'm not really sure whats the "proper" way to evaluate/roadtest FPGAs. For instance FPGA features depend only on the FPGA chip, but how its integrated into the board will define stuff like voltages, peripherals, available pins, etc. I was offered this FPGA board, and Randall asked me to blog about my experience while exploring it, and that's what I did, just play with it and have fun. Before getting the FPGA I just knew a bit about them from reading and watching videos, I always found them intriguing and interesting, but I wasn't sure if they would be my thing. After getting the FPGA I ended up liking them much more than what I expected.

    Now back to where to start I can only tell you about my experience learning Verilog. At the beginning there are many hard to grasp concepts, caused by 2 reasons: the particularities of FPGA programming, and the amount of Verilog tutorials in the net. I ended up learning from many different sources and when in doubt, I used google to find answers.

    It is possible to learn Verilog and run code in the simulator, but it's kinda boring. Even a light blinker is very rewarding once you see it run in a physical FPGA.

     

    In my CMOD S7 post I tried to explain/expose some of the concepts that I initially didn't feel were explained in much detail in the tutorials I read. One of them is how the HDL gets converted into the FPGA fabric. In my post I showed a few simple examples where I explored how the connected hardware IPs performed the task described in the HDL code.

  • Thanks for the link to your report. It was helpful to see real work using the FPGA.

    I'd like to learn more about FPGA applications, how to use them, when to use them, VS microcontrollers or S.O.C.

     

    I like your comments about apprehension about doing a road test, and share the same thought.

    I'd prefer to do an FPGA Road Test when it comes with a training course, or aimed at beginners.

    Its not fair to the vendor to provide samples for evaluating their product if I don't know where to start.  

     

    Do you have more recommendations for getting a noob started with FPGAs ?

  • This was my first FPGA board, and I've had a lot of fun playing with it. Here is a link to my journey exploring the board:

     

    Learning Verilog with the Digilent Cmod S7

  • This is a Spartan 7 so you should be working with Vivado. I think you need ISE for Spartan 6 and below. [This was a reply to a comment which has now been deleted.]