InfiniiVision 3000T X-Series Oscilloscope MSOX3034

Table of contents

image

 

{tabbedtable} Tab LabelTab Content
About

The Keysight Technologies MSOX3034T is a 350Mhz Mixed Signal Oscilloscope (MSO) with 4 analog plus 16 digital channels. It features a large 8.5-inch capacitive touch screen so you can easily view and analyze signals and isolate signals in seconds with exclusive Zone touch triggering. This oscilloscope allows you to see more signal detail with the 1,000,000 wfms/s update rate and capture more data with up to 4 Mpts memory.

image

image

Basic Features

  • Bandwidth: 350 MHz
  • Bandwidth Upgrades: Available
  • Channels: 4 + 16
  • Max Memory Depth: 4 Mpts
  • Max Sample Rate: 5 GSa/s
  • Display Size: 8.5 inch
  • Waveform Update Rate: 1,000,000 wfms/s
  • ADC Bits: 8 bits
  • Special Triggers: edge, pulse width, video, protocol decodes, zone touch, edge then edge, pattern, runt pulse, rise/fall time, Nth edge burst, setup and hold
  • Operating System: Embedded

 

About Keysight InfiniiVision 3000T X-Series Oscilloscopes

The 3000T X-Series takes everything that was revolutionary about the A model and adds a capacitive touch screen, a user interface designed for touch, and the exclusive Zone touch trigger, all combined with an industry-leading uncompromised update rate of 1 million wfm/s to give you the confidence that you're seeing all of your signal detail, and the ability to discover any issues. And the addition of new analysis capabilities help you solve your hardest problems quickly. The 3000T X-Series once again redefines what you can expect in a general purpose oscilloscope by providing all of the performance and capability you need to get to measurement insights faster.

 

Additional Features

  • 8.5-inch capacitive touch screen
  • Designed for touch interface
  • Exclusive InfiniiScan Zone touch trigger
  • Wide range of serial decodes
  • 6-in-1 instrument integration
  • Analogue, digital, and frequency domain correlation with the gated FFT
  • 3-year standard calibration cycle

 

Contents

  • MSOX3034T -  MSO / MDO Oscilloscope
  • One N2843A 500MHz Passive Probe Per Channel (10:1)
  • N2756A 16 digital channel MSO cable
  • Certificate of Calibration
  • BenchVue software license (BV0004B)

 

Additional Information

 

Videos

Important Dates

Enrollment Begin: June 9 2020

Enrollment Ends: July 10 2020

RoadTesters Selected: July 17 2020 (estimated)

Product Shipped: July 31 2020

RoadTesting Begins: Aug 6 2020

Reminder/Update Email: Sept 6 2020

Submit Reviews By: Oct 6 2020

*The element14 RoadTest Staff will send this reminder/update email.

**If a RoadTester is unable to meet the deadline, please notify the RoadTest Program Lead, , as soon as possible before the deadline.

RoadTesters

Terms and Conditions

InfiniiVision 3000T X-Series Oscilloscope MSOX3034  – RoadTest

Terms and Conditions

These are the terms and conditions which govern the InfiniiVision 3000T X-Series Oscilloscope MSOX3034 RoadTest contest. This Contest requires participants to submit an application indicating their previous experience with this type of equipment/component, information on what they would do to test the equipment/component, and the applicant’s desire to post a thorough review of their experience with images, photos, or other supplemental materials. Participants will be required to meet the Conditions for Participation.  The winners of this RoadTest will receive the item(s) listed below. RoadTest Reviews are due no later than 60 days after the receipt of the item(s). No other prizes are offered.

The Principal terms of the Competition:

The following words and phrases are used in these terms and conditions and have the meanings given to them below.

 

Key dates:

Applications Close: midnight (GMT) on July 10 2020

Announcement of Winner (estimated): July 17 2020

Prize:  InfiniiVision 3000T X-Series Oscilloscope MSOX3034

Additional Prizes: none

Competition Site: https://www.element14.com/community/groups/roadtest?ICID=menubar_resources_roadtest

Site or element14 Community: www.element14.com/community

Judges: members of the element14 community team chosen at the Organiser’s discretion.

Judging Criteria, All of the following which will have equal weighting:

· Demonstrated competence with the technologies including links or descriptions of past projects

· Qualifications as indicated by current job role and/or schooling/vocational training;

· A thorough description of how the prize would be tested;

· Likelihood that the Applicant will blog about the prize and provide a review on element14.com;

· Originality;

· Innovation.

Organiser: Premier Farnell plc (registered in England and Wales under company number 876412) whose registered office is at Farnell House, Forge Lane, Leeds, UK

Conditions for Qualification: in addition to meeting the requirements of these terms, all persons applying to take part in the Contest (each one an Applicant) must:

· Provide a RoadTest application describing what he/she would do if awarded the Prize including similar previous projects, product experience and qualifications

Terms: these terms and conditions which govern the Competition and to which the Organiser reserves the right to make changes from time to time and the latest version of these Terms from time to time will be posted to the Site.

  1. Eligibility
  2. Applications:
  3. Selecting Winners: 
  4. Liability:
  5. General:

1.1 Save as set out in these Terms, the Contest is open to any natural or legal person, firm or company or group of natural persons or unincorporated body.

1.2 All Applicants must be aged at least 18 at the time of their application.

1.3 Applicants must not enter the RoadTest if doing so or taking part may:

1.3.1 cause the Organiser and/or themselves to be in breach of any agreement (including but not limited to any contract of employment) to which they are a party or in breach of any law, regulation or rule having the force of law to which the Organiser or the Applicant may be subject or any policy of the Organiser or the Sponsor;

1.3.2 Require the Organiser to obtain any licence, authorisation or permission to deal with the Applicant; or

1.3.3 Be in breach of any policy or practice of their employer. Some employers prohibit or restrict their employees from taking part in competitions such as these or receiving prizes under them and the Organiser respects those policies and practices.

The Organiser reserves the right to disqualify any Application made in breach of these Terms and to reject any Application which it reasonably believes may be or become in breach. The Organiser reserves the right to require evidence in such form as the Organiser may reasonably require of any Applicant’s compliance with any of these Terms and to disqualify any Applicant or Participant who cannot provide such evidence reasonably promptly.

1.4 Multiple applications are not permitted.

1.5 Applications may not be submitted by an agent whether acting on behalf of an undisclosed principal or otherwise.

1.6 The Contest is NOT open to:

1.6.1 Any person or entity who is a resident or national of any country which is subject to sanctions, embargoes or national trade restrictions of the United States of America, the European Union or the United Kingdom;

1.6.2 Any employee, director, member, shareholder (as appropriate) or any of their direct families (parents, siblings, spouse, partner, children) (“Direct Families”) of the Organiser and Sponsors; or

2.1 Each Applicant must fully complete and submit a RoadTest Application by the Application Close.

2.2 By submitting a Registration Form, each Applicant:

2.2.1 Authorises the Organiser to use his or her personal data (as defined in the Data Protection Act 1998) for the purposes of running and promoting the RoadTest;

2.2.2 Authorises the Organizer to copy, reproduce and publish their application should they be accepted as a Participant;

2.2.3 Will be deemed to have read, accepted and agree to be bound by these Terms. Applicants are advised to print and keep safe these Terms;

2.2.4 Authorises the Organiser to copy, reproduce and use the Application and/or Review for the purposes of the RoadTest and as otherwise contemplated by these Terms. The Organiser will not be responsible for any inaccuracy, error or omission contained in any reproduction or use of the Project Blogs.

2.2.5 Licenses the Organiser to use the intellectual property in the Project (IP) for the purposes of this Contest. As between the Applicant and the Organiser the IP remains owned by the Applicant.

2.2.6 Grants the Organiser the right to use his or her likeness, photographs, logos, trademarks, audio or video recordings without restriction for the purposes of Contest or the promotion of it or the Site;

2.2.7 Agrees to participate positively in all publicity surrounding the Contest;

2.2.8 Agrees to be responsible for all expenses and costs incurred by him or her in preparing for, entering and participating in the Contest (save for any expenses expressly agreed by the Organiser to be borne by it in these Terms);

2.2.9 Confirms that he or she owns all IP used in his or her application or Project or Blogs and indemnifies the Organiser from any claim by a third party that use of any material provided by an Applicant to the Organiser infringes the intellectual property rights of any third party;

2.2.10 Agrees not to act in any way or fail to act in any way or be associated with any cause or group which would have a negative impact on the reputation of the Organiser and/or the RoadTest.

2.3 All applications submitted to this RoadTest must meet the following criteria:

2.3.1 Applicants must be the author, creator and owner of the proposed review idea. Applicants must not submit someone else’s idea;

2.3.2 The proposed application must be reasonably achievable by the within the time constraints of the Contest;

2.3.3 Applications must not include or propose any of the following, the inclusion of which shall render any proposed application ineligible:

(a) Applications which relate to socially taboo topics, such as illicit drug use or sexual gratification;

(b) Applications that are or could reasonably be considered to be illegal, immoral, discriminatory or offensive as determined by the Organiser;

(c) Applications in relation to them which if accepted would infringe or breach any of the policies or terms of access or use of the Site.

2.4 No Application may contain any of the hazardous substances identified by Article 4 of Directive 2002/95/EC of the European Parliament on the Restrictions on the Use of Substances in Electronic and Electrical Equipment ("the Directive") or the use of such hazardous substances in the in any such Project must not exceed the maximum concentration values set out in the Directive.

3.1 Winners will be selected by the Organiser on the basis of the quality of his or her application and its adherence to these Terms.

3.2 The total number of Winners selected will be at least the minimum number set out above but the actual number is at the sole discretion of the Organizer and/or the Sponsor, if applicable.

3.3 The Organiser will use all reasonable efforts to announce the Winners via an update to the RoadTest page by the date listed above.

3.4 Winners agree to take part in all publicity which the Organiser or the Sponsor wishes to use to promote the RoadTest, the Products featured or other Contests with which the Organiser may be connected from time to time.

3.5 Details of the Winners may also be published in the media.

3.6 Winners are responsible for all applicable taxes, duties or other charges payable in relation to any prize.

3.7

4.1 The Organiser hereby excludes all and any Liability arising out of the Contest or the acceptance, use, quality, condition, suitability or performance of any Prize, even where that Liability may arise from the Organiser’s negligence.

4.2 Nothing in these Terms will affect any Liability of the Organiser for death or personal injury arising from its negligence, for breach of Part II of the Consumer Protection Act 1987 (in the event that any entrant is entitled to claim rights under the Consumer Protection Act 1987) or for any matter in relation to which it would be illegal for the Organiser to exclude or to attempt to exclude its Liability.

4.3 Subject to 4.2, neither the Organiser, any parent company nor any subsidiary of the Organiser or such parent company or any of their directors, officers and employees (together referred to in these terms and the ‘Associates’) makes any guarantee, warranty or representation of any kind, express or implied, with respect to this Competition or the Prizes potentially available under it. Neither the Organiser nor any of its Associates shall be responsible for any Liability that may arise out of or in connection with person’s participation in this Competition, the claiming, redemption or value of any prizes under it, the use or enjoyment of such prizes or any events or circumstances arising out of or in connection with any of them. Any implied warranties of condition, merchantability or suitability or fitness for purpose of any of them are hereby expressly excluded. Wherever used in these Terms, ‘Liability’ shall mean any and all costs, expenses, claims, damages, actions, proceedings, demands, losses and other liabilities (including legal fees and costs on a full indemnity basis) arising directly or indirectly out of or in connection with the matter concerned.

5.1 The RoadTest is organised and sponsored by the Organiser. The Organiser reserves the right to delegate all or any of its powers, rights and obligations arising in relation to the RoadTest to any Associate and certain such rights and powers are assumed by the Organiser on behalf of itself and each Associate. Reference to “Organiser” shall be deemed to include reference to each Associate.

5.2 The RoadTest may be terminated at any time if there are, in the sole opinion of the Organiser, an insufficient number of entries, or if the Applications are not of an appropriate standard for a competition of this nature. The Organiser has the right to cancel or suspend the RoadTest at any time due to circumstances outside its reasonable control.

5.3 The Organiser shall have the sole discretion to disqualify (without correspondence or right of appeal) any Applicant it considers to be adversely affecting the process or the operation of the RoadTest or to be in breach of these Terms or to be acting in a disruptive manner or with intent to annoy, abuse, threaten or harass any other Applicant or Participant.

5.4 The Organiser has the right to amend or add to these Terms from time to time. Revised Terms and Conditions will be posted on the Contest Site and it is a condition of entry to the RoadTest that Applicants agree to comply with these Terms and, if appropriate, such Terms as amended from time to time.

5.5 Headings are for convenience only and do not affect the interpretation or construction of these Terms and Conditions.

5.6 These Terms and the operation of the Contest shall be governed by and construed in accordance with English Law and any claim or matter arising under these Terms shall be subject to the exclusive jurisdiction of the English courts.

Comment List
Anonymous
  • The tax laws are different for each country, so you would need to consult with a local tax accountant and how prizes of this nature are treated in your country.

     

    Generally, element14 will pay any duties applicable at import, it will be more a case of how competition prizes are taxed or if the winnings are seen as part of your income.

     

    Kind regards

  • , no I have not upgraded the software on the MDO34, I must look into that, it seems to have a few quirks and had locked up a few times in use. Hopefully that will sort some of them out. Thanks for letting me know, seems like Tektronix don't send out update alerts for registered instruments, unless I did not opt for it.

     

    The lack of a sweep generator is strange, you can program it to perform the function using external computer, but would certainly be nice to have it built in.

     

    I have no object to road testers applying for the same type of apparatus in order to do a comparison style review, they can be interesting to follow along with. I just have a few more interests to follow closer to my home territory at the moment.

     

    I wonder if you can get loan unit for a couple of weeks, as you can with the Tektronix unit and do a quick overview comparison.

     

    Kind regards.

  •   wrote:

     

    I am happy with the MDO34 I tested, so as per Doug, I will sit and watch this from the side.

     

    same here, but I'm very curious how it compares to the MDO34, so selected reviewers, please have a look at our MDO34 reviews.

     

    BTW, did you see that there is a software update for the MDO34? I just upgraded a few weeks ago and will update my review accordingly soon. Some bugs are fixed, and there are some nice additions, like modulation on the AFG. (no sweep yet unfortunately).

     

    Best,

    Gerrit.

  • How does this tax bill work? Say if you are shipping this to India. We have 18 % of GST and 15 % customs duty for electronics equipments.

    So do I need to pay 32 % of the cost of the item ? Which means I need to pay ~$3520 ?

  • Yes, it will certainly be interesting to see what the testers make of this oscilloscope. Curious to know what the exact specification is of the units offered, you may be lucky and get some unofficial upgrades thrown in, even if they are just time limited licences for the evaluation.

     

    I am happy with the MDO34 I tested, so as per Doug, I will sit an watch this from the side.

     

    Good luck to those that apply.

  • I'd love to RoadTest a piece of gear like this, but I'm positive I could not afford the tax bill.

  • This looks like a great scope for people into MSP and other embedded applications. Very eager to apply for this.

  • Oh yeah! Nice Device.

    Here can you download the actual firmware, 2020-02-26; Version 7.31.20200128; for 3000T X-Series oscilloscopes:

     

    https://www.keysight.com/main/software.jspx?ckey=2573488&lc=ger&cc=AT&nid=-32541.1150362&id=2573488

     

    Supported Instruments

    DSOX3012T, DSOX3014T, DSOX3022T, DSOX3024T, DSOX3032T, DSOX3034T, DSOX3052T, DSOX3054T, DSOX3102T, DSOX3104T, MSOX3012T, MSOX3014T, MSOX3022T, MSOX3024T, MSOX3032T, MSOX3034T, MSOX3052T, MSOX3054T, MSOX3102T, MSOX3104T

     

    Best Regards

    Gerald

    ---

  • Question 1:  "Bandwidth Upgrades: Available"  Will the unit include the bandwidth upgrades and, if so, what are the upgrades?

    Question 2:  "6-in-1 instrument integration" Are there any HW or SW upgrades included? (i.e. WaveGen, GPIB/Lan interface, Power SW package, Embedded SW package, etc.)

     

    In general the USA tax liability for ~$11000 piece of equipment may be too high for many applicants.  Was E14 looking into reducing the liability?

     

    Gordon